This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:ad5110 [28 Sep 2012 11:27] – Added common section for describing the evaluation setup and System Demonstration Platform Adrian Costina | resources:fpga:xilinx:interposer:ad5110 [13 Aug 2013 14:34] – [Downloads] Lucian Sin | ||
---|---|---|---|
Line 11: | Line 11: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi> | + | This document presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
Line 34: | Line 34: | ||
* [[adi>/ | * [[adi>/ | ||
* [[http:// | * [[http:// | ||
- | * [[http:// | ||
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 44: | Line 43: | ||
* [[http:// | * [[http:// | ||
* FMC-SDP adapter board | * FMC-SDP adapter board | ||
- | * **EVAL-AD5110** evaluation board | + | * **EVAL-AD5110SDZ** evaluation board |
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6. |
- | * [[http://micrium.com/ | + | * UART Terminal (Termite/Tera Term/Hyperterminal), |
+ | * The EVAL-AD5110 reference project for Xilinx KC705 FPGA. | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | + | <WRAP round download 80%> | |
- | * {{: | + | \\ |
- | + | * {{: | |
- | The following table presents a short description the reference design archive contents. | + | * **AD511x Driver:** https:// |
- | + | * **AD5110 Commands:** https:// | |
- | ^ **Folder** ^ **Description** ^ | + | |
- | | Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation. | | + | \\ |
- | | Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | | + | </ |
- | | Software | Contains the source files of the software project that will be run by the Microblaze processor.| | + | |
- | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microbalze memory. | | + | |
====== Run the Demonstration Project ====== | ====== Run the Demonstration Project ====== | ||
- | {{page> | + | ===== Hardware setup ===== |
- | + | ||
- | ===== Demonstration Project User Interface | + | |
- | + | ||
- | The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-AD5110SDZ** evaluation board. | + | |
- | + | ||
- | {{ : | + | |
- | **Section A** is used to activate | + | <WRAP round important 80%> |
+ | \\ | ||
+ | Before connecting | ||
+ | </ | ||
- | **Section B** allows | + | |
+ | * Connect | ||
- | **Section C** allows | + | ===== Quick start evaluation ===== |
+ | For a quick start evaluation, run the **download.bat** script located in the **SDK/ | ||
- | **Section D** is used to read the value of RDAC programmed in the internal EEPROM. | + | <WRAP round info 80%> |
+ | \\ | ||
+ | The **download.bat** script assumes that the Xilinx ISE Design Suite 14.6 is installed at this path: **C:/ | ||
+ | </ | ||
- | **Section E** displays | + | If programming was successful, you should be seeing |
- | **Section F** is used to shutdown | + | ===== Reference Project Overview ===== |
+ | The following commands were implemented in this version of EVAL-AD5110 reference project for Xilinx KC705 FPGA board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **reset!** | Makes a software reset of the device. | | ||
+ | | **rdac=** | Writes | ||
+ | | **rdac?** | Displays the last written value in RDAC register. | | ||
+ | | **rdacToEeprom!** | Writes the content of RDAC register to EEPROM. | | ||
+ | | **wiper?** | Displays the wiper resistance from EEPROM. | | ||
+ | | **tolerance? | ||
+ | | **power=** | Turns on/ | ||
+ | | **power?** | Displays the power status of the device. | | ||
- | **Section G** is used to perform a Software Reset (loads the RDAC Register with the value programmed in the EEPROM). | ||
- | **Section H** allows the user to save the current value of the RDAC Register into the internal EEPROM. | + | Commands can be executed using a serial terminal connected |
- | ===== Troubleshooting ===== | + | The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. |
+ | {{ : | ||
- | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | + | ===== Software Project Setup ===== |
- | * Check that the evaluation board is powered as instructed in the board' | + | {{page> |
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols// | + | |
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | + | |
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |