This is an old revision of the document!
FMC-IMAGEON Xilinx Reference Design
Introduction
The FMC-IMAGEON is a HDMI input/output FMC card that provides high definition video interface for Xilinx FPGAs. The HDMI input interface is implemented with the ADV7611, a 165MHz, 24bit pixel output, HDCP capable HDMI 1.4a receiver. The HDMI output interface is implemented with the ADV7511, a 225MHz, 36bit deep color, HDMI 1.4 transmitter. This reference design provides the video and audio interface between the FPGA and ADV7511/ADV7611 on board. The video uses a 16bit 422 YCbCr interface and the audio uses a single bit SPDIF interface in both directions.
Supported Devices
Supported Carriers
Required Hardware
Required Software
We upgrade the Xilinx tools on every release. The supported version number can be found in our
git repository .
A
UART terminal (Tera Term/Hyperterminal), Baud rate 57600.
Using the reference design
Functional description
Xilinx block diagram
FMC-IMAGEON block diagram
The reference design consists of two independent IP modules.
The video part consists of an AXI DMAC interface and the ADV7511/ADV7611 video interface. The video interface consists of a 16bit YCbCr 422 with embedded synchronization signals.
Video Transmit (DMA to HDMI)
In the transmit direction, the DMA streams frame data to this core. The internal buffers of this IP are small (1k) and do NOT buffer any frames as such. Additional resources may cause loss of synchronization due to DDR bandwidth requirements. The video core is capable of supporting any formats through a set of parameter registers (given below). The pixel clock is generated internal to the device and must be configured for the correct pixel frequency. It also allows a programmable color pattern for debug purposes. A zero to one transition on the enable bits trigger the corresponding action for HDMI enable and color pattern enable.
The reference design defaults to the 1080p video mode. Users may change the video settings by programming the video size registers. The core requires a corresponding pixel clock to generate the video. This clock must be generated externally.
Note that the pixel frequency for 1080p is 148.5MHz.
The reference design reads 24bits of RGB data from DDR and performs color space conversion (RGB to YCbCr) and down sampling (444 to 422). If bypassed, the lower 16bits of DDR data is passed to the HDMI interface as it is.
A color pattern register provides a quick check of any RGB values on the monitor. If enabled, the register data is used as the pixel data for the entire frame.
Video Receive (HDMI to DMA)
In the receive direction, the HDMI data is first decoded and the synchronization signals are generated. The core then streams video data to DMA. The internal buffers of this IP are small (1k) and do NOT buffer any frames as such. Additional resources may cause loss of synchronization due to DDR bandwidth requirements. The video core is capable of supporting any formats through a set of parameter registers (given below). The core runs at the pixel clock from ADV7611.
The core decodes the active video size from the received data and compares it against an expected video size. If they do not match, the core will NOT stream data to DMA to avoid possible lock up conditions in the DMA core due to byte length mismatches. Also, the reference design performs color space conversion (YCbCr to RGB) and up sampling (422 to 444). If bypassed, the lower 16bits of DDR data is passed to the DMA interface as it is.
Test pattern generators and monitors are provided at each interface and clock domain boundaries. The default configuration is in loop back mode with the HDMI interface acting as a direct pass through.
Audio
The audio part consists of an AXI DMAC interface and the ADV7511 spdif audio interface. The audio clock is derived from the bus clock. A programmable register (see below) controls the division factor. The audio data is read from the DDR as two 16bit words for the left and right channels. It is then transmitted on the SPDIF frame. The sample frequency and format may be controlled using the registers below. The reference design defaults to 48KHz.
Registers
Base (common to all cores)
Click to expand regmap
Address | Bits | Name | Type | Default | Description |
DWORD | BYTE |
0x0000 | 0x0000 | REG_VERSION | Version and Scratch Registers |
| | [31:0] | VERSION[31:0] | RO | 0x00000000 | Version number. Unique to all cores. |
0x0001 | 0x0004 | REG_ID | Version and Scratch Registers |
| | [31:0] | ID[31:0] | RO | 0x00000000 | Instance identifier number. |
0x0002 | 0x0008 | REG_SCRATCH | Version and Scratch Registers |
| | [31:0] | SCRATCH[31:0] | RW | 0x00000000 | Scratch register. |
0x0003 | 0x000c | REG_CONFIG | Version and Scratch Registers |
| | [0] | IQCORRECTION_DISABLE | RO | 0x0 | If set, indicates that the IQ Correction module was not implemented. (as a result of a configuration of the IP instance) |
[1] | DCFILTER_DISABLE | RO | 0x0 | If set, indicates that the DC Filter module was not implemented. (as a result of a configuration of the IP instance) |
[2] | DATAFORMAT_DISABLE | RO | 0x0 | If set, indicates that the Data Format module was not implemented. (as a result of a configuration of the IP instance) |
[3] | USERPORTS_DISABLE | RO | 0x0 | If set, indicates that the logic related to the User Data Format (e.g. decimation) was not implemented. (as a result of a configuration of the IP instance) |
[4] | MODE_1R1T | RO | 0x0 | If set, indicates that the core was implemented in 1 channel mode. (e.g. refer to AD9361 data sheet) |
[5] | DELAY_CONTROL_DISABLE | RO | 0x0 | If set, indicates that the delay control is disabled for this IP. (as a result of a configuration of the IP instance) |
[6] | DDS_DISABLE | RO | 0x0 | If set, indicates that the DDS is disabled for this IP. (as a result of a configuration of the IP instance) |
[7] | CMOS_OR_LVDS_N | RO | 0x0 | CMOS or LVDS mode is used for the interface. (as a result of a configuration of the IP instance) |
[8] | PPS_RECEIVER_ENABLE | RO | 0x0 | If set, indicates the PPS receiver is enabled. (as a result of a configuration of the IP instance) |
[9] | SCALECORRECTION_ONLY | RO | 0x0 | If set, indicates that the IQ Correction module implements only scale correction. IQ correction must be enabled. (as a result of a configuration of the IP instance) |
[12] | EXT_SYNC | RO | 0x0 | If set the transport layer cores (ADC/DAC) have implemented the support for external synchronization signal. |
[13] | RD_RAW_DATA | RO | 0x0 | If set, the ADC has the capability to read raw data in register REG_CHAN_RAW_DATA from adc_channel. |
0x0004 | 0x0010 | REG_PPS_IRQ_MASK | PPS Interrupt mask |
| | [0] | PPS_IRQ_MASK | RW | 0x1 | Mask bit for the 1PPS receiver interrupt |
0x0007 | 0x001c | REG_FPGA_INFO | FPGA device information Intel encoded values Xilinx encoded values |
| | [31:24] | FPGA_TECHNOLOGY | RO | 0x0 | Encoded value describing the technology/generation of the FPGA device (arria 10/7series) |
[23:16] | FPGA_FAMILY | RO | 0x0 | Encoded value describing the family variant of the FPGA device(e.g., SX, GX, GT or zynq, kintex, virtex) |
[15:8] | SPEED_GRADE | RO | 0x0 | Encoded value describing the FPGA's speed-grade |
[7:0] | DEV_PACKAGE | RO | 0x0 | Encoded value describing the device package. The package might affect high-speed interfaces |
Tue Mar 14 10:17:59 2023 | |
HDMI Transmit (axi_hdmi_tx)
Click to expand regmap
Address | Bits | Name | Type | Default | Description |
DWORD | BYTE |
0x0010 | 0x0040 | REG_RSTN | HDMI Interface Control & Status |
| | [0] | RSTN | RW | 0x0 | Reset, a common reset is used for all the interface modules, The default is reset (0x0), software must write 0x1 to bring up the core. |
0x0011 | 0x0044 | REG_CNTRL1 | HDMI Interface Control & Status |
| | [2] | SS_BYPASS | RW | 0x0 | If set (0x1) bypasses the chroma sub-sampler. This is primarily intended to be used to send the test-pattern directly to the HDMI transmitter without modifying it. |
[1] | RESERVED | RO | 0x0 | Reserved |
[0] | CSC_BYPASS | RW | 0x0 | If set (0x1) bypasses color space conversion (if equipped). And depending on its value, the default value of color space boundaries is set in the REG_CLIPP_MAX and REG_CLIPP_MIN registers. |
0x0012 | 0x0048 | REG_CNTRL2 | HDMI Interface Control & Status |
| | [1:0] | SOURCE_SEL | RW | 0x0 | Select the HDMI data source- register constant (0x3), incr-pattern (0x2), input (0x1) or disabled (0x0). |
0x0013 | 0x004c | REG_CNTRL3 | HDMI Interface Control & Status |
| | [23:0] | CONST_RGB[23:0] | RW | 0x000000 | This is the RGB value transmitted, if the source is constant (see above). |
0x0015 | 0x0054 | REG_CLK_FREQ | HDMI Interface Control & Status |
| | [31:0] | CLK_FREQ[31:0] | RO | 0x00000000 | Interface clock frequency. This is relative to the processor clock and in many cases is 100MHz. The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock the minimum is 1.523kHz and maximum is 6.554THz. The actual interface clock is CLK_FREQ * CLK_RATIO (see below). Note that the actual sampling clock may not be the same as the interface clock- software must consider device specific implementation parameters to calculate the final sampling clock. |
0x0016 | 0x0058 | REG_CLK_RATIO | HDMI Interface Control & Status |
| | [31:0] | CLK_RATIO[31:0] | RO | 0x00000000 | Interface clock ratio - as a factor actual received clock. This is implementation specific and depends on any serial to parallel conversion and interface type (ddr/sdr/qdr). |
0x0017 | 0x005c | REG_STATUS | ADC Interface Control & Status |
| | [0] | STATUS | RO | 0x0 | Interface status, if set indicates no errors. If not set, there are errors, software may try resetting the cores. |
0x0018 | 0x0060 | REG_VDMA_STATUS | HDMI Interface Control & Status |
| | [1] | VDMA_OVF | RW1C | 0x0 | If set, indicates vdma overflow. |
[0] | VDMA_UNF | RW1C | 0x0 | If set, indicates vdma underflow. |
0x0019 | 0x0064 | REG_TPM_STATUS | HDMI Interface Control & Status |
| | [1] | HDMI_TPM_OOS | RW1C | 0x0 | If set, indicates TPM OOS at the HDMI interface. |
[0] | VDMA_TPM_OOS | RW1C | 0x0 | If set, indicates TPM OOS at the VDMA interface. |
0x001a | 0x0068 | REG_CLIPP_MAX | HDMI Interface Control & Status |
| | [23:16] | R_MAX/Cr_MAX | RW | 0xF0 | Defines the maximum value for clipping the red or red-difference chroma component. Default value are 0xf0 for red-difference chroma and 0xfe for red. |
[16:8] | G_MAX/Y_MAX | RW | 0xEB | Defines the maximum value for clipping the green or luma component. Default values are 0xeb for luma and and 0xfe for green. |
[7:0] | B_MAX/Cb_MAX | RW | 0xF0 | Defines the maximum value for clipping the blue or blue-difference chroma component. Default value are 0xf0 for blue-difference chroma and 0xfe for blue. |
0x001b | 0x006c | REG_CLIPP_MIN | HDMI Interface Control & Status |
| | [23:16] | R_MIN/Cr_MIN | RW | 0x10 | Defines the minimum value for clipping the red or red-difference chroma component. Default value are 0x10 for red-difference chroma and 0x01 for red. |
[16:8] | G_MIN/Y_MIN | RW | 0x10 | Defines the minimum value for clipping the green or luma component. Default values are 0x10 for luma and and 0x01 for green. |
[7:0] | B_MIN/Cb_MIN | RW | 0x10 | Defines the minimum value for clipping the blue or blue-difference chroma component. Default value are 0x10 for blue-difference chroma and 0x01 for blue. |
0x0100 | 0x0400 | REG_HSYNC_1 | HDMI Interface Control & Status |
| | [31:16] | H_LINE_ACTIVE[15:0] | RW | 0x0000 | This is the horizontal line active pixel width (active resolution length). e.g. 1920 (1080p) |
[15:0] | H_LINE_WIDTH[15:0] | RW | 0x0000 | This is the horizontal line width (no. of pixel clocks per line). e.g. 2200 (1080p) |
0x0101 | 0x0404 | REG_HSYNC_2 | HDMI Interface Control & Status |
| | [15:0] | H_SYNC_WIDTH[15:0] | RW | 0x0000 | This is the horizontal sync width (no. of pixel clocks). e.g. 44 (1080p) |
0x0102 | 0x0408 | REG_HSYNC_3 | HDMI Interface Control & Status |
| | [31:16] | H_ENABLE_MAX[15:0] | RW | 0x0000 | This is the horizontal data enable maximum. It is the sum of H_ENABLE_MIN and the active pixel width. e.g. 2112 (192 + 1920) (1080p) |
[15:0] | H_ENABLE_MIN[15:0] | RW | 0x0000 | This is the horizontal data enable minimum. It is the sum of horizontal back porch (number of clock cycles between the falling edge of HSYNC to the rising edge of DE) and the sync width. e.g. 192 (44 + 148) (1080p) |
0x0110 | 0x0440 | REG_VSYNC_1 | HDMI Interface Control & Status |
| | [31:16] | V_FRAME_ACTIVE[15:0] | RW | 0x0000 | This is the vertical frame active line width (active resolution height). e.g. 1080 (1080p) |
[15:0] | V_FRAME_WIDTH[15:0] | RW | 0x0000 | This is the vertical frame width (no. of lines per frame). e.g. 1125 (1080p) |
0x0111 | 0x0444 | REG_VSYNC_2 | HDMI Interface Control & Status |
| | [15:0] | V_SYNC_WIDTH[15:0] | RW | 0x0000 | This is the vertical sync width (no. of lines). e.g. 5 (1080p) |
0x0112 | 0x0448 | REG_VSYNC_3 | HDMI Interface Control & Status |
| | [31:16] | V_ENABLE_MAX[15:0] | RW | 0x0000 | This is the vertical data enable maximum. It is the sum of V_ENABLE_MIN and the active pixel height. e.g. 1121 (41 + 1080) (1080p) |
[15:0] | V_ENABLE_MIN[15:0] | RW | 0x0000 | This is the vertical data enable minimum. It is the sum of vertical back porch (number of lines between the falling edge of VSYNC to the rising edge of DE) and the sync width. e.g. 41 (36 + 5) (1080p) |
Tue Mar 14 10:17:59 2023 | |
HDMI Receive (axi_hdmi_rx)
Click to expand regmap
Address | Bits | Name | Type | Default | Description |
DWORD | BYTE |
0x0010 | 0x0040 | REG_RSTN | HDMI Interface Control & Status |
| | [0] | RSTN | RW | 0x0 | Reset, a common reset is used for all the interface modules, The default is reset (0x0), software must write 0x1 to bring up the core. |
0x0011 | 0x0044 | REG_CNTRL | HDMI Interface Control & Status |
| | [3] | EDGE_SEL | RW | 0x0 | If set (0x1), incoming data is registered on the falling edge of the clock first. The default uses rising edge. |
[2] | BGR | RW | 0x0 | If set (0x1), output BGR. The default is RGB. |
[1] | PACKED | RW | 0x0 | If set (0x1) pack 24bit RGB data on 32bit dwords. The default pads the MSB to zeros. |
[0] | CSC_BYPASS | RW | 0x0 | If set (0x1) bypasses color space conversion (if equipped). |
0x0015 | 0x0054 | REG_CLK_FREQ | HDMI Interface Control & Status |
| | [31:0] | CLK_FREQ[31:0] | RO | 0x00000000 | Interface clock frequency. This is relative to the processor clock and in many cases is 100MHz. The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock the minimum is 1.523kHz and maximum is 6.554THz. The actual interface clock is CLK_FREQ * CLK_RATIO (see below). Note that the actual sampling clock may not be the same as the interface clock- software must consider device specific implementation parameters to calculate the final sampling clock. |
0x0016 | 0x0058 | REG_CLK_RATIO | HDMI Interface Control & Status |
| | [31:0] | CLK_RATIO[31:0] | RO | 0x00000000 | Interface clock ratio - as a factor actual received clock. This is implementation specific and depends on any serial to parallel conversion and interface type (ddr/sdr/qdr). |
0x0018 | 0x0060 | REG_VDMA_STATUS | HDMI Interface Control & Status |
| | [1] | VDMA_OVF | RW1C | 0x0 | If set, indicates vdma overflow. |
[0] | VDMA_UNF | RW1C | 0x0 | If set, indicates vdma underflow. |
0x0019 | 0x0064 | REG_TPM_STATUS1 | HDMI Interface Control & Status |
| | [1] | HDMI_TPM_OOS | RW1C | 0x0 | If set, indicates TPM OOS at the HDMI interface. |
0x0020 | 0x0080 | REG_TPM_STATUS2 | HDMI Interface Control & Status |
| | [3] | VS_OOS | RW1C | 0x0 | If set, indicates VSYNC OOS - the core is unabled to detect/track VSYNC. Consecutive frames have different number of lines. |
[2] | HS_OOS | RW1C | 0x0 | If set, indicates HSYNC OOS - the core is unabled to detect/track HSYNC. Consecutive lines have different lengths. |
[1] | VS_MISMATCH | RW1C | 0x0 | If set, indicates received (detected) & programmed VSYNC (number of lines) mismatch. Incoming frames are stable but not the expected resolution. |
[0] | HS_MISMATCH | RW1C | 0x0 | If set, indicates received (detected) & programmed HSYNC (number of pixels) mismatch. Incoming frames are stable but not the expected resolution. |
0x0100 | 0x0400 | REG_HVCOUNTS1 | HDMI Interface Control & Status |
| | [31:16] | VS_COUNT[15:0] | RW | 0x0000 | This is the expected active horizontal pixel lines (active resolution length). e.g. 1080 (1080p) |
[15:0] | HS_COUNT[15:0] | RW | 0x0000 | This is the expected horizontal pixel count (no. of pixel clocks per line). e.g. 1920 (1080p) |
0x0101 | 0x0404 | REG_HVCOUNTS2 | HDMI Interface Control & Status |
| | [31:16] | VS_COUNT[15:0] | RO | 0x0000 | This is the detected horizontal active pixel lines (active resolution length). This field is valid only if VS_OOS is zero. |
[15:0] | HS_COUNT[15:0] | RO | 0x0000 | This is the detected horizontal pixel count (no. of pixel clocks per line). This field is valid only if HS_OOS is zero. |
Tue Mar 14 10:17:59 2023 | |
Audio Registers (axi_spdif_tx)
QW Address1 | Bits | Default | Name | Description |
0x00 | 23:20 | 0 | mode | Sample format 0 to 8 (0-16bit, 8-24bit). |
| 15:8 | 0 | ratio | Clock divider for the transmit frequency = bus_clock/(1+ratio). |
| 1 | 0 | txdata | Transmit data buffer enable (0x1) or disable (0x0). |
| 0 | 0 | txenable | Transmitter enable (0x1) or disable (0x0). |
0x01 | 7:6 | 0 | frequency | Sample frequency 0(44.1KHz), 1(48KHz), 2(32KHz) or 3(sample rate converter) (RO). |
| 3 | 0 | gstat | Generation status original/commercially pre-recorded data (0x1) or none (0x0) (RO). |
| 2 | 0 | pre-emphasis | Pre-emphasis 50/15s (0x1) or none (0x0) (RO). |
| 1 | 0 | copy | Copy permitted (0x1) or inhibited (0x0) (RO). |
| 0 | 0 | audio | Data format is non-audio (0x1) or audio (0x0) (RO). |
1. For AXI-Lite byte addresses, multiply by 4. |
Using the ADV7511 Transmitter Library
The transmitter library is a collection of APIs that provide a consistent interface to ADV7511.
The library is a software layer that sits between the application and the TX hardware. The library is intended to serve two purposes:
Provide the application with a set of APIs that can be used to configure HDMI TX hardware without the need for low-level register access. This makes the application portable across different revisions of the hardware and even across different hardware modules.
Provide basic services to aid the application in controlling the TX module, such as interrupt service routine, HDCP high-level control and status information.
The Demo project uses the ADV7511 Transmitter Library.
The project is an example of how to:
Initialize the ADV7511 High-Definition Multimedia Interface (HDMI®) transmitter.
Check current AVR operating mode and depending on this result set the AV mute state.
Display an image and play a sound.
The project contains 2 components: the Demo project files and the ADV7511 Transmitter Library. All the components have to be downloaded from the links provided in the Downloads section.
Software Setup
The ADV7511 Transmitter Library Demo contains a folder called SDK_Workspace which stores the Xilinx SDK project files needed to build the no-OS software and also the .bit files with the HDL design that must be programmed into the FPGA.
These are the steps that need to be followed to recreate the software project:
Open the Xilinx SDK. When the SDK starts it asks for a to provide a folder where to store the workspace. Any folder can be provided.
In the SDK select the File→Import menu option to import the software projects into the workspace.
Downloads
ADV7511 Transmitter Library Demo Software
Help & Support
-
The
HDL user guide contains all the documentation, build instructions and register map tables.
-
-