This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:fmc:fmc-imageon [29 Sep 2017 09:34] – [Supported Carriers] Added FMC slot specification Adrian Costina | resources:fpga:xilinx:fmc:fmc-imageon [20 Dec 2023 12:02] (current) – Add obsolesce notice Stefan-Robert Raus | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== FMC-IMAGEON Xilinx Reference Design ====== | ====== FMC-IMAGEON Xilinx Reference Design ====== | ||
+ | <note warning> | ||
+ | Support for the fmc-imageon is discontinued starting with 2022_r2 Kuiper Linux release and it will not be supported in future releases. Last Kuiper Linux release that contains pre-build files is 2021_r2. Check this [[: | ||
+ | </ | ||
+ | |||
===== Introduction ===== | ===== Introduction ===== | ||
Line 11: | Line 15: | ||
===== Supported Carriers ===== | ===== Supported Carriers ===== | ||
- | * [[xilinx> | ||
* [[http:// | * [[http:// | ||
- | |||
Line 25: | Line 27: | ||
* We upgrade the Xilinx tools on every release. The supported version number can be found in our [[https:// | * We upgrade the Xilinx tools on every release. The supported version number can be found in our [[https:// | ||
* A UART terminal (Tera Term/ | * A UART terminal (Tera Term/ | ||
- | |||
- | |||
- | |||
- | |||
===== Using the reference design ===== | ===== Using the reference design ===== | ||
Line 34: | Line 32: | ||
==== Functional description ==== | ==== Functional description ==== | ||
- | |{{.:cf_adv7x11_bd.jpg?200|Block Diagram}} | + | === Xilinx block diagram === |
+ | {{resources:fpga: | ||
- | The reference design consists of two independent pcore modules. | + | === FMC-IMAGEON block diagram === |
+ | {{resources: | ||
- | The video part consists of a Xilinx VDMA interface and the ADV7511/ | + | The reference design |
- | ==== Video Transmit (VDMA to HDMI) ==== | + | The video part consists of an AXI DMAC interface and the ADV7511/ |
- | In the transmit direction, the VDMA streams frame data to this core. The internal buffers of this pcore are small (1k) and do NOT buffer any frames as such. Additional resources may cause loss of synchronization due to DDR bandwidth requirements. The video core is capable of supporting any formats through a set of parameter registers (given below). The pixel clock is generated internal to the device and must be configured for the correct pixel frequency. It also allows a programmable color pattern for debug purposes. A zero to one transition on the enable bits trigger the corresponding action for HDMI enable and color pattern enable. | + | ==== Video Transmit (DMA to HDMI) ==== |
+ | |||
+ | In the transmit direction, the DMA streams frame data to this core. The internal buffers of this IP are small (1k) and do NOT buffer any frames as such. Additional resources may cause loss of synchronization due to DDR bandwidth requirements. The video core is capable of supporting any formats through a set of parameter registers (given below). The pixel clock is generated internal to the device and must be configured for the correct pixel frequency. It also allows a programmable color pattern for debug purposes. A zero to one transition on the enable bits trigger the corresponding action for HDMI enable and color pattern enable. | ||
The reference design defaults to the 1080p video mode. Users may change the video settings by programming the video size registers. The core requires a corresponding pixel clock to generate the video. This clock must be generated externally. | The reference design defaults to the 1080p video mode. Users may change the video settings by programming the video size registers. The core requires a corresponding pixel clock to generate the video. This clock must be generated externally. | ||
Line 52: | Line 54: | ||
A color pattern register provides a quick check of any RGB values on the monitor. If enabled, the register data is used as the pixel data for the entire frame. | A color pattern register provides a quick check of any RGB values on the monitor. If enabled, the register data is used as the pixel data for the entire frame. | ||
- | ==== Video Receive (HDMI to VDMA) ==== | + | ==== Video Receive (HDMI to DMA) ==== |
- | In the receive direction, the HDMI data is first decoded and the synchronization signals are generated. The core then streams video data to VDMA. The internal buffers of this pcore are small (1k) and do NOT buffer any frames as such. Additional resources may cause loss of synchronization due to DDR bandwidth requirements. The video core is capable of supporting any formats through a set of parameter registers (given below). The core runs at the pixel clock from ADV7611. | + | In the receive direction, the HDMI data is first decoded and the synchronization signals are generated. The core then streams video data to DMA. The internal buffers of this IP are small (1k) and do NOT buffer any frames as such. Additional resources may cause loss of synchronization due to DDR bandwidth requirements. The video core is capable of supporting any formats through a set of parameter registers (given below). The core runs at the pixel clock from ADV7611. |
- | The core decodes the active video size from the received data and compares it against an expected video size. If they do not match, the core will NOT stream data to VDMA to avoid possible lock up conditions in the VDMA core due to byte length mismatches. Also, the reference design performs color space conversion (YCbCr to RGB) and up sampling (422 to 444). If bypassed, the lower 16bits of DDR data is passed to the VDMA interface as it is. | + | The core decodes the active video size from the received data and compares it against an expected video size. If they do not match, the core will NOT stream data to DMA to avoid possible lock up conditions in the DMA core due to byte length mismatches. Also, the reference design performs color space conversion (YCbCr to RGB) and up sampling (422 to 444). If bypassed, the lower 16bits of DDR data is passed to the DMA interface as it is. |
Test pattern generators and monitors are provided at each interface and clock domain boundaries. The default configuration is in loop back mode with the HDMI interface acting as a direct pass through. | Test pattern generators and monitors are provided at each interface and clock domain boundaries. The default configuration is in loop back mode with the HDMI interface acting as a direct pass through. | ||
Line 62: | Line 64: | ||
==== Audio ==== | ==== Audio ==== | ||
- | The audio part consists of a Xilinx DMA interface and the ADV7511 spdif audio interface. The audio clock is derived from the bus clock. A programmable register (see below) controls the division factor. The audio data is read from the DDR as two 16bit words for the left and right channels. It is then transmitted on the SPDIF frame. The sample frequency and format may be controlled using the registers below. The reference design defaults to 48KHz. | + | The audio part consists of an AXI DMAC interface and the ADV7511 spdif audio interface. The audio clock is derived from the bus clock. A programmable register (see below) controls the division factor. The audio data is read from the DDR as two 16bit words for the left and right channels. It is then transmitted on the SPDIF frame. The sample frequency and format may be controlled using the registers below. The reference design defaults to 48KHz. |
==== Registers ==== | ==== Registers ==== | ||
- | Please refer to the regmap.txt file inside the pcores. | + | {{page>: |
+ | |||
+ | {{page>: | ||
+ | |||
+ | {{page>: | ||
==== Audio Registers (axi_spdif_tx) ==== | ==== Audio Registers (axi_spdif_tx) ==== | ||
Line 81: | Line 87: | ||
| | 0 | 0 | audio | Data format is non-audio (0x1) or audio (0x0) (RO). | | | | 0 | 0 | audio | Data format is non-audio (0x1) or audio (0x0) (RO). | | ||
| 1. For AXI-Lite byte addresses, multiply by 4. ||||| | | 1. For AXI-Lite byte addresses, multiply by 4. ||||| | ||
- | |||
===== Using the ADV7511 Transmitter Library ===== | ===== Using the ADV7511 Transmitter Library ===== | ||
Line 115: | Line 120: | ||
* In the //Import Projects// window select the // | * In the //Import Projects// window select the // | ||
{{: | {{: | ||
- | * The //Project Explorer// window now shows the projects that exist in the workspace and the files for each project. The SDK should automatically build the projects and the //Console// window will display | + | * The //Project Explorer// window now shows the projects that exist in the workspace and the files for each project. The SDK should automatically build the projects and the //Console// window will display the result of the build. If the build is not done automatically select the // |
{{: | {{: | ||
- | |||
===== Downloads ===== | ===== Downloads ===== | ||
Line 123: | Line 127: | ||
**HDL Reference Designs:** | **HDL Reference Designs:** | ||
- | <WRAP round download 80%> | + | {{page>resources/fpga/ |
- | * **ML605: ** {{:resources:fpga: | + | |
- | * **Zed: ** {{: | + | |
- | * **ADV7511 Transmitter Library Demo: ** {{: | + | |
- | </ | + | |
**ADV7511 Transmitter Library Demo Software** | **ADV7511 Transmitter Library Demo Software** | ||
<WRAP round download 80%> | <WRAP round download 80%> | ||
\\ | \\ | ||
- | * **ADV7511 Transmitter Library: ** https://github.com/analogdevicesinc/no-OS/tree/master/ | + | * **ADV7511 Transmitter Library: ** https://www.analog.com/media/en/dsp-hardware-software/software-modules/ADV7511_API_Library.exe\\ |
- | * **ADV7511 Transmitter Library Demo files: ** https:// | + | * **ADV7511 Transmitter Library Demo files: ** https:// |
</ | </ | ||
- | <WRAP round help 80%> | + | {{page>resources/fpga/docs/hdl/downloads_insert# |
- | * Questions? [[https:// | + | |
- | </WRAP> | + | |
- | + | ||
- | + | ||
- | ===== Tar file contents ===== | + | |
- | + | ||
- | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[http:// | + | |
- | + | ||
- | | license.txt | ADI license & copyright information. | | + | |
- | | system.mhs | + | |
- | | system.xmp | + | |
- | | data/ | UCF file and/or DDR MIG project files. | | + | |
- | | docs/ | Documentation files (Please note that this wiki page is the documentation for the reference design). | | + | |
- | | sw/ | Software (Xilinx SDK) & bit file(s). | | + | |
- | | cf_lib/ | + | |