This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:xilinx:fmc:ad9467 [03 Jan 2021 22:12] – fix links Robin Getz | resources:fpga:xilinx:fmc:ad9467 [09 Jan 2021 00:39] – user interwiki links Robin Getz | ||
---|---|---|---|
Line 23: | Line 23: | ||
<WRAP round important 100%> | <WRAP round important 100%> | ||
\\ | \\ | ||
- | Please make sure you have removed or inserted the corresponding components on the board to select the desired clock path. The schematic of the board can be found at the [[http:// | + | Please make sure you have removed or inserted the corresponding components on the board to select the desired clock path. The schematic of the board can be found at the [[/ |
</ | </ | ||
Line 37: | Line 37: | ||
==== Required Software ==== | ==== Required Software ==== | ||
- | * We're upgrade the Xilinx tools on every release. The supported version number can be found in our HDL [[https:// | + | * We're upgrade the Xilinx tools on every release. The supported version number can be found in our HDL [[/ |
* A UART terminal (Tera Term/ | * A UART terminal (Tera Term/ | ||
Line 43: | Line 43: | ||
<WRAP round info 100%> | <WRAP round info 100%> | ||
- | Instruction about how to build the HDL design and generate a bit stream can be found [[https:// | + | Instruction about how to build the HDL design and generate a bit stream can be found [[/ |
</ | </ | ||
Line 75: | Line 75: | ||
* Capture data from the AD9467 using DMA transfers | * Capture data from the AD9467 using DMA transfers | ||
- | The software project contains 3 components: the AD9467-FMC-EBZ reference design files, the AD9467 driver and the AD9517 driver. All the components have to be downloaded from the links provided in the [[http:// | + | The software project contains 3 components: the AD9467-FMC-EBZ reference design files, the AD9467 driver and the AD9517 driver. All the components have to be downloaded from the links provided in the [[/ |
==== AD9467 Software Driver ==== | ==== AD9467 Software Driver ==== | ||
Line 109: | Line 109: | ||
<WRAP round info 100%> | <WRAP round info 100%> | ||
- | Instruction about how to create a software application can be found [[http:// | + | Instruction about how to create a software application can be found [[/ |
</ | </ | ||
- | The exact location of the no-OS source files can be found in the [[http:// | + | The exact location of the no-OS source files can be found in the [[/ |
| | ||
===== Downloads ===== | ===== Downloads ===== |