This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:fpga:xilinx:fmc:ad7961 [07 Aug 2013 14:32] – [Data Capture] Alexandru.Tofan | resources:fpga:xilinx:fmc:ad7961 [25 Jan 2021 19:33] (current) – update renesas links after their web site update Robin Getz | ||
---|---|---|---|
Line 30: | Line 30: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <WRAP round tip 80%>If you are not familiar with KC705 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/ | + | <WRAP round tip 80%>If you are not familiar with KC705 and/or Xilix tools, please visit\\ [[xilinx>products/ |
</ | </ | ||
Extract the project from the archive file to the location you desire. | Extract the project from the archive file to the location you desire. | ||
Line 46: | Line 46: | ||
==== FPGA Configuration ==== | ==== FPGA Configuration ==== | ||
- | Start IMPACT, and initialze the JTAG chain. The program should recognize the FPGA device. Program the device. | + | Start IMPACT, and initialze the JTAG chain. The program should recognize the FPGA device. Program the device |
{{: | {{: | ||
Line 52: | Line 52: | ||
==== Data Capture ==== | ==== Data Capture ==== | ||
- | After successfully programming | + | At this point everything is set up and it is possible to start the evaluation of the ADI hardware. To capture data from the ADC run the **data_capture.bat** script located in the **" |
- | {{: | + | Data Capture Script\\ |
+ | {{: | ||
- | After data has been read from the device, | + | Acquisition.csv\\ |
+ | {{: | ||
+ | |||
+ | UART Messages\\ | ||
+ | {{: | ||
+ | |||
+ | <WRAP round tip 80%>The first time the data capture script is run it is possible that an error will occur while the script is trying to connect to the system. Just run the script again and the error shouldn' | ||
- | {{: | ||
===== Using the reference design ===== | ===== Using the reference design ===== | ||
Line 66: | Line 72: | ||
The reference design is built on a Microblaze based system. It consists of two functional modules, a LVDS interface, and a DMA interface. The LVDS interface captures and buffers data from the ADC. The data is captured using Echoed-Clock mode or Self-Clock mode (depending on the project). The DMA interface then transfers the samples to the external DDR-DRAM. The capture is initiated by the software, and transfered to the PC using a *.tcl script. | The reference design is built on a Microblaze based system. It consists of two functional modules, a LVDS interface, and a DMA interface. The LVDS interface captures and buffers data from the ADC. The data is captured using Echoed-Clock mode or Self-Clock mode (depending on the project). The DMA interface then transfers the samples to the external DDR-DRAM. The capture is initiated by the software, and transfered to the PC using a *.tcl script. | ||
- | ==== Registers ==== | ||
- | |||
- | The IP Core contains only a control register, that sets/clears the EN pins of the device. | ||
===== Downloads ===== | ===== Downloads ===== | ||
Line 82: | Line 85: | ||
<WRAP round help 80%> | <WRAP round help 80%> | ||
- | * Questions? [[http://ez.analog.com/ | + | * Questions? [[ez>fpga|Ask Help & Support]]. |
</ | </ | ||
===== Zip file contents ===== | ===== Zip file contents ===== | ||
- | The zip file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[http://www.xilinx.com/support/ | + | The zip file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[xilinx>support/ |
| Bit | The bitfile required for Quick Evaluation | | | Bit | The bitfile required for Quick Evaluation | |