This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:xilinx:fmc:ad-fmcjesdadc1-ebz [16 Apr 2014 13:16] – [Supported Carriers] Robin Getz | resources:fpga:xilinx:fmc:ad-fmcjesdadc1-ebz [29 Apr 2014 20:12] – [Running Demo (SDK) Program] rejeesh kutty | ||
---|---|---|---|
Line 49: | Line 49: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
+ | |||
+ | Please Note: For Zynq devices, programming the bit file alone is not sufficient. You need to initialize PS7 and run the elf. Run the provided tcl script (sw/ | ||
+ | |||
+ | Example: xmd -tcl sw/ | ||
+ | |||
To begin make the following connections (see image below): | To begin make the following connections (see image below): |