Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:fpga:xilinx:fmc:ad-fmcadc3-ebz [11 Nov 2016 09:47] – [Required Software] syntax error Lucian Sin | resources:fpga:xilinx:fmc:ad-fmcadc3-ebz [03 Aug 2018 17:56] – The design no longer uses the Xilinx IP Lars-Peter Clausen |
---|
| |
===== Introduction ===== | ===== Introduction ===== |
| |
<WRAP important round>This design uses the [[http://www.xilinx.com/products/intellectual-property/EF-DI-JESD204.htm|Xilinx JESD204B core]] which requires either a commercial (pay $) or [[http://www.xilinx.com/ipcenter/ipevaluation/jesd204_evaluation.htm|evaluation]] license (eventually pay $) to use. If this is not what you are looking for, you should not use this board.</WRAP> | |
| |
The [[adi>EVAL-AD-FMCADC3-EBZ|AD-FMCADC3-EBZ]] is a high speed data acquisition board featuring [[adi>AD9625]] single channel ADC at 2500 MSPS and the ADA4961 [[adi>ADA4961]] Low Distortion, 3.2 GHz, RF DGA driving the converter. The FMC form factor supports the JESD204B high speed serial interface. This board meets most of the FMC specifications in terms of mechanical size, mounting hole locations, and more. For that information, please refer to the FMC specification. | The [[adi>EVAL-AD-FMCADC3-EBZ|AD-FMCADC3-EBZ]] is a high speed data acquisition board featuring [[adi>AD9625]] single channel ADC at 2500 MSPS and the ADA4961 [[adi>ADA4961]] Low Distortion, 3.2 GHz, RF DGA driving the converter. The FMC form factor supports the JESD204B high speed serial interface. This board meets most of the FMC specifications in terms of mechanical size, mounting hole locations, and more. For that information, please refer to the FMC specification. |