Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:fpga:peripherals:spi_engine [11 May 2018 11:21] – [Tutorial] remove tutorial section for now Lars-Peter Clausen | resources:fpga:peripherals:spi_engine [22 Dec 2022 13:07] (current) – remove broken backlinks sergiu arpadi |
---|
| |
The core component of the SPI Engine framework is a lean but powerful fully programmable execution module, which implements the SPI bus control logic. The SPI Engine execution module is controlled by a command stream which is generated by a separate module. Different command stream master modules are available and can be used depending on the system requirements. For example a software controlled memory mapped command stream offers high flexibility, while a offload core which executes a pre-programmed command stream when triggered by an external event allows for very low latency response times. By using a SPI Engine interconnect it is possible to connect multiple command stream master modules to a SPI Engine execution module. | The core component of the SPI Engine framework is a lean but powerful fully programmable execution module, which implements the SPI bus control logic. The SPI Engine execution module is controlled by a command stream which is generated by a separate module. Different command stream master modules are available and can be used depending on the system requirements. For example a software controlled memory mapped command stream offers high flexibility, while a offload core which executes a pre-programmed command stream when triggered by an external event allows for very low latency response times. By using a SPI Engine interconnect it is possible to connect multiple command stream master modules to a SPI Engine execution module. |
| |
| |
===== Sub-modules ===== | ===== Sub-modules ===== |
* [[.:spi_engine:offload|Offload Module]]: Stores a SPI Engine command stream, execution is triggered by an external event | * [[.:spi_engine:offload|Offload Module]]: Stores a SPI Engine command stream, execution is triggered by an external event |
* [[.:spi_engine:interconnect|Interconnect Module]]: Connects multiple SPI Engine command streams to a SPI Engine execution module | * [[.:spi_engine:interconnect|Interconnect Module]]: Connects multiple SPI Engine command streams to a SPI Engine execution module |
| |
| |
===== Interfaces ===== | ===== Interfaces ===== |
* [[.:spi_engine:spi_engine_offload_control_interface|SPI Engine Offload Control Interface]]: Program the command stream stored in a offload module | * [[.:spi_engine:spi_engine_offload_control_interface|SPI Engine Offload Control Interface]]: Program the command stream stored in a offload module |
* [[.:spi_engine:spi_bus_interface|SPI Bus Interface]]: Low-level SPI bus interface | * [[.:spi_engine:spi_bus_interface|SPI Bus Interface]]: Low-level SPI bus interface |
| |
| |
===== Software ===== | ===== Software ===== |
| |
* [[resources:tools-software:linux-drivers:spi:spi_engine|Linux Driver]]: Linux driver for the SPI Engine framework | * [[resources:tools-software:linux-drivers:spi:spi_engine|Linux Driver]]: Linux driver for the SPI Engine framework |
* [[resources:tools-software:uc-drivers:spi_engine|No-OS bare-metal Driver]]: No-OS bare-metal driver | * [[.:spi_engine:instruction_format|SPI Engine Instruction Format]]: Overview of the SPI Engine Instruction format |
* [[SPI Engine Compiler]]: Compiler for generating SPI Engine bytecode | |
* [[.:spi_engine:instruction_format|SPI Engine Instruction Format]]: Overview of the SPI Engine Instruction format | |
| |
| |
| |
* [[util_sigma_delta_spi|Sigma-Delta SPI Util]]: Helper module for interfacing ADCs from the Analog Devices Sigma-Delta family | * [[util_sigma_delta_spi|Sigma-Delta SPI Util]]: Helper module for interfacing ADCs from the Analog Devices Sigma-Delta family |
| |
| |
===== Examples ===== | ===== Examples ===== |
| |
* [[resources:eval:user-guides:eval-cn0363-pmdz|CN0363]] - Colorimeter application using the [[adi>AD7175-2]] Sigma-Delta ADC | * [[resources:eval:user-guides:eval-cn0363-pmdz|CN0363]] - Colorimeter application using the [[adi>AD7175-2]] Sigma-Delta ADC |
| * [[resources:eval:user-guides:adaq7980-sdz]] - A 16-bit ADC subsystem with four common signal processing and conditioning blocks. |
| * [[resources:tools-software:uc-drivers:ad5766]] - 16-channel, 16-/12-bit, voltage output Digital-to-Analog Converters (DAC) |
| * [[resources:eval:user-guides:ad7768-1]] - The AD7768-1 is a low power, high performance, Σ-Δ analog-to-digital converter (ADC). |
| * [[https://github.com/analogdevicesinc/hdl/tree/master/projects/ad40xx_fmc|AD40xx-FMC]] - Evaluation Board for the AD4000 Series 16-/18-/20-Bit Precision SAR ADCs |
| * [[:resources:eval:user-guides:ad469x|AD469x]] - 16-Bit, 16-Channel, 500 kSPS/1 MSPS, Easy Drive Multiplexed SAR ADC |
| * [[:resources:eval:user-guides:ad463x:hdl|AD4630-24 / AD4030-24 / AD4630-16]] - 16/24-Bit, 2 MSPS Single or Dual Channel SAR ADC |
| |
===== Additional Documents ===== | ===== Additional Resources ===== |
| |
* {{:resources:fpga:peripherals:spi-engine3.pdf|Presentation: SPI Engine Design Philosophy}} | * {{:resources:fpga:peripherals:spi-engine3.pdf|Presentation: SPI Engine Design Philosophy}} |
| * [[:resources:fpga:peripherals:spi_engine:tutorial|PulSAR ADC Tutorial]] |
| |
| {{navigation HDL User Guide#../docs/ip_cores|IP cores#../docs/hdl|Main page#../docs/tips|Using and modifying the HDL design}} |