This is an old revision of the document!
The SPI Engine Control Interface is used to exchange data between different cores within the SPI Engine framework. It is used to exchange the commands and synchronization points as well as the SPI bus transmit and receive data.
The interface consists of four streams:
Each of the streams has a valid, ready and data signal. They follow the handshaking protocol as defined by the AXI standard. Meaning the master asserts valid when the data on the data signal is valid and the slave asserts ready when it is able to accept new data. If both valid and ready are asserted at the same time the data has been transmitted from the master to the slave.
Name | Direction (Master) | Description | |
---|---|---|---|
cmd_ready | Input | Ready signal of the CMD stream | |
cmd_valid | Output | Valid signal of the CMD stream | |
[15:0] | cmd_data | Output | Data signal of the CMD stream |
sdo_ready | Input | Ready signal of the SDO stream | |
sdo_valid | Output | Valid signal of the SDO stream | |
[7:0] | sdo_data | Output | Data signal of the SDO stream |
sdi_ready | Output | Ready signal of the SDI stream | |
sdi_valid | Input | Valid signal of the SDI stream | |
[7:0] | sdi_data | Input | Data signal of the SDI stream |
sync_ready | Output | Ready signal of the SYNC stream | |
sync_valid | Input | Valid signal of the SYNC stream | |
[7:0] | sync_data | Input | Data signal of the sync stream |