This is an old revision of the document!
The SPI bus interface carries logical low-level SPI bus signals.
Name | Description |
---|---|
spi_master_rtl.xml | Interface definition file |
Name | Direction (Master) | Description |
---|---|---|
sclk | Output | SPI Clock. |
sdo | Output | SPI SDO (MOSI) signal. |
sdo_t | Output | sdo tri-state enable. If 1 the MOSI signal should be tristated and not be connected to sdo |
sdi | Input | SPI SDI (MISO) signal. |
cs | Output | SPI chip-select signal. |
three_wire | Output | If set to 1 the bus should operate in three-wire mode. In three-wire mode sdi is connected to MOSI instead of MISO. |
The SPI bus interface only carries a logical representation of the low-level SPI bus signals. The top-level module in the FPGA design project is responsible for translating the signal to physical SPI bus signals by instantiating and connecting it to appropriate IO primitives.
The sclk
and cs
signals can typically be directly connected to a output buffer. sdi
should be connected to a mux, that depending on the setting of the three_wire
signal connects to a input buffer connected to the miso
signal or to a input buffer connected to the mosi
signal. The sdo
signal should be connected to a output tri-state buffer with the sdo_t
signal controlling the tri-state setting.
In some configurations three-wire support may not be required and sdi
can directly be connected to the input buffer for the miso
signal. Similarly when mosi
tri-stating is not required the sdo
signal can be directly connected to the mosi
signal leaving the sdo_t
signal unconnected.