Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:fpga:peripherals:spi_engine:spi_bus_interface [30 Mar 2015 17:41] – [Signal Pins] Lars-Peter Clausen | resources:fpga:peripherals:spi_engine:spi_bus_interface [11 May 2018 17:42] (current) – [Files] Switch to master branch Istvan Csomortani |
---|
====== SPI Bus Interface ====== | ====== SPI Bus Interface ====== |
| |
The SPI Bus Interface carries logical low-level SPI bus signals. | The SPI bus interface carries logical low-level SPI bus signals. |
| |
| ===== Files ===== |
| |
| ^ Name ^ Description ^ |
| | [[github>hdl?master/library/spi_engine/interfaces/spi_master_rtl.xml|spi_master_rtl.xml]] | Interface definition file | |
===== Signal Pins ===== | ===== Signal Pins ===== |
| |
| ''sdo'' | Output | SPI SDO (MOSI) signal. | | | ''sdo'' | Output | SPI SDO (MOSI) signal. | |
| ''sdo_t'' | Output | ''sdo'' tri-state enable. If 1 the MOSI signal should be tristated and not be connected to ''sdo'' | | | ''sdo_t'' | Output | ''sdo'' tri-state enable. If 1 the MOSI signal should be tristated and not be connected to ''sdo'' | |
| ''sdi'' | Input | SPI SDI (MISO) signal. | | | ''sdi'' | Input | SPI SDI (MISO) signal. Execution module supports max 8 individual ''sdi'' lines. | |
| ''cs'' | Output | SPI chip-select signal. | | | ''cs'' | Output | SPI chip-select signal. | |
| ''three_wire'' | Output | If set to 1 the bus should operate in three-wire mode. In three-wire mode ''sdi'' is connected to MOSI instead of MISO. | | | ''three_wire'' | Output | If set to 1 the bus should operate in three-wire mode. In three-wire mode ''sdi'' is connected to MOSI instead of MISO. | |
| |
In some configurations three-wire support may not be required and ''sdi'' can directly be connected to the input buffer for the ''miso'' signal. Similarly when ''mosi'' tri-stating is not required the ''sdo'' signal can be directly connected to the ''mosi'' signal leaving the ''sdo_t'' signal unconnected. | In some configurations three-wire support may not be required and ''sdi'' can directly be connected to the input buffer for the ''miso'' signal. Similarly when ''mosi'' tri-stating is not required the ''sdo'' signal can be directly connected to the ''mosi'' signal leaving the ''sdo_t'' signal unconnected. |
| |
| ==== Example Verilog IO configuration ==== |
| |
| The following example Verilog code shows the most generic IO configuration, which represents the diagram above. Depending on system requirements some simplification might be possible. |
| |
| Signals with **phy** prefix are assumed to be connected to the physical input/output pins and signals with the **spi** prefix are assumed to be connected SPI-Engine bus interface. |
| |
| <code verilog> |
| assign phy_sclk = spi_sclk; |
| assign phy_cs = spi_cs; |
| assign phy_mosi = spi_sdo_t ? 1'bz : spi_sdo; |
| assign spi_sdi = spi_three_wire ? phy_mosi : phy_miso; |
| </code> |
| |
| |
===== More Information ===== | ===== More Information ===== |
* [[.|SPI Engine Framework]] | * [[.|SPI Engine Framework]] |