Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:fpga:peripherals:spi_engine:interconnect [11 May 2018 17:47] – [Files] Switch to master Istvan Csomortaniresources:fpga:peripherals:spi_engine:interconnect [04 Sep 2019 12:47] (current) – Add configuration parameters, fix some grammar mistakes Istvan Csomortani
Line 3: Line 3:
 {{ :resources:fpga:peripherals:spi_engine:spi_engine_interconnect.png|}} {{ :resources:fpga:peripherals:spi_engine:spi_engine_interconnect.png|}}
  
-The SPI Engine Interconnect module allows to connect multiple [[SPI Engine Control Interface]] masters to a single [[SPI Engine Control Interface]] slave. This enables multiple command stream generators to connect to a single [[engine|SPI Engine Execution module]] and consequential give them access to the same SPI bus. The interconnect modules takes care of properly arbitrating between the different command streams.+The SPI Engine Interconnect module allows connecting multiple [[SPI Engine Control Interface]] masters to a single [[SPI Engine Control Interface]] slave. This enables multiple command stream generators to connect to a single [[engine|SPI Engine Execution module]] and consequential give them access to the same SPI bus. The interconnect modules take care of properly arbitrating between the different command streams.
  
-Combining multiple command stream generators in a design and connecting them to a single execution modules allows for the creation of flexible and efficient designs using standard components.+Combining multiple command stream generators in a design and connecting them to a single execution module allows for the creation of flexible and efficient designs using standard components.
  
 ===== Files ===== ===== Files =====
Line 16: Line 16:
  
 ^ Name ^ Description ^ Default ^ ^ Name ^ Description ^ Default ^
 +| ''DATA_WIDTH'' | Data width of the parallel SDI/SDO data interfaces. | 8 |
 +| ''NUM_OF_SDI'' | Number of SDI lines on the physical SPI interface. | 1 |
  
 ===== Signal and Interface Pins ===== ===== Signal and Interface Pins =====
Line 21: Line 23:
 ^ Name ^ Type ^ Description ^ ^ Name ^ Type ^ Description ^
 | clk | Clock | A signals of the module are synchronous to this clock. | | clk | Clock | A signals of the module are synchronous to this clock. |
-| resetn | Synchronous active low reset | Resets the internal state of the module. |+| resetn | Synchronous active-low reset | Resets the internal state of the module. |
 | s0_ctrl | [[SPI Engine Control Interface]] slave | Connects to the first control interface master | | s0_ctrl | [[SPI Engine Control Interface]] slave | Connects to the first control interface master |
 | s1_ctrl | [[SPI Engine Control Interface]] slave | Connects to the second control interface master | | s1_ctrl | [[SPI Engine Control Interface]] slave | Connects to the second control interface master |
resources/fpga/peripherals/spi_engine/interconnect.1526053646.txt.gz · Last modified: 11 May 2018 17:47 by Istvan Csomortani