This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:peripherals:spi_engine:interconnect [29 Feb 2016 14:48] – syntax correction Mihai Ionut Suciu | resources:fpga:peripherals:spi_engine:interconnect [04 Sep 2019 12:47] (current) – Add configuration parameters, fix some grammar mistakes Istvan Csomortani | ||
---|---|---|---|
Line 3: | Line 3: | ||
{{ : | {{ : | ||
- | The SPI Engine Interconnect module allows | + | The SPI Engine Interconnect module allows |
- | Combining multiple command stream generators in a design and connecting them to a single execution | + | Combining multiple command stream generators in a design and connecting them to a single execution |
===== Files ===== | ===== Files ===== | ||
^ Name ^ Description ^ | ^ Name ^ Description ^ | ||
- | | [[github> | + | | [[github> |
- | | [[github> | + | | [[github> |
===== Configuration Parameters ===== | ===== Configuration Parameters ===== | ||
^ Name ^ Description ^ Default ^ | ^ Name ^ Description ^ Default ^ | ||
+ | | '' | ||
+ | | '' | ||
===== Signal and Interface Pins ===== | ===== Signal and Interface Pins ===== | ||
Line 21: | Line 23: | ||
^ Name ^ Type ^ Description ^ | ^ Name ^ Type ^ Description ^ | ||
| clk | Clock | A signals of the module are synchronous to this clock. | | | clk | Clock | A signals of the module are synchronous to this clock. | | ||
- | | resetn | Synchronous active low reset | Resets the internal state of the module. | | + | | resetn | Synchronous active-low reset | Resets the internal state of the module. | |
| s0_ctrl | [[SPI Engine Control Interface]] slave | Connects to the first control interface master | | | s0_ctrl | [[SPI Engine Control Interface]] slave | Connects to the first control interface master | | ||
| s1_ctrl | [[SPI Engine Control Interface]] slave | Connects to the second control interface master | | | s1_ctrl | [[SPI Engine Control Interface]] slave | Connects to the second control interface master | |