This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:peripherals:jesd204:jesd204_troubleshooting [05 Mar 2021 12:35] – [Link status stays in CGS and SYNC~ de-asserts, subclass 1] Laszlo Nagy | resources:fpga:peripherals:jesd204:jesd204_troubleshooting [22 Apr 2021 08:36] – [Link is DISABLED, In Linux boot log following appears: axi-adxcvr-tx: QPLL: failed to find setting for lane rate ...] Laszlo Nagy | ||
---|---|---|---|
Line 63: | Line 63: | ||
</ | </ | ||
+ | ---- | ||
+ | |||
+ | ====Link is DISABLED, In Linux boot log following appears: | ||
+ | <WRAP center round box 100%> | ||
+ | **Cause:** QPLL can't find a configuration for desired lane rate with the given reference clock. | ||
+ | |||
+ | **Identify: | ||
+ | |||
+ | **Fix:** Configure the clock chip for different reference clock or switch to CPLL or QPLL0/1. | ||
+ | </ | ||
---- | ---- | ||