This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:docs:axi_sysid [14 Nov 2019 12:19] – Fix few typeos Istvan Csomortani | resources:fpga:docs:axi_sysid [13 Oct 2021 10:13] (current) – Edit footer Iulia Moldovan | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== System ID ====== | ====== System ID ====== | ||
- | The System ID solution is comprised of 2 cores: the [[https:// | + | The System ID solution is comprised of 2 cores: the [[https:// |
+ | The System ID information is used to provide information about the system’s bit file to facilitate future debugging actions. This information will be stored internally in a ROM and will be made available to the system via the AXI Lite interface. | ||
+ | |||
+ | |||
+ | ===== Block Diagram ===== | ||
- | ==== Block Diagram ==== | ||
{{: | {{: | ||
- | ====== Introduction ====== | ||
- | The System ID information is used to provide information about the system’s bit file to facilitate future debugging actions. This information will be stored internally in a ROM and will be made available to the system via the AXI Lite interface. | ||
- | ==== AXI Sysid IP Configuration | + | ===== AXI Sysid IP Configuration |
^ Name ^ Description ^ Default Value^ | ^ Name ^ Description ^ Default Value^ | ||
| '' | | '' | ||
| '' | | '' | ||
- | ==== AXI Sysid IP Signal and Interface Pins ==== | + | ===== AXI Sysid IP Signal and Interface Pins ===== |
^ Interface ^ Pin ^ Type ^ Description ^ | ^ Interface ^ Pin ^ Type ^ Description ^ | ||
| | '' | | | '' | ||
Line 22: | Line 25: | ||
| | '' | | | '' | ||
- | ==== Sysid ROM IP Configuration | + | ===== Sysid ROM IP Configuration |
^ Name ^ Description ^ Default Value^ | ^ Name ^ Description ^ Default Value^ | ||
| '' | | '' | ||
Line 28: | Line 32: | ||
| '' | | '' | ||
- | ==== Sysid ROM IP Signal and Interface Pins ==== | + | ===== Sysid ROM IP Signal and Interface Pins ===== |
^ Interface ^ Pin ^ Type ^ Description ^ | ^ Interface ^ Pin ^ Type ^ Description ^ | ||
| | '' | | | '' | ||
Line 34: | Line 39: | ||
| | '' | | | '' | ||
- | ==== Register Map ==== | ||
- | {{page>: | ||
+ | ===== Register Map ===== | ||
+ | | ||
+ | {{page>: | ||
+ | |||
+ | |||
+ | ===== Clocking ===== | ||
- | ==== Clocking ==== | ||
The IP core runs on the AXI clock and requires a frequency of 100MHz. | The IP core runs on the AXI clock and requires a frequency of 100MHz. | ||
- | ==== Theory of Operation ==== | + | |
+ | ===== Theory of Operation | ||
The System ID consists of a system of 2 or more IP cores where one provides access to the AXI Lite interface, and the other behaves as a ROM. There can be more than one ROM IP cores if required. The information contained by the ROM will be generated and written at synthesis and will provide details as revealed further in this document. | The System ID consists of a system of 2 or more IP cores where one provides access to the AXI Lite interface, and the other behaves as a ROM. There can be more than one ROM IP cores if required. The information contained by the ROM will be generated and written at synthesis and will provide details as revealed further in this document. | ||
Line 47: | Line 56: | ||
Once written, these contents cannot be changed, only read. These ROMs will be 32 bits wide with a fixed length of 512 lines for the System ROM (2KiB). The secondary PR ROM will generally be smaller. | Once written, these contents cannot be changed, only read. These ROMs will be 32 bits wide with a fixed length of 512 lines for the System ROM (2KiB). The secondary PR ROM will generally be smaller. | ||
- | ==== Data format ==== | ||
- | === Common Header === | + | ===== Data format ===== |
+ | |||
+ | ==== Common Header | ||
^ Field size ^ Field ^ Value ^ Data format^ | ^ Field size ^ Field ^ Value ^ Data format^ | ||
Line 61: | Line 71: | ||
| 4B * | Checksum | | 4B * | Checksum | ||
- | === Internal Use Area === | + | ==== Internal Use Area ==== |
^ Field size ^ Field ^ Data format^ | ^ Field size ^ Field ^ Data format^ | ||
+ | | 28B * | Git branch | ||
| 44B * | Git tag (sha) | hex | | | 44B * | Git tag (sha) | hex | | ||
| 4B * | Git clean check | hex | | | 4B * | Git clean check | hex | | ||
Line 87: | Line 98: | ||
**PR Custom String Area:** This area provides a region where a custom string provided by the user will be written to. This will be stored in ROM2, inside the PR bit where available. Data converted from ASCII to hex. | **PR Custom String Area:** This area provides a region where a custom string provided by the user will be written to. This will be stored in ROM2, inside the PR bit where available. Data converted from ASCII to hex. | ||
- | ==== Working with the Core ==== | + | |
+ | ===== Working with the Core ===== | ||
The System ID solution is automatically placed into a project by the Tcl code ADI uses to build projects. It is instantiated in two stages, first in the " | The System ID solution is automatically placed into a project by the Tcl code ADI uses to build projects. It is instantiated in two stages, first in the " | ||
Line 97: | Line 109: | ||
sysid_gen_sys_init_file $sys_cstring | sysid_gen_sys_init_file $sys_cstring | ||
</ | </ | ||
+ | |||
+ | |||
+ | {{navigation HDL User Guide# |