The AXI DMAC is a high-speed, high-throughput, general purpose DMA controller intended to be used to transfer data between system memory and other peripherals like high-speed converters.
Name | Description |
---|---|
axi_dmac.v | Verilog source for the peripheral. |
Name | Description | Default |
---|---|---|
ID | Instance identification number. | 0 |
DMA_DATA_WIDTH_SRC | Data path width of the source interface in bits. | 64 |
DMA_DATA_WIDTH_DEST | Data path width of the destination interface in bits. | 64 |
DMA_DATA_WIDTH_SG | Data path width of the scatter-gather interface in bits. | 64 |
DMA_LENGTH_WIDTH | Width of transfer length control register in bits. Limits length of the transfers to 2** DMA_LENGTH_WIDTH . | 24 |
DMA_2D_TRANSFER | Enable support for 2D transfers. | 0 |
DMA_SG_TRANSFER | Enable support for scatter-gather transfers. | 0 |
ASYNC_CLK_REQ_SRC | Whether the request and source clock domains are asynchronous. | 1 |
ASYNC_CLK_SRC_DEST | Whether the source and destination clock domains are asynchronous. | 1 |
ASYNC_CLK_DEST_REQ | Whether the destination and request clock domains are asynchronous. | 1 |
ASYNC_CLK_REQ_SG | Whether the request and scatter-gather clock domains are asynchronous. | 1 |
ASYNC_CLK_SRC_SG | Whether the source and scatter-gather clock domains are asynchronous. | 1 |
ASYNC_CLK_DEST_SG | Whether the destination and scatter-gather clock domains are asynchronous. | 1 |
AXI_SLICE_DEST | Whether to insert an extra register slice on the source data path. | 0 |
AXI_SLICE_SRC | Whether to insert an extra register slice on the destination data path. | 0 |
SYNC_TRANSFER_START | Enable the transfer start synchronization feature. | 0 |
CYCLIC | Enable support for Cyclic transfers. | 1 |
DMA_AXI_PROTOCOL_SRC | AXI protocol version of the source interface (0 = AXI4, 1 = AXI3). | 0 |
DMA_AXI_PROTOCOL_DEST | AXI protocol version of the destination interface (0 = AXI4, 1 = AXI3). | 0 |
DMA_AXI_PROTOCOL_SG | AXI protocol version of the scatter-gather interface (0 = AXI4, 1 = AXI3). | 0 |
DMA_TYPE_SRC | Interface type for the source interface (0 = AXI-MM, 1 = AXI-Streaming, 2 = ADI-FIFO). | 2 |
DMA_TYPE_DEST | Interface type for the destination interface (0 = AXI-MM, 1 = AXI-Streaming, 2 = ADI-FIFO). | 0 |
DMA_AXI_ADDR_WIDTH | Maximum address width for AXI interfaces. | 32 |
MAX_BYTES_PER_BURST | Maximum size of bursts in bytes. Must be power of 2 in a range of 2 beats to 4096 bytes The size of the burst is limited by the largest burst that both source and destination supports. This depends on the selected protocol. For AXI3 the maximum beats per burst is 16, while for AXI4 is 256. For non AXI interfaces the maximum beats per burst is in theory unlimited but it is set to 1024 to provide a reasonable upper threshold. This limitation is done internally in the core. | 128 |
FIFO_SIZE | Size of the store-and-forward memory in bursts. Size of a burst is defined by the MAX_BYTES_PER_BURST parameter. Must be power of 2 in the range of 2 to 32. | 4 |
DISABLE_DEBUG_REGISTERS | Disable debug registers. | 0 |
ENABLE_DIAGNOSTICS_IF | Add insight into internal operation of the core, for debug purposes only. | 0 |
Name | Type | Description |
---|---|---|
s_axi_aclk | Clock | All s_axi signals and irq are synchronous to this clock. |
s_axi_aresetn | Synchronous active low reset | Resets the internal state of the peripheral. |
s_axi | AXI4-Lite bus slave | Memory mapped AXI-lite bus that provides access to modules register map. |
irq | Level-High Interrupt | Interrupt output of the module. Is asserted when at least one of the modules interrupt is pending and enabled. |
m_src_axi_aclk | Clock | The m_src_axi interface is synchronous to this clock. Only present when DMA_TYPE_SRC parameter is set to AXI-MM (0). |
m_src_axi_aresetn | Synchronous active low reset | Reset for the m_src_axi interface. Only present when DMA_TYPE_SRC parameter is set to AXI-MM (0). |
m_src_axi | AXI3/AXI4 bus master | Only present when DMA_TYPE_SRC parameter is set to AXI-MM (0). |
m_dest_axi_aclk | Clock | The m_src_axi interface is synchronous to this clock. Only present when DMA_TYPE_DEST parameter is set to AXI-MM (0). |
m_dest_axi_aresetn | Synchronous active low reset | Reset for the m_dest_axi interface. Only present when DMA_TYPE_DEST parameter is set to AXI-MM (0). |
m_dest_axi | AXI3/AXI4 bus master | Only present when DMA_TYPE_DEST parameter is set to AXI-MM (0). |
m_sg_axi_aclk | Clock | The m_sg_axi interface is synchronous to this clock. Only present when DMA_SG_TRANSFER parameter is set. |
m_sg_axi_aresetn | Synchronous active low reset | Reset for the m_sg_axi interface. Only present when DMA_SG_TRANSFER parameter is set. |
m_sg_axi | AXI3/AXI4 bus master | Only present when DMA_SG_TRANSFER parameter is set. |
s_axis_aclk | Clock | The s_axis interface is synchronous to this clock. Only present when DMA_TYPE_SRC parameter is set to AXI-Streaming (1). |
s_axis | AXI-streaming bus slave | Only present when DMA_TYPE_SRC parameter is set to AXI-Streaming (1). |
m_axis_aclk | Clock | The m_axis interface is synchronous to this clock. Only present when DMA_TYPE_DEST parameter is set to AXI-Streaming (1). |
m_axis | AXI-streaming bus master | Only present when DMA_TYPE_DEST parameter is set to AXI-Streaming (1). |
fifo_wr_clk | Clock | The fifo_wr interface is synchronous to this clock. Only present when DMA_TYPE_SRC parameter is set to FIFO (2). |
fifo_wr | FIFO write interface | Only present when DMA_TYPE_SRC parameter is set to FIFO (2). |
fifo_rd_clk | Clock | The fifo_rd interface is synchronous to this clock. Only present when DMA_TYPE_DEST parameter is set to FIFO (2). |
fifo_rd | FIFO read interface | Only present when DMA_TYPE_DEST parameter is set to FIFO (2). |
dest_diag_level_bursts | Diagnostics interface | Only present when ENABLE_DIAGNOSTICS_IF parameter is set . |
Access Type | Name | Description |
---|---|---|
RO | Read-only | Reads will return the current register value. Writes have no effect. |
RW | Read-write | Reads will return the current register value. Writes will change the current register value. |
RW1C | Write-1-to-clear | Reads will return the current register value. Writing the register will clear those bits of the register which were set to 1 in the value written. Bits are set by hardware. |
RW1S | Write-1-to-set | Reads will return the current register value. Writing the register will set those bits of the register which were set to 1 in the value written. Bits are cleared by hardware. |
V | Volatile | The V suffix indicates that the register is volatile and its content might change without software interaction. The value of registers without the volatile designation will not change without an explicit write done by software. |
An internal buffer is used to store data from the source interface before it is forwarded to the destination once that can accept it. The purpose of the buffer is to even out the rate mismatches between the source and destination. e.g if the destination is a FIFO interface with a fixed data rate and the source is a MM interface, the intent is to keep the buffer as full as possible so in case of the MM interface is not ready data can be still provided to the destination without risking an underflow. Similarly in case the destination is a MM interface and the source a FIFO interface with a fixed data rate, the intent is to keep the buffer as empty as possible so in case the MM interface is not ready data can be still accepted from the source without risking an overflow.
The size of the buffer in bytes is determined by the synthesis parameters of the module and it is equal to FIFO_SIZE
* MAX_BYTES_PER_BURST
The register map configuration interface can be accessed through the AXI4-Lite S_AXI
interface. The interface is synchronous to the s_axi_aclk
. The s_axi_aresetn
signal is used to reset the peripheral and should be asserted during system startup until the s_axi_aclk
is active and stable. De-assertion of the reset signal should by synchronous to s_axi_aclk
.
The interface back-pressures through the s_axis_ready
signal.
If the core is in the idle state the s_axis_ready
signal will stay low until a descriptor is submitted.
The s_axis_ready
will go low once the internal buffer of the core is full. It will go high only after enough space is available to store at least a burst (MAX_BYTES_PER_BURST
bytes); Once the current transfer is finished and a new descriptor was not submitted the s_axis_ready
will go low.
The s_axis_ready
will go low also when the TLAST is used that asserts unexpectedly. Unexpectedly means that the transfer length defined by TLAST is shorter than the transfer length programmed in the descriptor (X_LENGTH
register). If the next descriptor was already submitted the s_axis_ready
will assert within few cycles, in other hand will stay low until a new descriptor is submitted.
The xfer_req
is asserted once a transfer is submitted to the descriptor queue and stays high until all data from the current transfer is received/send through the AXI Stream/FIFO interface. If during the current transfer another descriptor is queued (submitted) it will stay high and so on.
The peripheral features a register map configuration interface that can be accessed through the AXI4-Lite S_AXI
port. The register map can be used to configure the peripherals operational parameters, query the current status of the device and query the features supported by the device.
The peripheral contains multiple registers that allow the identification of the peripheral as well as discovery of features that were configured at HDL synthesis time. Apart from the SCRATCH
register all registers in this section are read only and writes to them will be ignored.
The VERSION
(0x000
) register contains the version of the peripheral. The version determines the register map layout and general features supported by the peripheral. The version number follows semantic versioning. Increments in the major number indicate backwards incompatible changes, increments in the minor number indicate backwards compatible changes, patch letter increments indicate fixed incorrect behavior.
The PERIPHERAL_ID
(0x004
) register contains the value of the ID
HDL configuration parameter that was set during synthesis. Its primary function is to allow to distinguish between multiple instances of the peripheral in the same design.
The SCRATCH
(0x008
) register is a general purpose 32-bit register that can be set to an arbitrary values. Reading the register will yield the value previously written (The value will be cleared when the peripheral is reset). It's content does not affect the operation of the peripheral. It can be used by software to test whether the register map is accessible or store custom peripheral associated data.
The IDENTIFICATION
(0x00c
) register contains the value of “DMAC”
. This value is unique to this type of peripheral and can be used to ensure that the peripheral exists at the expected location in the memory mapped IO register space.
Interrupt processing is handled by three closely related registers. All three registers follow the same layout, each bit in the register corresponds to one particular interrupt.
When an interrupt event occurs it is recorded in the IRQ_SOURCE
(0x088
) register. For a recorded interrupt event the corresponding bit is set to 1. If an interrupt event occurs while the bit is already set to 1 it will stay set to 1.
The IRQ_MASK
(0x080
) register controls how recorded interrupt events propagate. An interrupt is considered to be enabled if the corresponding bit in the IRQ_MASK
register is set to 0, it is considered to be disabled if the bit is set to 1.
Disabling an interrupt will not prevent it from being recorded, but only its propagation. This means if an interrupt event was previously recorded while the interrupt was disabled and the interrupt is being enabled the interrupt event will then propagate.
An interrupt event that has been recorded and is enabled propagates to the IRQ_PENDING
(0x084
) register. The corresponding bit for such an interrupt will read as 1. Disabled or interrupts for which no events have been recorded will read as 0. Also if at least one interrupt has been recorded and is enabled the external irq
signal will be asserted to signal the IRQ event to the upstream IRQ controller.
A recorded interrupt event can be cleared (or acknowledged) by writing a 1 to the corresponding bit to either the IRQ_SOURCE
or IRQ_PENDING
register. It is possible to clear multiple interrupt events at the same time by setting multiple bits in a single write operation.
For more details regarding interrupt operation see the interrupts section of this document.
The DEST_ADDRESS
(0x410
) register contains the destination address of the transfer. The address must be aligned to the destination bus width. Non-aligned addresses will be automatically aligned internally by setting the LSBs to 0. This register is only valid if the DMA channel has been configured for write to memory support.
The SRC_ADDRESS
(0x414
) register contains the source address of the transfer. The address must be aligned to the source bus width. Non-aligned addresses will be automatically aligned internally by setting the LSBs to 0. This register is only valid if the DMA channel has been configured for write from memory support.
The X_LENGTH
(0x418
) register contains the number of bytes to transfer per row. The number of bytes is equal to the value of the register + 1 (E.g. a value of 0x3ff means 0x400 bytes).
The Y_LENGTH
(0x41C
) register contains the number of rows to transfer. The number of rows is equal to the value of the register + 1 (E.g. a value of 1079 means 1080 rows). This register is only valid if the DMA channel has been configured with 2D transfer support. If 2D transfer support is disabled the number of rows is always 1 per transfer.
The SRC_STRIDE
(0x424
) and DEST_STRIDE
(0x420
) registers contain the number of bytes between the start of one row and the next row. Needs to be aligned to the bus width. This field is only valid if the DMA channel has been configured with 2D transfer support.
The total number of bytes transferred is equal to (X_LENGTH
+ 1
) * (Y_LENGTH
+ 1
).
The FLAGS
(0x40C
) register controls the behavior of the transfer.
TLAST
([1]
) bit is set the TLAST signal will be asserted during the last beat of the AXI Stream transfer.
Writing a 1 to the TRANSFER_SUBMIT
(0x408
) register queues a new transfer. If the internal transfer queue is full the TRANSFER_SUBMIT
bit will stay asserted until room becomes available, the bit transitions back to 0 once the transfer has been queued. Writing a 0 to this register has no effect. Writing a 1 to the register while it is already 1 will also have no effect. When submitting a new transfer software should always check that the TRANSFER_SUBMIT
[0] bit is 0 before setting it, otherwise the transfer will not be queued.
If the DMA channel is disabled (ENABLE
control bit is set to 0) while a queuing operation is in progress it will be aborted and the TRANSFER_SUBMIT
bit will de-assert.
The TRANSFER_ID
(0x404
) register contains the ID of the next transfer. The ID is generated by the DMA controller and can be used to check if a transfer has been completed by checking the corresponding bit in the TRANSFER_DONE
(0x428
) register. The contents of this register is only valid if TRANSFER_SUBMIT
is 0. Software should read this register before asserting the TRANSFER_SUBMIT
bit.
The TRANSFER_DONE
(0x428
) register indicates whether a submitted transfer has been completed. Each bit in the register corresponds to transfer ID. When a new transfer is submitted the corresponding bit in the register is cleared, once the the transfer has been completed the corresponding bit will be set.
The ACTIVE_TRANSFER_ID
(0x42C
) register holds the ID of the currently active transfer. When no transfer is active the value of register will be equal to the value of the TRANSFER_ID
(0x404
) register.
When using MM or FIFO source interfaces the amount of data which the core will transfer is defined by X_LENGTH
and Y_LENGTH
registers in the moment of the transfer submission. Once the corresponding bit from the TRANSFER_DONE
is set the programmed amount of data is transferred.
When using streaming interface (AXIS) as source, the length of transfers will be defined by the assertion of TLAST
signal which is unknown at the moment of transfer submission. In this case X_LENGTH
and Y_LENGTH
specified during the transfer submission will act as upper limits for the transfer.
Transfers where the TLAST occurs ahead of programmed length will be noted as partial transfers.
If PARTIAL_REPORTING_EN
bit from the FLAGS
register is set, the length of partial transfers will be recorded and exposed through the PARTIAL_TRANSFER_LENGTH
and PARTIAL_TRANSFER_ID
registers. The availability of information regarding partial transfers is done through the PARTIAL_TRANSFER_DONE
field of TRANSFER_DONE
register.
During operation the TRANSFER_PROGRESS
register can be consulted to check the progress of the current transfer. The register presents the number of bytes the destination accepted during the in progress transfer.
This register will be cleared once the transfer completes. This register should be used for debugging purposes only.
Non-cyclic transfers stop once the programmed amount of data is transferred to the destination.
Cyclic transfers needs to be stopped with software intervention by setting the ENABLE
control bit to 0.
In case if required, non cyclic transfers can be interrupted in the same way.
The transfer tear down is done gracefully and is done at a burst resolution on MM interfaces and beat resolution on non-MM interfaces. DMAC shuts down gracefully as fast as possible while completing all in-progress MM transactions.
Source side:
For MM interface once the ENABLE
bit de-asserts the DMAC won't issue new requests towards the source interface but will wait until all pending requests are fulfilled by the source.
For non-MM interfaces, once the ENABLE
bit de-asserts the DMAC will stop to accept new data. This will lead to partial bursts in the internal buffer but this data will be cleared/lost once the destination side completes all pending bursts.
Destination side:
For MM interface the DMAC will complete all pending requests that have been started by issuing the address.
For non-MM interfaces once the ENABLE
bit de-asserts the DMAC will stop to drive new data. All the data from the internal buffer will be cleared/lost.
In case of AXIS the DMAC will wait for data to be accepted if valid is high since it can't just de-assert valid without breaking the interface semantics
The DMA controller supports interrupts to allow asynchronous notification of certain events to the CPU. This can be used as an alternative to busy-polling the status registers. Two types of interrupt events are implemented by the DMA controller.
The TRANSFER_QUEUED
interrupt is asserted when a transfer is moved from the register map to the internal transfer queue. This is equivalent to the TRANSFER_SUBMIT
register transitioning from 1 to 0. Software can use this interrupt as an indication that the next transfer can be submitted.
Note that a transfer being queued does not mean that it has been started yet. If other transfers are already queued those will be processed first.
The TRANSFER_COMPLETED
interrupt is asserted when a previously submitted transfer has been completed. To find out which transfer has been completed the TRANSFER_DONE
register should be checked.
Note that depending on the transfer size and interrupt latency it is possible for multiple transfers to complete before the interrupt handler runs. In that case the interrupt handler will only run once. Software should always check all submitted transfers for completion.
If the DMA_2D_TRANSFER
HDL synthesis configuration parameter is set the DMA controller has support for 2D transfers.
A 2D transfer is composed of a number of rows with each row containing a certain number of bytes. Between each row there might be a certain amount of padding bytes that are skipped by the DMA.
For 2D transfers the X_LENGTH
register configures the number of bytes per row and the Y_LENGTH
register configures the number of rows. The SRC_STRIDE
and DEST_STRIDE
registers configure the number of bytes in between start of two rows.
E.g. the first row will start at the configured source or destination address, the second row will start at the configured source or destination address plus the stride and so on.
ROW_SRC_ADDRESS = SRC_ADDRESS + SRC_STRIDE * N
ROW_DEST_ADDRESS = DEST_ADDRESS + DEST_STRIDE * N
If support for 2D transfers is disabled only the X_LENGTH register is considered and the number of rows per transfer is fixed to 1.
If the CYCLIC
HDL synthesis configuration parameter is set the DMA controller has support for cyclic transfers.
A cyclic transfer once completed will restart automatically with the same configuration. The behavior of cyclic transfer is equivalent to submitting the same transfer over and over again, but generates less software management overhead.
A transfer is cyclic if the CYCLIC
([0]
) bit of the FLAGS
(0x40C
) is set to 1 during transfer submission.
For cyclic transfers no end-of-transfer interrupts will be generated. To stop a cyclic transfer the DMA channel must be disabled.
Any additional transfers that are submitted after the submission of a cyclic transfer (and before stopping the cyclic transfer) will never be executed.
If the DMA_SG_TRANSFER
HDL synthesis configuration parameter is set the DMA controller has support for scatter-gather transfers.
The scatter-gather optional feature allows the DMA to access noncontiguous areas of memory within a single transfer.
The DMA can read from or write to different memory addresses in one transaction by using a list of vectors called descriptors. Each descriptor provides the starting address and the length of the current memory block to be accessed, as well as the next address of the following descriptor to be processed. By chaining these descriptors, the DMA can gather the data into a contiguous transfer from the scattered memory data from multiple addresses.
The scatter-gather has its own dedicated AXI3/4 memory mapped interface m_sg_axi
through which it receives the descriptor data.
The scatter-gather interface fetches the descriptor information from memory in the following order:
Size | Name | Description |
---|---|---|
32-bit | flags | This field includes 2 control bits: * bit0: if set, the transfer will complete after this last descriptor is processed, and the DMA core will go back to idle state; if cleared, the next DMA descriptor pointed to by next_sg_addr will be loaded. * bit1: if set, an end-of-transfer interrupt will be raised after the memory segment pointed to by this descriptor has been transferred. |
32-bit | id | This field corresponds to an identifier of the descriptor. |
64-bit | dest_addr | This field contains the destination address of the transfer. |
64-bit | src_addr | This field contains the source address of the transfer. |
64-bit | next_sg_addr | This field contains the address of the next descriptor. |
32-bit | y_len | This field contains the number of rows to transfer, minus one. |
32-bit | x_len | This field contains the number of bytes to transfer, minus one. |
32-bit | src_stride | This field contains the number of bytes between the start of one row and the next row for the source address. |
32-bit | dst_stride | This field contains the number of bytes between the start of one row and the next row for the destination address. |
The y_len
, src_stride
and dst_stride
fields are only useful for 2D transfers and should be set to 0 if 2D transfers are not required.
The scatter-gather transfers are enabled through the HWDESC
bit from the CONTROL
(0x400
) register. Once this bit is set, cyclic transfers are disabled.
To start a scatter-gather transfer, the address of the first DMA descriptor must be written to the register pair [SG_ADDRESS_HIGH
(0x4BC
), SG_ADDRESS
(0x47C
)].
To end a scatter-gather transfer, the last descriptor of the transfer must have the flags
[0] bit set.
The scatter-gather transfer is queued in a similar way to the simple transfers, through the TRANSFER_SUBMIT
. Software should always poll this bit to be 0 before setting it, otherwise the scatter-gather transfer will not be queued.
The scatter-gather transfers support the generation of the same two types of interrupt events as the simple transfers. However, the scatter-gather transfers have the distinct advantage of generating fewer interrupts by treating the chained descriptor transfers as a single transfer, thus improving the performance of the application.
If the transfer start synchronization feature of the DMA controller is enabled the start of a transfer is synchronized to a flag in the data stream. This is primarily useful if the data stream does not have any back-pressure and one unit of data spans multiple beats (e.g. packetized data). This ensures that the data is properly aligned to the beginning of the memory buffer.
Data that is received before the synchronization flag is asserted will be ignored by the DMA controller.
For the FIFO write interface the fifo_wr_sync
signal is the synchronization flag signal. For the AXI-Streaming interface the synchronization flag is carried in s_axis_user[0]
. In both cases the synchronization flag is qualified by the same control signal as the data.
For debug purposes a diagnostics interface is added to the core.
The dest_diag_level_bursts
signal adds insight into the fullness of the internal memory buffer during operation.
The information is exposed in number of bursts where the size of a burst is defined by the MAX_BYTES_PER_BURST
parameter. The value of dest_diag_level_bursts
increments for each burst accumulated in the DMACs internal buffer. It decrements once the burst leaves the DMAC on its destination port.
The signal is synchronous to the destination clock domain (m_dest_axi_aclk
or m_axis_aclk
depending on DMA_TYPE_DEST
).
Software must program the SRC_ADDRESS
and DEST_ADDRESS
registers in such way that AXI burst won't cross the 4kB address boundary. The following condition must hold:
MAX_BYTES_PER_BURST
≤ 4096; MAX_BYTES_PER_BURST
is power of 2; SRC/DEST_ADDRESS
mod MAX_BYTES_PER_BURST
== 0 SRC/DEST_ADDRESS[11:0]
+ MIN(X_LENGTH
+1,MAX_BYTES_PER_BURST
) ≤ 4096
Software must program the SRC_ADDRESS
and DEST_ADDRESS
registers to be multiple of the corresponding MM data bus. The following conditions must hold:
SRC_ADDRESS
MOD (DMA_DATA_WIDTH_SRC
/8) == 0 DEST_ADDRESS
MOD (DMA_DATA_WIDTH_DEST
/8) == 0
Software must program the X_LENGTH
register to be multiple of the widest data bus. The following condition must hold:
X_LENGTH
+1) MOD MAX(DMA_DATA_WIDTH_SRC
, DMA_DATA_WIDTH_DEST
)/8 == 0This restriction can be relaxed for the memory mapped interfaces. This is done by partially ignoring data of a beat from/to the MM interface:
E.g. the length alignment requirement of a DMA configured for a 64-bit memory mapped interface and a 16-bit streaming interface is only 2 bytes instead of 8 bytes.
Note that the address alignment requirement is not affected by this. The address still needs to be aligned to the width of the MM interface that it belongs to.
The scatter-gather dedicated interface m_sg_axi
currently supports only 64-bit transfers. DMA_DATA_WIDTH_SG
can only be set to 64.
Analog Devices recommends to use the provided software drivers.
1. When max bytes per burst matches the data width of destination interface an erroneous extra beat is inserted after every valid beat on the destination side. Example configuration:
- axi mm → axi stream
- max bytes per burst = 128
- destination width = 1024 bits
Workaround: increase the max bytes per burst to larger than 128
Analog Devices will provide limited online support for anyone using the core with Analog Devices components (ADC, DAC, Video, Audio, etc) via the EngineerZone.
Term | Description |
---|---|
beat | Represents the amount of data that is transferred in one clock cycle. |
burst | Represents the amount of data that is transferred in a group of consecutive beats. |
partial transfer | Represents a transfer which is shorter than the programmed length that is based on the X_LENGTH and Y_LENGTH registers. This can occur on AXIS source interfaces when TLAST asserts earlier than the programmed length. |