This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:docs:axi_adc_trigger [13 Mar 2019 10:00] – [Block Diagram] Andrei Grozav | resources:fpga:docs:axi_adc_trigger [13 Oct 2021 09:56] (current) – Edit footer & add reference to generic ADC Iulia Moldovan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ===== AXI_ADC_TRIGGER ===== | + | ====== AXI_ADC_TRIGGER |
- | The AXI_ADC_TRIGGER IP implements triggering for the ADC path and also controls two I/O triggering pins. | + | The AXI_ADC_TRIGGER IP implements triggering for the ADC path and also controls two I/O triggering pins.\\ |
+ | \\ | ||
+ | More about the generic framework interfacing ADCs can be read here: [[: | ||
- | ==== Features ==== | + | |
+ | ===== Features | ||
* AXI Lite control/ | * AXI Lite control/ | ||
Line 18: | Line 21: | ||
* Falling edge | * Falling edge | ||
* Mixing analog and digital triggers | * Mixing analog and digital triggers | ||
+ | * Instrument trigger (from Logic Analyzer) | ||
* Controls two IO trigger pins | * Controls two IO trigger pins | ||
- | ==== Block Diagram ==== | ||
- | {{: | + | ===== Block Diagram ===== |
- | ==== Interface ==== | + | {{: |
+ | |||
+ | ==== AXI ADC Tigger submodules ==== | ||
+ | |||
+ | * [[: | ||
+ | * **Channel trigger** | ||
+ | * Channel A | ||
+ | * Amplitude limit - REG_LIMIT_A(0x0014) - Defines the treashold level for the ADC trigger | ||
+ | * Function - TRIGGER_FUNCTION_A(0x0018) - Lower, higher than limit; pass through limit | ||
+ | * Hysteresis - TRIGGER_FUNCTION_A (0x001c) - " | ||
+ | * Channel B | ||
+ | * Amplitude limit - REG_LIMIT_A(0x0024) - Defines the treashold level for the ADC trigger | ||
+ | * Function - TRIGGER_FUNCTION_A(0x0028) - Lower, higher than limit; pass through limit | ||
+ | * Hysteresis - TRIGGER_FUNCTION_A (0x002c) - " | ||
+ | |||
+ | * **External trigger** | ||
+ | * Pin 0 (Ti) \\ Configurations - REG_CONFIG_TRIGGER_I(0x004) allows for: | ||
+ | * falling edge (bit 8) | ||
+ | * rising edge (bit 6) | ||
+ | * any edge (bit 4) | ||
+ | * high level (bit 2) | ||
+ | * low level (bit 0) | ||
+ | * Pin 1 (To) \\ Configurations - REG_CONFIG_TRIGGER_I(0x004) allows for: | ||
+ | * falling edge (bit 9) | ||
+ | * rising edge (bit 7) | ||
+ | * any edge (bit 5) | ||
+ | * high level (bit 3) | ||
+ | * low level (bit 1) | ||
+ | |||
+ | <note important> | ||
+ | |||
+ | * **Channel A MUX** - REG_TRIGGER_MUX_A(0x0020) - Selects between a combination of ADC trigger and the external trigger | ||
+ | * **Channel B MUX** - REG_TRIGGER_MUX_B(0x0030) - Selects between a combination of ADC trigger and the external trigger | ||
+ | |||
+ | * **Output MUX** - REG_TRIGGER_OUT_CONTROL(0x0034) - Selects a combination between the channel A and/or B MUX's and the input of the instrument trigger | ||
+ | * **Holdoff counter** (32 bit) - REG_TRIGGER_HOLDOFF(0x0048) - Controls the trigger out silent period after an event. | ||
+ | * **Delay counter** (32 bit) - REG_TRIGGER_DELAY(0x0040) - Controls the trigger delay | ||
+ | |||
+ | * **External trigger control** | ||
+ | * REG_IO_SELECTION(0x000c) - Controls the direction of the external trigger pins, and the source(for each pin configured as output) | ||
+ | * REG_TRIGGER_OUT_HOLD_PINS(0x004c) - Controls the hold period after a transition to a new logic level. | ||
+ | |||
+ | |||
+ | ===== Interface | ||
^ Interface ^ Pin ^ Type ^ Description ^ | ^ Interface ^ Pin ^ Type ^ Description ^ | ||
Line 43: | Line 89: | ||
| | '' | | | '' | ||
| | '' | | | '' | ||
+ | | | '' | ||
+ | | | '' | ||
| **Fifo Depth** |||| | | **Fifo Depth** |||| | ||
| |'' | | |'' | ||
Line 48: | Line 96: | ||
| | '' | | | '' | ||
- | ==== Detailed Description ==== | ||
- | The AXI_ADC_TRIGGER IP implements triggering for the ADC path based on two trigger pins or based on the analog channel. | + | ===== Detailed Description ===== |
- | The trigger pins are controlled by the core and can be both input or output. For external | + | The AXI_ADC_TRIGGER IP implements triggering for the ADC path. The trigger is generated based on two external |
- | The analog triggering is based on comparison with a limit. The data format must be 2's complement and maximum number of bits of the analog channel is 15. | + | The external |
- | The trigger | + | |
- | Embedding the trigger with the data allows for additional IPs with unknown pipeline length | + | |
- | If a history for data before | + | The analog triggering is based on comparison with a limit. The data format must be 2's complement and the maximum number of bits of the analog channel |
+ | The trigger can be transmitted independent or embedded in the output word, at bit 15. When embedded, the triggers must be extracted and data must be reconstructed, | ||
+ | Embedding | ||
- | ==== Register Map ==== | + | If a history for data before the trigger is needed, a [[: |
- | |< 100% 5% 5% 5% 25% 5% 5% 50% >| | + | |
- | |Address ||Bits |Name |Type |Default |Description | | + | ===== Register Map ===== |
- | |DWORD |BYTE |::: |::: |::: |::: |::: | | + | |
- | ^0x0000 ^0x0000 ^REG_VERSION ^^^^Version Register ^ | + | |< 100% 5% 5% 5% 25% 5% 5% 50% >| |
- | | | |[31:0] |VERSION |RO |0x00 |Version number | | + | |Address ||Bits |Name |Type |Default |Description | |
- | ^0x0001 ^0x0004 ^REG_SCRATCH ^^^^Scratch Register ^ | + | |DWORD |BYTE |::: |::: |::: |::: |::: | |
- | | | |[31:0] |SCRATCH |RW |0x00 |Scratch register | | + | ^0x0000 ^0x0000 ^REG_VERSION ^^^^Version Register ^ |
- | ^0x0002 ^0x0008 ^REG_TRIGGER_O ^^^^Control TRIGGER_O Value ^ | + | | | |[31:0] |VERSION |RO |0x00 |Version number | |
- | | | |[1] |TRIGGER_O[1] |RW |0x00 |Set TRIGGER_O[1] value | | + | ^0x0001 ^0x0004 ^REG_SCRATCH ^^^^Scratch Register ^ |
- | |::: |::: |[0] |TRIGGER_O[0] |RW |0x00 |Set TRIGGER_O[0] value | | + | | | |[31:0] |SCRATCH |RW |0x00 |Scratch register | |
- | ^0x0003 ^0x000c ^REG_IO_SELECTION ^^^^Control Trigger Pins Direction ^ | + | ^0x0002 ^0x0008 ^REG_TRIGGER_O ^^^^Control TRIGGER_O Value ^ |
- | | | |[5:4] |TRIGGER_O[1] (PIN) |RW |0x00 |Select output trigger pin 1 \\ 0: SOFTWARE TRIGGER - TRRIGER_O[1](0x0004) \\ | + | | | |[1] |TRIGGER_O[1] |RW |0x00 |Set TRIGGER_O[1] value | |
- | |::: |::: |[3:2] |TRIGGER_O[0] (PIN) |RW |0x00 |Select output trigger pin 0 \\ 0: SOFTWARE TRIGGER - TRRIGER_O[0](0x0004) \\ | + | |::: |::: |[0] |TRIGGER_O[0] |RW |0x00 |Set TRIGGER_O[0] value | |
- | |::: |::: |[1] |IO_SELECTION[1] |RW |0x00 |Drives the TRIGGER_T[1] pin | | + | ^0x0003 ^0x000c ^REG_IO_SELECTION ^^^^Control Trigger Pins Direction ^ |
- | |::: |::: |[0] |IO_SELECTION[0] |RW |0x00 |Drives the TRIGGER_T[0] pin | | + | | | |[7:5] |TRIGGER_O[1] (To PIN) |RW |0x00 |Select output trigger pin 1 \\ 0: SOFTWARE TRIGGER - TRRIGER_O[1](0x0004) \\ |
- | ^0x0004 ^0x0010 ^REG_CONFIG_TRIGGER_I ^^^^Configure Digital Triggering ^ | + | |::: |::: |[4:2] |TRIGGER_O[0] (Ti PIN) |RW |0x00 |Select output trigger pin 0 \\ 0: SOFTWARE TRIGGER - TRRIGER_O[0](0x0004) \\ |
+ | |::: |::: |[1] |IO_SELECTION[1] |RW |0x00 |Drives the TRIGGER_T[1](To) pin | | ||
+ | |::: |::: |[0] |IO_SELECTION[0] |RW |0x00 |Drives the TRIGGER_T[0](Ti) pin | | ||
+ | ^0x0004 ^0x0010 ^REG_CONFIG_TRIGGER_I ^^^^Configure Digital Triggering ^ | ||
| | |[9:8] |FALL_EDGE |RW |0x00 |Enable falling edge triggering for TRIGGER[0] or TRIGGER[1] pin | | | | |[9:8] |FALL_EDGE |RW |0x00 |Enable falling edge triggering for TRIGGER[0] or TRIGGER[1] pin | | ||
|::: |::: |[7:6] |RISE_EDGE |RW |0x00 |Enable rising edge triggering for TRIGGER[0] or TRIGGER[1] pin | | |::: |::: |[7:6] |RISE_EDGE |RW |0x00 |Enable rising edge triggering for TRIGGER[0] or TRIGGER[1] pin | | ||
Line 83: | Line 133: | ||
|::: |::: |[3:2] |HIGH_LEVEL |RW |0x00 |Enable high level triggering for TRIGGER[0] or TRIGGER[1] pin | | |::: |::: |[3:2] |HIGH_LEVEL |RW |0x00 |Enable high level triggering for TRIGGER[0] or TRIGGER[1] pin | | ||
|::: |::: |[1:0] |LOW_LEVEL |RW |0x00 |Enable low level triggering for TRIGGER[0] or TRIGGER[1] pin | | |::: |::: |[1:0] |LOW_LEVEL |RW |0x00 |Enable low level triggering for TRIGGER[0] or TRIGGER[1] pin | | ||
- | ^0x0005 ^0x0014 ^REG_LIMIT_A ^^^^Analog Trigger Level for Channel ^ | + | ^0x0005 ^0x0014 ^REG_LIMIT_A ^^^^Analog Trigger Level for Channel ^ |
| | |[15:0] |LIMIT_A[15: | | | |[15:0] |LIMIT_A[15: | ||
- | ^0x0006 ^0x0018 ^REG_FUNCTION_A ^^^^Analog Triggering Function ^ | + | ^0x0006 ^0x0018 ^REG_FUNCTION_A ^^^^Analog Triggering Function ^ |
| | |[1:0] |TRIGGER_FUNCTION_A |RW |0x00 |Analog triggering function for channel A: \\ 0: Lower than limit \\ 1: higher than limit \\ 2: pass through high limit \\ 3: passthrough low limit | | | | |[1:0] |TRIGGER_FUNCTION_A |RW |0x00 |Analog triggering function for channel A: \\ 0: Lower than limit \\ 1: higher than limit \\ 2: pass through high limit \\ 3: passthrough low limit | | ||
- | ^0x0007 ^0x001c ^REG_HYSTERESIS_A ^^^^Analog Trigger | + | ^0x0007 ^0x001c ^REG_HYSTERESIS_A ^^^^Analog Trigger |
- | | | |[31:0] |HISTERESYS_A | + | | | |[31:0] |HYSTERESIS_A |
- | ^0x0008 ^0x0020 ^REG_TRIGGER_MUX_A ^^^^Trigger Selection for Path ^ | + | ^0x0008 ^0x0020 ^REG_TRIGGER_MUX_A ^^^^Trigger Selection for Path ^ |
- | | | |[3:0] |TRIGGER_MUX_A |RW |0x00 |Selects trigger a mode: \\ 0: Always on \\ 1: Digital triggering, based on trigger[0] \\ 2: ADC triggering, based on channel A \\ 3: Reserved \\ 4: Digital triggering OR ADC triggering \ \ 5: Digital triggering AND ADC triggering \\ 6: Digital triggering XOR ADC triggering \\ 7: Option 4 negated \\ 8: Option 5 negated \\ 9: Option 6 negated | | + | | | |[3:0] |TRIGGER_MUX_A |RW |0x00 |Selects trigger a mode: \\ 0: Always on \\ 1: Digital triggering, based on trigger[0] \\ 2: ADC triggering, based on channel A \\ 3: Reserved \\ 4: Digital triggering OR ADC triggering \\ 5: Digital triggering AND ADC triggering \\ 6: Digital triggering XOR ADC triggering \\ 7: Option 4 negated \\ 8: Option 5 negated \\ 9: Option 6 negated | |
- | ^0x0009 ^0x0024 ^REG_LIMIT_B ^^^^Analog Trigger Level for Channel ^ | + | ^0x0009 ^0x0024 ^REG_LIMIT_B ^^^^Analog Trigger Level for Channel ^ |
| | |[15:0] |LIMIT_B[15: | | | |[15:0] |LIMIT_B[15: | ||
- | ^0x000A ^0x0028 ^REG_FUNCTION_B ^^^^Analog Triggering Function ^ | + | ^0x000A ^0x0028 ^REG_FUNCTION_B ^^^^Analog Triggering Function ^ |
| | |[1:0] |TRIGGER_FUNCTION_B |RW |0x00 |Analog triggering function for channel B: \\ 0: Lower than limit \\ 1: higher than limit \\ 2: pass through high limit \\ 3: passthrough low limit | | | | |[1:0] |TRIGGER_FUNCTION_B |RW |0x00 |Analog triggering function for channel B: \\ 0: Lower than limit \\ 1: higher than limit \\ 2: pass through high limit \\ 3: passthrough low limit | | ||
- | ^0x000B ^0x002c ^REG_HYSTERESIS_B ^^^^Analog Trigger | + | ^0x000B ^0x002c ^REG_HYSTERESIS_B ^^^^Analog Trigger |
- | | | |[31:0] |HISTERESYS_B | + | | | |[31:0] |HYSTERESIS_B |
- | ^0x000C ^0x0030 ^REG_TRIGGER_MUX_B ^^^^Trigger Selection for Path ^ | + | ^0x000C ^0x0030 ^REG_TRIGGER_MUX_B ^^^^Trigger Selection for Path ^ |
- | | | |[3:0] |TRIGGER_MUX_B |RW |0x00 |Selects trigger B mode: \\ 0: Always on \\ 1: Digital triggering, based on trigger[1] \\ 2: ADC triggering, based on channel B \\ 3: Reserved \\ 4: Digital triggering OR ADC triggering \ \ 5: Digital triggering AND ADC triggering \\ 6: Digital triggering XOR ADC triggering \\ 7: Option 4 negated \\ 8: Option 5 negated \\ 9: Option 6 negated | | + | | | |[3:0] |TRIGGER_MUX_B |RW |0x00 |Selects trigger B mode: \\ 0: Always on \\ 1: Digital triggering, based on trigger[1] \\ 2: ADC triggering, based on channel B \\ 3: Reserved \\ 4: Digital triggering OR ADC triggering \\ 5: Digital triggering AND ADC triggering \\ 6: Digital triggering XOR ADC triggering \\ 7: Option 4 negated \\ 8: Option 5 negated \\ 9: Option 6 negated | |
^0x000D ^0x0034 ^REG_TRIGGER_OUT_CONTROL ^^^^Selection Multiplexer and embedded trigger selection ^ | ^0x000D ^0x0034 ^REG_TRIGGER_OUT_CONTROL ^^^^Selection Multiplexer and embedded trigger selection ^ | ||
- | | | |[16] |EMBEDDE_TRIGGER |RW |0x00 |When set the bit 15 of the out channel data will be the trigger. This alows to keep the data in sync with the trigger in future data processing, before feeding the data to the DMA.\\ When set a u til_extract | + | | | |[16] |EMBEDDE_TRIGGER |RW |0x00 |When set the bit 15 of the out channel data will be the trigger. This alows to keep the data in sync with the trigger in future data processing, before feeding the data to the DMA.\\ When set a util_extract |
- | |::: |::: |[2:0] |TRIGGER_MUX_OUT |RW |0x00 |Final Trigger Selection Multiplexer \\ Selects trigger a mode: \\ 0: Trigger A \\ 1: Trigger B \\ 2: Trigger A OR Trigger B \\ 3: Trigger A AND Trigger B \\ 4: Trigger A XOR Trig ger | | + | |::: |::: |[3:0] |TRIGGER_MUX_OUT |RW |0x00 |Final Trigger Selection Multiplexer \\ Selects trigger a mode: \\ 0: Trigger A \\ 1: Trigger B \\ 2: Trigger A OR Trigger B \\ 3: Trigger A AND Trigger B \\ 4: Trigger A XOR Trigger B \\ 5: Trigger LA \\ 6: Trigger A OR Trigger LA \\ 7: Trigger B OR Trigger LA \\ 8: Trigger A OR Trigger B OR Trigger LA | |
^0x000E ^0x0038 ^REG_FIFO_DEPTH ^^^^Controls the Dynamic Depth of the History FIFO ^ | ^0x000E ^0x0038 ^REG_FIFO_DEPTH ^^^^Controls the Dynamic Depth of the History FIFO ^ | ||
| | |[31:0] |FIFO_DEPTH |RW |0x00 |Controls the depth of the history FIFO. Should be less than the maximum FIFO depth. If set to 0, the FIFO is bypassed. | | | | |[31:0] |FIFO_DEPTH |RW |0x00 |Controls the depth of the history FIFO. Should be less than the maximum FIFO depth. If set to 0, the FIFO is bypassed. | | ||
- | ^0x000F ^0x003c ^REG_TRIGGERED ^^^^Indicates Triggering Status ^ | + | ^0x000F ^0x003c ^REG_TRIGGERED ^^^^Indicates Triggering Status ^ |
- | | | |[0] |TRIGGERED |RW1C |0x00 |Indicates if the trigger has been triggered since the last time this register has been reset. | | + | | | |[0] |TRIGGERED |RW1C |0x00 |Indicates if the trigger has been triggered since the last time this register has been reset. | |
- | ^0x0010 ^0x0040 ^REG_TRIGGER_DELAY ^^^^Control the Trigger Delay ^ | + | ^0x0010 ^0x0040 ^REG_TRIGGER_DELAY ^^^^Control the Trigger Delay ^ |
| | |[31:0] |TRIGGER_DELAY |RW |0x00 |Delays the start of data capture with TRIGGER_DELAY number of samples after the trigger. | | | | |[31:0] |TRIGGER_DELAY |RW |0x00 |Delays the start of data capture with TRIGGER_DELAY number of samples after the trigger. | | ||
- | ^0x0011 ^0x0044 ^REG_STREAMING ^^^^Controls Streaming Mode ^ | + | ^0x0011 ^0x0044 ^REG_STREAMING ^^^^Controls Streaming Mode ^ |
- | | | |[0] |STREAMING |RW |0x00 |If the streaming bit is set, after the trigger condition is met data will be continuosly | + | | | |[0] |STREAMING |RW |0x00 |If the streaming bit is set, after the trigger condition is met data will be continuously |
- | ^Wed Mar 13 08:36:51 2019 ^^^^^^ | + | ^0x0012 ^0x0048 ^REG_TRIGGER_HOLDOFF ^^^^Controls hold off time ^ |
- | ==== References ==== | + | | | |[31:0] |TRIGGER_HOLDOFF |RW |0x00 |Defines the time interval, after a trigger event, where the next trigger events will be ignored, until the end of the interval. The time interval is set by counter. Down-counting on the ADC clock(100MHz). The value written in the register is loaded in the counter at a trigger event. | |
- | * [[https:// | + | ^0x0013 ^0x004c ^REG_TRIGGER_OUT_HOLD_PINS ^^^^Controls external trigger hold time ^ |
- | * [[https:// | + | | | |[19:0] |TRIGGER_OUT_HOLD_PINS |RW |0x00 |Defines a time period, in which the external trigger pins, configured as outputs, will hold the new logic level after a transition. The down-counter, |
+ | ^Tue Sep 1 09:58:53 2020 ^^^^^^ | ||
+ | |||
+ | |||
+ | ===== Aditional notes ===== | ||
+ | |||
+ | <note important> | ||
+ | |||
+ | |||
+ | ===== References ===== | ||
+ | |||
+ | * [[https:// | ||
+ | * [[/ | ||
* [[https:// | * [[https:// | ||
- | {{navigation #axi_ip|AXI IP#hdl|Main page#tips|Tips}} | + | {{navigation |