Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:fpga:docs:axi_ad9265 [16 Apr 2019 10:27] – [Register Map] Laszlo Nagy | resources:fpga:docs:axi_ad9265 [23 Jan 2020 17:55] – Update DEVICE_TYPE Istvan Csomortani |
---|
^ Name ^ Description ^ Default Value^ | ^ Name ^ Description ^ Default Value^ |
| ''ID'' | Core ID should be unique for each AD9265 IP in the system | 0 | | | ''ID'' | Core ID should be unique for each AD9265 IP in the system | 0 | |
| ''DEVICE_TYPE'' | Used to select between Virtex 6 (1) or 7 Series (0) devices | 0 | | | ''DEVICE_TYPE'' | Used to select between 7 Series (1), Ultrascale (2) or Ultrascale+ (3) devices | 0 | |
| ''ADC_DATAPATH_DISABLE'' | If set, the datapath processing is not generated and output data is taken directly from the AD9265 | 0 | | | ''ADC_DATAPATH_DISABLE'' | If set, the datapath processing is not generated and output data is taken directly from the AD9265 | 0 | |
| ''IO_DELAY_GROUP'' | The delay group name which is set for the delay controller | "adc_if_delay_group" | | | ''IO_DELAY_GROUP'' | The delay group name which is set for the delay controller | "adc_if_delay_group" | |
==== Register Map ==== | ==== Register Map ==== |
| |
| |
==== Register Map base addresses ==== | |
|< 100% 5% 5% 5% 25% 5% 55% >| | |
|Address ||Name |||Description | | |
|DWORD |BYTE |::: |::: |::: |::: | | |
^0x0000 ^0x0000 ^BASE ^^^See the [[#base_common_to_all_cores|Base (common to all cores)]] table for more detail ^ | |
^0x0010 ^0x0040 ^RX COMMON ^^^ See the [[#adc_common_axi_ad|ADC Common]] table for more detail ^ | |
^0x0100 ^0x0400 ^RX CHANNELS ^^^ See the [[#adc_channel_axi_ad|ADC Channel]] table for more detail ^ | |
| |
| |