This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:docs:axi_ad9265 [16 Apr 2019 10:27] – [Register Map] Laszlo Nagy | resources:fpga:docs:axi_ad9265 [16 Apr 2019 10:27] – [Register Map base addresses] Laszlo Nagy | ||
---|---|---|---|
Line 71: | Line 71: | ||
==== Register Map ==== | ==== Register Map ==== | ||
- | |||
- | ==== Register Map base addresses ==== | ||
- | |< 100% 5% 5% 5% 25% 5% 55% >| | ||
- | |Address ||Name |||Description | | ||
- | |DWORD |BYTE |::: |::: |::: |::: | | ||
- | ^0x0000 ^0x0000 ^BASE ^^^See the [[# | ||
- | ^0x0010 ^0x0040 ^RX COMMON ^^^ See the [[# | ||
- | ^0x0100 ^0x0400 ^RX CHANNELS ^^^ See the [[# | ||