This is an old revision of the document!
HDL Architecture
Every HDL design of a reference project can be divided into two subsystems:
How they're instantiated:
In case of a project, inside the system_bd.tcl file, we have to source the base design first, then the board design.
Example
Take FMCOMMS2 with Zedboard, the system_bd.tcl will look like the following:
source $ad_hdl_dir/projects/common/zed/zed_system_bd.tcl
source ../common/fmcomms2_bd.tcl
Typical project diagram
Base Design
The base design contains all the I/O peripheral and memory interfaces and processing components, which are necessary for a fully functional Linux system. The majority of these components are Intel and Xilinx IP cores.
Typically, this contains:
Microprocessor
In our designs, we use only two types:
Worth mentioning in case of SoCs, the Hard Processor System (HPS) or Processing System 7/8 (PS7/8) do not contain just the dual-core ARM® Cortex® - A9 MPCore™ processor, they also have other integrated peripherals and memory interfaces. For more information please visit the manufacturer's website, listed in the table above.
We are calling:
PS7
— the instance from Xilinx Vivado called processing_system7
PS8
— the instance from Xilinx Vivado called zynq_ultra_ps_e
Versal
— the instance from Xilinx Vivado called versap_cips
Memory Interface Controller
In almost all cases, the carrier board is not made and designed by Analog Devices, so the external memory solution of the system is given. Meaning we can not support, modify or alter this important part of the system, in several cases we even have system limitations because of it (e.g. the memory interface is not fast enough to handle the required data throughput).
Under the two links below the user can find the landing page of the available memory solutions for both Altera and Xilinx:
Peripheral Interfaces
SPI
In general, the base system has two Serial Peripheral Interfaces, which are used as a control interface for FMC/HSMC devices. These SPI interfaces are controlled by the integrated SPI controller of the Hard Processor System (HPS) or Processing System 7/8 (PS7/8) or an Intel or Xilinx SPI controller core.
PS7
It has 2 SPIs: SPIO0 and SPIO1, as in the documentation.
Correlation between the naming from HDL and doc.
The default value from the table is the one put normally in the HDL design if that SPI port is not used.
As per page 18 from the PG082:
HDL naming | Doc naming | Default |
spi0_clk_i | spi0_sclk_i | 0 |
spi0_clk_o | spi0_sclk_o | -- |
-- | spi0_sclk_t | -- |
spi0_sdi_i | spi0_miso_i | 0 |
-- | spi0_miso_o | -- |
-- | spi0_mosi_t | -- |
spi0_sdo_i | spi0_mosi_i | 0 |
spi0_sdo_o | spi0_miso_o | -- |
-- | spi0_miso_t | -- |
spi0_csn_i | spi0_ss_i | 1 |
spi0_csn_2_o | spi0_ss2_o | -- |
spi0_csn_1_o | spi0_ss1_o | -- |
spi0_csn_0_o | spi0_ss0_o | -- |
-- | spi0_ss_t | -- |
spi1_clk_i | spi1_sclk_i | 0 |
spi1_clk_o | spi1_sclk_o | -- |
-- | spi1_sclk_t | -- |
spi1_sdi_i | spi1_miso_i | 0 |
-- | spi1_miso_o | -- |
-- | spi1_mosi_t | -- |
spi1_sdo_i | spi1_mosi_i | 0 |
spi1_sdo_o | spi1_miso_o | -- |
-- | spi1_miso_t | -- |
spi1_csn_i | spi1_ss_i | 1 |
spi1_csn_2_o | spi1_ss2_o | -- |
spi1_csn_1_o | spi1_ss1_o | -- |
spi1_csn_0_o | spi1_ss0_o | -- |
-- | spi1_ss_t | -- |
PS8 (Zynq PSU)
It has 2 SPIs: SPIO0 and SPIO1, as in the documentation.
Correlation between the naming from HDL and doc.
The default value
GND
from the table is the one put in the base design, in projects/common/carrier/carrier_system_bd.tcl. These default values are to be used when that
SPI connection is not used.
If there is no HDL naming, it means it's not used in our designs.
Where N
is present, it represents the number of the slave component
spi0/1_csn
is a concatenation of all the spi0_N_ss_o_n
signals
As per page 92 from the documentation:
HDL naming | Doc naming | Default |
-- | spi0_sclk_i | GND |
spi0_sclk | spi0_sclk_o | -- |
-- | spi0_sclk_t | -- |
spi0_miso | spi0_m_i | 0 |
spi0_mosi | spi0_m_o | -- |
-- | spi0_mo_t | -- |
-- | spi0_s_i | GND |
-- | spi0_s_o | -- |
spi0_csn | spi0_N_ss_o_n | -- |
-- | spi0_ss_N_t | -- |
-- | spi1_sclk_i | GND |
spi1_sclk | spi1_sclk_o | -- |
-- | spi1_sclk_t | -- |
spi1_miso | spi1_m_i | 0 |
spi1_mosi | spi1_m_o | -- |
-- | spi1_mo_t | -- |
-- | spi1_s_i | GND |
-- | spi1_s_o | -- |
spi1_csn | spi1_N_ss_o_n | -- |
-- | spi1_ss_N_t | -- |
Microblaze
HPS
I2C/I2S/SPDIF
A couple of carrier boards require these standard interfaces for different purposes, for example, a configuration interface for an audio peripheral device. These peripherals do not necessarily have vital roles in the reference design, it's more like a generic goal to support all the provided peripherals of the carrier board.
HDMI
There is HDMI support for all the carriers which are using the ADV7511 as HDMI transmitter. The HDMI transmitter core can be found here.
GPIOs
The general rule of thumb is to define 64 GPIO pins for the base design. The 32 LSB bit will be assigned to switches, buttons and/or LEDs, which can be found on the carrier board. The 32 MSB bits can be used for the FMC board.
Connectivity
These interfaces designs are borrowed from the golden reference design of the board.
Board design
Board capabilities
Board capabilities - Xilinx
Board name | Boots from | FMC connector 1 | FMC connector 2 |
AC701 | JTAG | HPC (2 GTP @ 6.6Gbps) | — |
Cora Z7-07S | SD card | — | — |
KC705 | JTAG | HPC (4 GTX @ 10.3125 Gbps) | LPC (1 GTX @ 10.3125 Gbps) |
KCU105 | JTAG | HPC (8 GTH @ 16.3 Gbps) | LPC (1 GTH @ 16.3 Gbps) |
Microzed | JTAG | — | — |
VC707 | JTAG | HPC (8 GTX @ 12.5 Gbps) | HPC (8 GTX @ 12.5 Gbps) |
VC709 | JTAG | HPC (10 GTH @ 13.1 Gbps) | — |
VCK190 | SD card | FMC+ (12 GTY @ 28.21 Gbps) | FMC+ (12 GTY @ 28.21 Gbps) |
VCU118 | JTAG | FMC+ (24 GTY @ 28.21 Gbps) | LPC |
VCU128 | JTAG | FMC+ (24 GTY @ 28.21 Gbps) | — |
VMK180 | SD card | FMC+ (12 GTY @ 28.21 Gbps) | FMC+ (12 GTY @ 28.21 Gbps) |
ZC702 | SD card | LPC | LPC |
ZC706 | SD card | HPC (8 GTX @ 10.3125 Gbps) | LPC (1 GTX @ 10.3125 Gbps) |
ZCU102 | SD card | HPC (8 GTH @ 16.3 Gbps) | HPC (8 GTH @ 16.3 Gbps) |
Zedboard | SD card | LPC | — |
VADJ values
Board name | FMC 1 | FMC 2 | Family |
AC701 | 3.3V/*2.5V/1.8V | — | Artix-7 |
Cora Z7-07S | — | — | Zynq-7000 |
KC705 | 3.3V/*2.5V/1.8V | 3.3V/*2.5V/1.8V | Kintex-7 |
KCU105 | *1.8V/1.5V/1.2V | *1.8V/1.5V/1.2V | Kintex UltraScale |
Microzed | — | — | Zynq-7000 |
VC707 | *1.8V/1.5V/1.2V | *1.8V/1.5V/1.2V | Virtex-7 |
VC709 | *1.8V | — | Virtex-7 |
VCK190 | *1.5V/1.2V | *1.5V/1.2V | Versal |
VCU118 | *1.8V/1.5V/1.2V | *1.8V/1.5V/1.2V | Virtex UltraScale+ |
VCU128 | *1.8V/1.5V/1.2V | — | Virtex UltraScale+ |
VMK180 | *1.5V/1.2V | *1.5V/1.2V | Versal |
ZC702 | 3.3V/*2.5V/1.8V | 3.3V/*2.5V/1.8V | Zynq-7000 |
ZC706 | 3.3V/*2.5V/1.8V | 3.3V/*2.5V/1.8V | Zynq-7000 |
ZCU102 | *1.8V/1.5V/1.2V | *1.8V/1.5V/1.2V | Zynq UltraScale+ MP |
Zedboard | 3.3V/2.5V/*1.8V | — | Zynq-7000 |
(* bold) = default VADJ
FMC1 & FMC2 columns → depending on the power supply of the device connected to the FMC, the custom VADJ will have the value supported by both the carrier and the device(s)
Board capabilities
Board capabilities - Intel
Board name | FMC connector 1 | FMC connector 2 |
A10GX | LPC () | HPC (8 x 17.4 Gbps) |
A10SOC | HPC (8) | LPC (8) |
Stratix10SoC | FMC+ (24 @ 28.3 Gbps) | FMC+ (24 @ 28.3 Gbps) |
VADJ values
Board name | FMC 1 | FMC 2 |
A10GX | *1.8V/1.5V/1.35V/1.2V | *1.8V/1.5V/1.35V/1.2V |
A10SOC | *1.8V/1.5V/1.35V/1.25V/1.2V/1.1V | *1.8V/1.5V/1.35V/1.2V/1.1V |
Stratix10SoC | *3.3V/1.8V/1.2V | *3.3V/1.8V/1.2V |
(* bold) = default VADJ
FMC1 & FMC2 columns → depending on the power supply of the device connected to the FMC, the custom VADJ will have the value supported by both the carrier and the device(s)
File structure of a project
Project files for Xilinx boards
A project for a Xilinx FPGA board should contain the following files:
system_bd.tcl — sources the base design first, then the board design, and afterwards it contains all the IP instances and connections that must be added on top of the sourced files, to complete the design of the project (these are specific to the combination of this carrier and board)
system_constr.xdc — constraints file of the design; it’s the connection between the physical pins of the FPGA that you want to use and the HDL code that describes the behavior; here you define the FMC I/O pins, board-specific clock signals, timing constraints, etc. The constraints specific to the carrier are imported in the system_project.tcl file
system_top.v — contains everything about the HDL part of the project; it instantiates the system_wrapper module, IO buffers, I/ODDRs, modules that transform signals from LVDS to single-ended, etc. The I/O ports of this Verilog module will be connected to actual I/O pads of the FPGA.
Project files for Intel boards
A project for an Intel FPGA board should contain the following files:
system_qsys.tcl — also called platform designer; sources the base design first, then the board design, and afterwards it contains all the IP instances and connections that must be added on top of the sourced files, to complete the design of the project (these are specific to the combination of this carrier and board)
system_top.v — contains everything about the HDL part of the project; it instantiates the system_wrapper module, IO buffers, I/ODDRs, modules that transform signals from LVDS to single-ended, etc. The I/O ports of this Verilog module will be connected to actual I/O pads of the FPGA
Examples
Some carriers have a different name for these files, for example A10SoC has constraints file for both PL side and PS side: