This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:docs:arch [19 Oct 2021 13:30] – Edit footer Iulia Moldovan | resources:fpga:docs:arch [03 Nov 2021 11:34] – Integrate board capabilities Iulia Moldovan | ||
---|---|---|---|
Line 5: | Line 5: | ||
* The **board design**, which is a direct integration of all the necessary IPs into a specific base design in order to support an FMC I/O board. These designs are carrier independent and common to all carrier boards. | * The **board design**, which is a direct integration of all the necessary IPs into a specific base design in order to support an FMC I/O board. These designs are carrier independent and common to all carrier boards. | ||
- | Currently ADI provides base designs for the following prototyping boards: | + | {{page>: |
- | + | {{page>:resources:fpga:docs:arch:intel_platforms## | |
- | ^Intel ^Xilinx | + | |
- | | [[https:// | + | |
- | | [[https:// | + | |
- | | [[https:// | + | |
- | | [[http:// | + | |
- | | | [[xilinx> | + | |
- | | | [[xilinx> | + | |
- | | | [[xilinx> | + | |
- | | | [[http:// | + | |
- | | | [[http:// | + | |