This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:fpga:altera:ced1z:ad7766 [05 Nov 2012 21:20] – [Software Tools] Andrei Cozma | resources:fpga:altera:ced1z:ad7766 [11 Jan 2021 09:38] (current) – Fixed bad links for AD7766 Ioana Chelaru | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Supported Devices ===== | ===== Supported Devices ===== | ||
- | * [[adi> | + | * [[adi>AD7766|AD7766-1]] |
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
Line 11: | Line 11: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi>AD7766-1|EVAL-AD7766-1EDZ]]** evaluation board together with the **[[adi> | + | This document presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
Line 17: | Line 17: | ||
The CED1Z board is intended for use in evaluation, demonstration and development of systems using Analog Devices precision converters. It provides the necessary communications between the converter and the PC, programming or controlling the device, transmitting or receiving data over a USB link. | The CED1Z board is intended for use in evaluation, demonstration and development of systems using Analog Devices precision converters. It provides the necessary communications between the converter and the PC, programming or controlling the device, transmitting or receiving data over a USB link. | ||
- | The [[adi> | + | The [[adi> |
===== More information ===== | ===== More information ===== | ||
- | * [[adi> | + | * [[adi> |
* [[adi>/ | * [[adi>/ | ||
* [[http:// | * [[http:// |