This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:fpga:altera:bemicro:common_spi_i2c [20 Sep 2011 12:55] – [FPGA Components] Andrei Cozma | resources:fpga:altera:bemicro:common_spi_i2c [05 Jan 2012 14:21] – [FPGA Design] Andrei Cozma | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== FPGA Design ====== | ||
- | |||
The lab is delivered together with a set of design files that are used to evaluate the ADI part. The FPGA image that must be loaded into the BeMicroSDK FPGA is included in the design files. This section presents the components included in the FPGA image and also the procedure to load the image into the FPGA. | The lab is delivered together with a set of design files that are used to evaluate the ADI part. The FPGA image that must be loaded into the BeMicroSDK FPGA is included in the design files. This section presents the components included in the FPGA image and also the procedure to load the image into the FPGA. | ||