This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:altera:bemicro:common [15 Sep 2011 15:47] – removed a section Andrei Cozma | resources:fpga:altera:bemicro:common [03 Jan 2013 20:42] (current) – external edit 127.0.0.1 | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== NIOS II Software Design ====== | ||
- | |||
This section presents the steps for developing a software application that will run on the **BeMicroSDK** system and will be used for controlling and monitoring the operation of the ADI evaluation board. | This section presents the steps for developing a software application that will run on the **BeMicroSDK** system and will be used for controlling and monitoring the operation of the ADI evaluation board. | ||
Line 8: | Line 6: | ||
Launch the **Nios II SBT** from the **//Start -> All Programs -> Altera -> Nios II EDS 11.0 -> Nios II 11.0 | Launch the **Nios II SBT** from the **//Start -> All Programs -> Altera -> Nios II EDS 11.0 -> Nios II 11.0 | ||
Software Build Tools for Eclipse (SBT)//**. | Software Build Tools for Eclipse (SBT)//**. | ||
- | <note tip> | + | <WRAP tip> |
=== 1. Initialize Eclipse workspace === | === 1. Initialize Eclipse workspace === | ||
- | * When Eclipse first launches, a dialog box appears asking what directory it should use for its workspace. It is useful to have a separate Eclipse workspace associated with each hardware project that is created in SOPC Builder. Browse to the **//ADIEvalBoardsLab//** directory and click //**Make New Folder**// to create a folder for the software project. Name the new folder “// | + | * When Eclipse first launches, a dialog box appears asking what directory it should use for its workspace. It is useful to have a separate Eclipse workspace associated with each hardware project that is created in SOPC Builder. Browse to the **//ADIEvalBoardLab//** directory and click //**Make New Folder**// to create a folder for the software project. Name the new folder “// |
- | {{: | + | {{ : |
=== 2. Create a new software project in the SBT === | === 2. Create a new software project in the SBT === | ||
Line 23: | Line 21: | ||
* Click the **// | * Click the **// | ||
- | * Select the **// | + | * Select the **// |
- | * Set the name of the Application project to “**//ADIEvalBoardsDemo//**”. | + | * Set the name of the Application project to “**//ADIEvalBoard//**”. |
* Select the **//Blank Project//** template under **//Project template// | * Select the **//Blank Project//** template under **//Project template// | ||
* Click the **// | * Click the **// | ||
- | {{ : | + | {{ : |
The tool will create two new software project directories. Each Nios II application has 2 project directories in the Eclipse workspace. | The tool will create two new software project directories. Each Nios II application has 2 project directories in the Eclipse workspace. | ||
Line 34: | Line 32: | ||
* The second is the **//Board Support Package (BSP)//** project associated with the main application software project. This project will build the system library drivers for the specific SOPC system. This project inherits the name from the main software project and appends “**// | * The second is the **//Board Support Package (BSP)//** project associated with the main application software project. This project will build the system library drivers for the specific SOPC system. This project inherits the name from the main software project and appends “**// | ||
- | {{ : | + | {{ : |
Since you chose the blank project template, there are no source files in the application project directory at this time. The BSP contains a directory of software drivers as well as a system.h header file, system initialization source code and other software infrastructure. | Since you chose the blank project template, there are no source files in the application project directory at this time. The BSP contains a directory of software drivers as well as a system.h header file, system initialization source code and other software infrastructure. | ||
Line 42: | Line 40: | ||
* Configure the board support package to specify the properties of this software system by using the **//BSP Editor//** tool. These properties include what interface should be used for //stdio// and //stderr// messages, the memory in which stack and heap should be allocated and whether an operating system or network stack should be included with this BSP. | * Configure the board support package to specify the properties of this software system by using the **//BSP Editor//** tool. These properties include what interface should be used for //stdio// and //stderr// messages, the memory in which stack and heap should be allocated and whether an operating system or network stack should be included with this BSP. | ||
- | * Right click on the **//ADIEvalBoardsDemo_bsp//** project and select **//Nios II -> BSP Editor…// | + | * Right click on the **//ADIEvalBoard_bsp//** project and select **//Nios II -> BSP Editor…// |
- | {{ : | + | {{ : |
The software project provided in this lab does not make use of an operating system. All //stdout//, //stdin// and //stderr// messages will be directed to the // | The software project provided in this lab does not make use of an operating system. All //stdout//, //stdin// and //stderr// messages will be directed to the // | ||
Line 60: | Line 58: | ||
In addition to the board support package settings configured using the **//BSP Editor//**, there are other compilation settings managed by the Eclipse environment such as compiler flags and optimization level. | In addition to the board support package settings configured using the **//BSP Editor//**, there are other compilation settings managed by the Eclipse environment such as compiler flags and optimization level. | ||
- | * Right click on the **//ADIEvalBoardsDemo_bsp//** software project and select **// | + | * Right click on the **//ADIEvalBoard_bsp//** software project and select **// |
* On the left-hand menu, select **//Nios II BSP Properties// | * On the left-hand menu, select **//Nios II BSP Properties// | ||
* During compilation, | * During compilation, | ||
* Since our software does not make use of C++, uncheck **//Support C++//**. | * Since our software does not make use of C++, uncheck **//Support C++//**. | ||
+ | * Check the **//Reduced device drivers//** option | ||
+ | * Check the **//Small C library//** option | ||
* Press **// | * Press **// | ||
- | {{ : | + | {{ : |
===== Add source code to the project ===== | ===== Add source code to the project ===== | ||
- | In Windows Explorer locate the project directory which contains a directory called **// | + | In Windows Explorer locate the project directory which contains a directory called **// |
- | * Select all the files and folders and drag them over the **//ADIEvalBoardsDemo//** project in the SBT window and drop the files onto the project folder. | + | * Select all the files and folders and drag them over the **//ADIEvalBoard//** project in the SBT window and drop the files onto the project folder. |
- | {{ : | + | {{ : |
* A dialog box will appear to select the desired operation. Select the option **//Copy files and folders//** and press **//OK//**. | * A dialog box will appear to select the desired operation. Select the option **//Copy files and folders//** and press **//OK//**. | ||
Line 82: | Line 82: | ||
* This should cause the source files to be physically copied into the file system location of the software project directory and register these source files within the Eclipse workspace so that they appear in the Project Explorer file listing. | * This should cause the source files to be physically copied into the file system location of the software project directory and register these source files within the Eclipse workspace so that they appear in the Project Explorer file listing. | ||
- | {{ : | + | {{ : |
===== Configure Application Project Build Properties ===== | ===== Configure Application Project Build Properties ===== | ||
- | Just as you configured the optimization level for the BSP project, you should set the optimization level for the application software project **//ADIEvalBoardsDemo//** as well. | + | Just as you configured the optimization level for the BSP project, you should set the optimization level for the application software project **//ADIEvalBoard//** as well. |
- | * Right click on the **//ADIEvalBoardsDemo//** software project and select **// | + | * Right click on the **//ADIEvalBoard//** software project and select **// |
* On the left-hand menu, select the **//Nios II Application Properties// | * On the left-hand menu, select the **//Nios II Application Properties// | ||
* Change the **// | * Change the **// | ||
* Press **// | * Press **// | ||
- | {{ : | + | {{ : |
===== Define Application Include Directories ===== | ===== Define Application Include Directories ===== | ||
Line 100: | Line 100: | ||
* Click the **// | * Click the **// | ||
- | {{ : | + | {{ : |
* Double click on **// | * Double click on **// | ||
* If you see the message shown here about resources being out of sync, right click on the **// | * If you see the message shown here about resources being out of sync, right click on the **// | ||
- | {{ : | + | {{ : |
* Select the line **APP_INCLUDE_DIRS :=** | * Select the line **APP_INCLUDE_DIRS :=** | ||
Line 121: | Line 121: | ||
=== 1. Build the Application and BSP Projects === | === 1. Build the Application and BSP Projects === | ||
- | * Right click the **//ADIEvalBoardsDemo_bsp//** software project and choose **//Build Project//** to build the board support package. | + | * Right click the **//ADIEvalBoard_bsp//** software project and choose **//Build Project//** to build the board support package. |
- | * When that build completes, right click the **//ADIEvalBoardsDemo//** application software project and choose **//Build Project//** to build the Nios II application. | + | * When that build completes, right click the **//ADIEvalBoard//** application software project and choose **//Build Project//** to build the Nios II application. |
- | These 2 steps will compile and build the associated board support package, then the actual application software project itself. The result of the compilation process will be an // | + | These 2 steps will compile and build the associated board support package, then the actual application software project itself. The result of the compilation process will be an // |
- | {{: | + | {{: |
+ | {{: | ||
=== 2. Verify the Board Connection === | === 2. Verify the Board Connection === | ||
Line 132: | Line 133: | ||
The **BeMicroSDK** hardware is designed with a //System ID// peripheral. This peripheral is assigned a unique value based on when the hardware design was last modified in the SOPC Builder tool. SOPC Builder also places this information in the // | The **BeMicroSDK** hardware is designed with a //System ID// peripheral. This peripheral is assigned a unique value based on when the hardware design was last modified in the SOPC Builder tool. SOPC Builder also places this information in the // | ||
- | * Select the **//ADIEvalBoardsDemo//** application software project. | + | * Select the **//ADIEvalBoard//** application software project. |
* Select **//Run -> Run Configurations…// | * Select **//Run -> Run Configurations…// | ||
* Select the **//Nios II Hardware// | * Select the **//Nios II Hardware// | ||
Line 138: | Line 139: | ||
* Change the configuration name to **// | * Change the configuration name to **// | ||
* On the **//Target Connection// | * On the **//Target Connection// | ||
- | * Select the **//jtag_uart_1//** as the **//Byte Stream Device//** for // | + | * Select the **//jtag_uart//** as the **//Byte Stream Device//** for // |
- | * Check the **//Ignore mismatched system ID// | + | * Check the **//Ignore mismatched system ID option//**. |
- | * Check the //**Ignore mismatched system timestamp**// option. | + | * Check the **//Ignore mismatched system timestamp |
- | {{: | + | {{: |
{{: | {{: | ||
- | {{ : | + | {{ : |
=== 3. Run the Software Project on the Target === | === 3. Run the Software Project on the Target === | ||
Line 157: | Line 158: | ||
{{ : | {{ : | ||
- | <note>The code size and start address might be different than the ones displayed in the above screenshot.</ | + | <WRAP round help>The code size and start address might be different than the ones displayed in the above screenshot.</ |