This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:fpga:altera:bemicro:common [16 Sep 2011 15:23] – updated the pictures Andrei Cozma | resources:fpga:altera:bemicro:common [27 Jan 2012 16:25] – Approved Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== NIOS II Software Design ====== | ||
- | |||
This section presents the steps for developing a software application that will run on the **BeMicroSDK** system and will be used for controlling and monitoring the operation of the ADI evaluation board. | This section presents the steps for developing a software application that will run on the **BeMicroSDK** system and will be used for controlling and monitoring the operation of the ADI evaluation board. | ||
Line 64: | Line 62: | ||
* During compilation, | * During compilation, | ||
* Since our software does not make use of C++, uncheck **//Support C++//**. | * Since our software does not make use of C++, uncheck **//Support C++//**. | ||
+ | * Check the **//Reduced device drivers//** option | ||
+ | * Check the **//Small C library//** option | ||
* Press **// | * Press **// | ||
Line 139: | Line 139: | ||
* Change the configuration name to **// | * Change the configuration name to **// | ||
* On the **//Target Connection// | * On the **//Target Connection// | ||
- | * Select the **//jtag_uart_1//** as the **//Byte Stream Device//** for //stdio//. | + | * Select the **//jtag_uart//** as the **//Byte Stream Device//** for //stdio//. |
+ | * Check the **//Ignore mismatched system ID option// | ||
+ | * Check the **//Ignore mismatched system timestamp option//**. | ||
{{: | {{: | ||
{{: | {{: | ||
- | {{ : | + | {{ : |
=== 3. Run the Software Project on the Target === | === 3. Run the Software Project on the Target === |