This shows you the differences between two versions of the page.
Last revisionBoth sides next revision | |||
resources:fpga:altera:bemicro:ad7656-1 [17 Oct 2012 09:36] – created Adrian Costina | resources:fpga:altera:bemicro:ad7656-1 [03 Jan 2013 20:42] – external edit | ||
---|---|---|---|
Line 175: | Line 175: | ||
After the FPGA is correctly programmed the data acquisition process can start by executing the data_capture.bat script. The data_capture.tcl file can be modified to acquire a variable number of channels. | After the FPGA is correctly programmed the data acquisition process can start by executing the data_capture.bat script. The data_capture.tcl file can be modified to acquire a variable number of channels. | ||
- | <note>The configuration from data_capture.tcl is performed the first time the script is executed. If changes are performed after that, the system must be reinitialized by reprogramming the FPGA.</note> | + | <WRAP round help>The configuration from data_capture.tcl is performed the first time the script is executed. If changes are performed after that, the system must be reinitialized by reprogramming the FPGA.</WRAP> |
{{ : | {{ : |