This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:altera:bemicro:ad5542a [26 Oct 2011 15:24] – [AD5542A: 2.7 V to 5.5 V, Serial-Input, Voltage-Output, 16-Bit nanoDAC™] Andrei Cozma | resources:fpga:altera:bemicro:ad5542a [26 Jan 2021 01:21] (current) – update arrow links after their web site update Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== BeMicro FPGA Project for AD5542A with Nios driver ====== | ====== BeMicro FPGA Project for AD5542A with Nios driver ====== | ||
+ | |||
+ | |||
+ | ===== Supported Devices ===== | ||
+ | |||
+ | * [[adi> | ||
+ | |||
+ | ===== Evaluation Boards ===== | ||
+ | |||
+ | * [[adi> | ||
====== Overview ====== | ====== Overview ====== | ||
- | This lab presents the steps to setup an environment for using the **[[adi> | + | This lab presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
- | For component evaluation and performance purposes, as opposed to quick prototyping, | + | {{page>common_sdp}} |
- | * a controller board, like the **[[resources/ | + | |
- | * an compatible Analog Devices SDP [[adi>sdp# | + | |
- | * corresponding PC software | + | |
- | The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. | + | |
Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5542ASDZ** Evaluation Board. | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5542ASDZ** Evaluation Board. | ||
Line 24: | Line 29: | ||
* [[adi> | * [[adi> | ||
* {{: | * {{: | ||
- | * [[http://www.arrownac.com/solutions/ | + | * [[https://www.intel.com/content/ |
* [[http:// | * [[http:// | ||
- | * [[http:// | + | * [[http:// |
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 36: | Line 41: | ||
Below is presented the list of required hardware items: | Below is presented the list of required hardware items: | ||
- | * Arrow Electronics [[http://www.arrow.com/bemicrosdk/|BeMicro SDK]] FPGA-based MCU Evaluation Board | + | * Arrow Electronics [[https://www.intel.com/content/www/ |
- | * [[http:// | + | * [[adi> |
* **EVAL-AD5542ASDZ** evaluation board | * **EVAL-AD5542ASDZ** evaluation board | ||
* Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory | * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory | ||
Line 47: | Line 52: | ||
* [[http:// | * [[http:// | ||
* [[https:// | * [[https:// | ||
- | * [[http:// | + | * [[http:// |
- | * {{: | + | |
The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web. | The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web. | ||
- | The **Micrium uC/Probe Trial** version is available via download from the web at [[http:// | + | The **Micrium uC/Probe Trial** version |
+ | ===== Downloads ===== | ||
+ | * {{: | ||
===== Extract the Lab Files ===== | ===== Extract the Lab Files ===== | ||
Line 65: | Line 70: | ||
{{page> | {{page> | ||
+ | ====== Quick Evaluation ====== | ||
{{page> | {{page> | ||
+ | ====== FPGA Design ====== | ||
{{page> | {{page> | ||
+ | ====== NIOS II Software Design ====== | ||
{{page> | {{page> | ||
- | |||
====== uC-Probe Interface ====== | ====== uC-Probe Interface ====== | ||
Line 134: | Line 141: | ||
{{page> | {{page> | ||
- |