This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:fpga:altera:bemicro:ad5446 [20 Jul 2012 15:42] – Approved Andrei Cozma | resources:fpga:altera:bemicro:ad5446 [28 Sep 2012 09:28] – Added common section for describing the evaluation setup and System Demonstration Platform Adrian Costina | ||
---|---|---|---|
Line 4: | Line 4: | ||
===== Supported Devices ===== | ===== Supported Devices ===== | ||
+ | * [[adi> | ||
* [[adi> | * [[adi> | ||
- | |||
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
Line 16: | Line 16: | ||
{{ : | {{ : | ||
- | For component evaluation and performance purposes, as opposed to quick prototyping, | + | {{page>common_sdp}} |
- | * a controller board, like the **[[resources/ | + | |
- | * an compatible Analog Devices SDP [[adi>sdp# | + | |
- | * corresponding PC software | + | |
- | The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. | + | |
Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5446SDZ** Evaluation Board. | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5446SDZ** Evaluation Board. |