Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:fpga:altera:bemicro:ad5110 [20 Mar 2012 10:48] – title Alexandru.Tofanresources:fpga:altera:bemicro:ad5110 [26 Jan 2021 01:20] (current) – update arrow links after their web site update Robin Getz
Line 11: Line 11:
 ====== Overview ====== ====== Overview ======
  
-This lab presents the steps to setup an environment for using the **[[adi>EVAL-AD5110SDZ]]** evaluation board together with the **[[http://www.arrownac.com/solutions/bemicro-sdk/|BeMicro SDK]]** USB stick, the Nios II Embedded Development Suite (EDS) and the [[http://micrium.com/page/products/tools/probe|Micrium μC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5110SDZ Evaluation Board with the BeMicro SDK Platform.+This lab presents the steps to setup an environment for using the **[[adi>EVAL-AD5110SDZ]]** evaluation board together with the **[[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]]** USB stick, the Nios II Embedded Development Suite (EDS) and the [[http://micrium.com/tools/ucprobe/overview/|Micrium μC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5110SDZ Evaluation Board with the BeMicro SDK Platform.
  
 {{ :resources:fpga:altera:bemicro:ad5110_bemicro.jpg?400 }} {{ :resources:fpga:altera:bemicro:ad5110_bemicro.jpg?400 }}
  
-For component evaluation and performance purposes, as opposed to quick prototyping, the user is directed to Analog Devices [[/resources/eval/sdp|System Demonstration Platform]] (**SDP**). The **SDP** consists of a: +{{page>common_sdp}}
-  * a controller board, like the **[[resources/eval/sdp/sdp-b|EVAL-SDP-CB1Z]] (SDP-B)** +
-  * an compatible Analog Devices SDP [[adi>sdp#exallist|product evaluation board]] +
-  * corresponding PC software +
-The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software.  Each SDP evaluation daughter board includes the necessary installation files needed for this performance testing. It's expected that the analog performance on the two platforms may differ.+
  
 Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5110SDZ** Evaluation Board. Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5110SDZ** Evaluation Board.
Line 34: Line 30:
   * [[adi>AD5110|AD5110 Product Info]] - pricing, samples, datasheet   * [[adi>AD5110|AD5110 Product Info]] - pricing, samples, datasheet
   * [[adi>/static/imported-files/user_guides/UG-323.pdf|EVAL-AD5110SDZ evaluation board user guide]]   * [[adi>/static/imported-files/user_guides/UG-323.pdf|EVAL-AD5110SDZ evaluation board user guide]]
-  * [[http://www.arrownac.com/solutions/bemicro-sdk|BeMicro SDK]]+  * [[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]]
   * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]]   * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]]
-  * [[http://micrium.com/page/products/tools/probe|Micrium uC-Probe]]+  * [[http://micrium.com/tools/ucprobe/overview/|Micrium uC-Probe]]
  
 ====== Getting Started ====== ====== Getting Started ======
Line 46: Line 42:
  
 Below is presented the list of required hardware items: Below is presented the list of required hardware items:
-  * Arrow Electronics [[http://www.arrow.com/bemicrosdk/|BeMicro SDK]] FPGA-based MCU Evaluation Board +  * Arrow Electronics [[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]] FPGA-based MCU Evaluation Board 
-  * [[http://www.arrownac.com/solutions/adi_interposer/|BeMicro SDK/SDP Interposer]] adapter board+  * [[adi>sdp-bemicro|BeMicro SDK/SDP Interposer]] adapter board
   * **EVAL-AD5110SDZ** evaluation board   * **EVAL-AD5110SDZ** evaluation board
   * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory   * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory
Line 57: Line 53:
   * [[http://www.altera.com/products/software/quartus-ii/web-edition/qts-we-index.html|Quartus II Web Edition]] design software v11.0   * [[http://www.altera.com/products/software/quartus-ii/web-edition/qts-we-index.html|Quartus II Web Edition]] design software v11.0
   * [[https://www.altera.com/download/software/nios-ii|Nios II EDS]] v11.0   * [[https://www.altera.com/download/software/nios-ii|Nios II EDS]] v11.0
-  * [[http://micrium.com/page/products/tools/probe|uC-Probe]] run-time monitoring tool +  * [[http://micrium.com/tools/ucprobe/trial/|uC-Probe]] run-time monitoring tool, version 2.5
-  * {{:resources:fpga:altera:bemicro:ad5110_evalboardlab.zip|Lab Design Files}}+
  
 The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web.  The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web. 
  
-The **Micrium uC/Probe Trial** version is available via download from the web at [[http://micrium.com/download/Micrium-uC-Probe-Setup-Trial.exe]].  After installation add to the “Path” system variable the entry "//%QUARTUS_ROOTDIR%\bin\//“ on the third position in the list. +The **Micrium uC/Probe Trial** version 2.5 is available via download from the web at [[http://micrium.com/tools/ucprobe/trial/]].  After installation add to the “Path” system variable the entry "//%QUARTUS_ROOTDIR%\bin\//“ on the third position in the list.
  
 +===== Downloads =====
 +  * {{:resources:fpga:altera:bemicro:ad5110_evalboardlab.zip|Lab Design Files}}
 ===== Extract the Lab Files ===== ===== Extract the Lab Files =====
  
Line 161: Line 157:
  
 {{page>troubleshooting}} {{page>troubleshooting}}
- 
resources/fpga/altera/bemicro/ad5110.txt · Last modified: 26 Jan 2021 01:20 by Robin Getz