Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:fpga:altera:bemicro:ad5110 [28 Sep 2012 09:47] – Added common section for describing the evaluation setup and System Demonstration Platform Adrian Costinaresources:fpga:altera:bemicro:ad5110 [26 Jan 2021 01:20] (current) – update arrow links after their web site update Robin Getz
Line 11: Line 11:
 ====== Overview ====== ====== Overview ======
  
-This lab presents the steps to setup an environment for using the **[[adi>EVAL-AD5110SDZ]]** evaluation board together with the **[[http://www.arrownac.com/solutions/bemicro-sdk/|BeMicro SDK]]** USB stick, the Nios II Embedded Development Suite (EDS) and the [[http://micrium.com/page/products/tools/probe|Micrium μC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5110SDZ Evaluation Board with the BeMicro SDK Platform.+This lab presents the steps to setup an environment for using the **[[adi>EVAL-AD5110SDZ]]** evaluation board together with the **[[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]]** USB stick, the Nios II Embedded Development Suite (EDS) and the [[http://micrium.com/tools/ucprobe/overview/|Micrium μC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5110SDZ Evaluation Board with the BeMicro SDK Platform.
  
 {{ :resources:fpga:altera:bemicro:ad5110_bemicro.jpg?400 }} {{ :resources:fpga:altera:bemicro:ad5110_bemicro.jpg?400 }}
Line 30: Line 30:
   * [[adi>AD5110|AD5110 Product Info]] - pricing, samples, datasheet   * [[adi>AD5110|AD5110 Product Info]] - pricing, samples, datasheet
   * [[adi>/static/imported-files/user_guides/UG-323.pdf|EVAL-AD5110SDZ evaluation board user guide]]   * [[adi>/static/imported-files/user_guides/UG-323.pdf|EVAL-AD5110SDZ evaluation board user guide]]
-  * [[http://www.arrownac.com/solutions/bemicro-sdk|BeMicro SDK]]+  * [[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]]
   * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]]   * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]]
-  * [[http://micrium.com/page/products/tools/probe|Micrium uC-Probe]]+  * [[http://micrium.com/tools/ucprobe/overview/|Micrium uC-Probe]]
  
 ====== Getting Started ====== ====== Getting Started ======
Line 42: Line 42:
  
 Below is presented the list of required hardware items: Below is presented the list of required hardware items:
-  * Arrow Electronics [[http://www.arrow.com/bemicrosdk/|BeMicro SDK]] FPGA-based MCU Evaluation Board +  * Arrow Electronics [[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]] FPGA-based MCU Evaluation Board 
-  * [[http://www.arrownac.com/solutions/adi_interposer/|BeMicro SDK/SDP Interposer]] adapter board+  * [[adi>sdp-bemicro|BeMicro SDK/SDP Interposer]] adapter board
   * **EVAL-AD5110SDZ** evaluation board   * **EVAL-AD5110SDZ** evaluation board
   * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory   * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory
Line 53: Line 53:
   * [[http://www.altera.com/products/software/quartus-ii/web-edition/qts-we-index.html|Quartus II Web Edition]] design software v11.0   * [[http://www.altera.com/products/software/quartus-ii/web-edition/qts-we-index.html|Quartus II Web Edition]] design software v11.0
   * [[https://www.altera.com/download/software/nios-ii|Nios II EDS]] v11.0   * [[https://www.altera.com/download/software/nios-ii|Nios II EDS]] v11.0
-  * [[http://micrium.com/page/products/tools/probe|uC-Probe]] run-time monitoring tool+  * [[http://micrium.com/tools/ucprobe/trial/|uC-Probe]] run-time monitoring tool, version 2.5
  
 The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web.  The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web. 
  
-The **Micrium uC/Probe Trial** version is available via download from the web at [[http://micrium.com/download/Micrium-uC-Probe-Setup-Trial.exe]].  After installation add to the “Path” system variable the entry "//%QUARTUS_ROOTDIR%\bin\//“ on the third position in the list.+The **Micrium uC/Probe Trial** version 2.5 is available via download from the web at [[http://micrium.com/tools/ucprobe/trial/]].  After installation add to the “Path” system variable the entry "//%QUARTUS_ROOTDIR%\bin\//“ on the third position in the list.
  
 ===== Downloads ===== ===== Downloads =====
Line 157: Line 157:
  
 {{page>troubleshooting}} {{page>troubleshooting}}
- 
resources/fpga/altera/bemicro/ad5110.txt · Last modified: 26 Jan 2021 01:20 by Robin Getz