This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:xud1a:user-guide [19 Sep 2022 12:46] – [PMOD Pinout] fixed part link Sam Ringwood | resources:eval:user-guides:xud1a:user-guide [19 May 2023 20:01] (current) – [Software/Digital Control] Sam Ringwood | ||
---|---|---|---|
Line 7: | Line 7: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
---- | ---- | ||
Line 59: | Line 62: | ||
=== SDP Control === | === SDP Control === | ||
* [[http:// | * [[http:// | ||
- | * {{ : | + | * {{ : |
+ | * {{ {{ : | ||
+ | < | ||
* [[adi> | * [[adi> | ||
Line 84: | Line 89: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
===== LO Signal Chain ===== | ===== LO Signal Chain ===== | ||
Line 91: | Line 96: | ||
By default, the board populates C165 for an external LO source with C61 not installed. The user can remove C165 and re-install on the C61 pad to enabled use of the ADF4371. When using the onboard ADF4371, the default reference is the onboard VCXO with C372 installed and C373 not installed. The user can remove C372 and re-install on the C373 pad to enabled use of the external reference port J3. | By default, the board populates C165 for an external LO source with C61 not installed. The user can remove C165 and re-install on the C61 pad to enabled use of the ADF4371. When using the onboard ADF4371, the default reference is the onboard VCXO with C372 installed and C373 not installed. The user can remove C372 and re-install on the C373 pad to enabled use of the external reference port J3. | ||
+ | < | ||
===== Digital Control ===== | ===== Digital Control ===== | ||
==== PMOD Pinout ==== | ==== PMOD Pinout ==== | ||
Line 96: | Line 102: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
==== Interposer Board ==== | ==== Interposer Board ==== | ||
Line 102: | Line 108: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
+ | |||
+ | ==== Control Logic ==== | ||
+ | The PMOD inputs are fed to a buffer and logic network for simplified board control and quick switching time. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | |||
+ | ^ Channel ^ Mode ^ TXRX0 ^ TXRX1 ^ TXRX2 ^ TXRX3 ^ Rx Gain Mode ^ | ||
+ | | | ||
+ | | ::: | ||
+ | | ::: | ||
+ | | | ||
+ | | ::: | ||
+ | | ::: | ||
+ | | | ||
+ | | ::: | ||
+ | | ::: | ||
+ | | | ||
+ | | ::: | ||
+ | | ::: | ||
+ | <WRAP centeralign> | ||
+ | ^ ADF4371 Output | ||
+ | | 8 - 16 GHz | 1 | | ||
+ | | 16 - 32 GHz | 0 | | ||
+ | <WRAP centeralign> | ||
====== Evaluation ====== | ====== Evaluation ====== |