This is an old revision of the document!
XUD1A Data Set
Data was collected on a total of four samples. With 4 channels each, there are a total of 16 datasets per measurement characterizing the XUD1A boards. Units were tested in a fixed IF configuration (swept LO & swept RF) with an IF Frequency of 4.5 GHz.
Receive High Gain Mode
S Parameters
Figure 1: RX High Gain Mode S11
Figure 2: RX High Gain Mode S21
Figure 3: RX High Gain Mode S22
Figure 4: RX High Gain Mode Noise Figure
IIP3
Figure 5: RX High Gain Mode IIP3
Receive Low Gain Mode
S Parameters
Figure 6: RX Low Gain Mode S11
Figure 7: RX Low Gain Mode S21
Figure 8: RX Low Gain Mode S22
Figure 9: RX Low Gain Mode Noise Figure
IIP3
Figure 10: RX Low Gain Mode IIP3
TX Mode
S Parameters