Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:eval:user-guides:targetting:xilinx_sdsoc [07 Aug 2015 15:58] – Andrei Cozma | resources:eval:user-guides:targetting:xilinx_sdsoc [07 Aug 2015 15:59] (current) – Andrei Cozma |
---|
* Update the HDL design to Vivado 2015.2 by running the //sdsoc_platform/update_hdl.tcl// script. This step needs to be ran only once after downloading the HDL reference design. | * Update the HDL design to Vivado 2015.2 by running the //sdsoc_platform/update_hdl.tcl// script. This step needs to be ran only once after downloading the HDL reference design. |
* Regenerate the IP libraries following the steps described here: http://wiki.analog.com/resources/fpga/docs/hdl. This step needs to be ran only once after downloading the HDL reference design, or every time the IP libraries are modified. | * Regenerate the IP libraries following the steps described here: http://wiki.analog.com/resources/fpga/docs/hdl. This step needs to be ran only once after downloading the HDL reference design, or every time the IP libraries are modified. |
* Generate the SDSoC platform by running the //sdsoc_platform/sdsoc_platform.tcl// script. Before running the script you need to edit it and change line 26 **//set argv [list D:/Xilinx/SDSoC/2015.2/platforms]//** to point to your SDSoC platforms folder. At the end of the process the new platform will be placed in the SDSoC platforms folder and will be named //<board>_<carrier>//, where //<board>// is the name of the FMCOMMSx board and //<carrier>// is the name of the Xilinx carrier, //eg. fmcomms2_zc702// | * Generate the SDSoC platform by running the //sdsoc_platform/sdsoc_platform.tcl// script. Before running the script you need to edit it and change line 26 "//set argv [list C:/Xilinx/SDSoC/2015.2/platforms]//" to point to your SDSoC platforms folder. At the end of the process the new platform will be placed in the SDSoC platforms folder and will be named //<board>_<carrier>//, where //<board>// is the name of the FMCOMMSx board and //<carrier>// is the name of the Xilinx carrier, //eg. fmcomms2_zc702// |
{{ :resources:eval:user-guides:targetting:tcl_update_hdl.png?500 |}} | {{ :resources:eval:user-guides:targetting:tcl_update_hdl.png?500 |}} |
| |