Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:targetting:xilinx_sdsoc [07 Aug 2015 15:44] Andrei Cozmaresources:eval:user-guides:targetting:xilinx_sdsoc [07 Aug 2015 15:59] (current) Andrei Cozma
Line 25: Line 25:
   * Update the HDL design to Vivado 2015.2 by running the //sdsoc_platform/update_hdl.tcl// script. This step needs to be ran only once after downloading the HDL reference design.   * Update the HDL design to Vivado 2015.2 by running the //sdsoc_platform/update_hdl.tcl// script. This step needs to be ran only once after downloading the HDL reference design.
   * Regenerate the IP libraries following the steps described here: http://wiki.analog.com/resources/fpga/docs/hdl. This step needs to be ran only once after downloading the HDL reference design, or every time the IP libraries are modified.   * Regenerate the IP libraries following the steps described here: http://wiki.analog.com/resources/fpga/docs/hdl. This step needs to be ran only once after downloading the HDL reference design, or every time the IP libraries are modified.
-  * Generate the SDSoC platform by running the //sdsoc_platform/sdsoc_platform.tcl// script. At the end of the process the new platform will be placed in the SDSoC platforms folder and will be named //<board>_<carrier>//, where //<board>// is the name of the FMCOMMSx board and //<carrier>// is the name of the Xilinx carrier, //eg. fmcomms2_zc702//+  * Generate the SDSoC platform by running the //sdsoc_platform/sdsoc_platform.tcl// script. Before running the script you need to edit it and change line 26 "//set argv [list C:/Xilinx/SDSoC/2015.2/platforms]//" to point to your SDSoC platforms folder. At the end of the process the new platform will be placed in the SDSoC platforms folder and will be named //<board>_<carrier>//, where //<board>// is the name of the FMCOMMSx board and //<carrier>// is the name of the Xilinx carrier, //eg. fmcomms2_zc702//
 {{ :resources:eval:user-guides:targetting:tcl_update_hdl.png?500 |}} {{ :resources:eval:user-guides:targetting:tcl_update_hdl.png?500 |}}
  
resources/eval/user-guides/targetting/xilinx_sdsoc.txt · Last modified: 07 Aug 2015 15:59 by Andrei Cozma