Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision |
resources:eval:user-guides:targetting:xilinx_sdsoc [17 Jul 2015 13:49] – [FMCOMMSx SDSoC Examples] Andrei Cozma | resources:eval:user-guides:targetting:xilinx_sdsoc [07 Aug 2015 15:58] – Andrei Cozma |
---|
* [[adi>AD-FMComms2-EBZ]] | * [[adi>AD-FMComms2-EBZ]] |
* [[adi>AD-FMComms3-EBZ]] | * [[adi>AD-FMComms3-EBZ]] |
* [[adi>AD-FMComms3-EBZ]] | |
* [[adi>AD-FMComms5-EBZ]] | |
The supported Xilinx Zynq based carriers are: | The supported Xilinx Zynq based carriers are: |
* [[xilinx>ZC702]] | * [[xilinx>ZC702]] |
{{ :resources:eval:user-guides:targetting:sdsoc_platform_folder.png?500 |}} | {{ :resources:eval:user-guides:targetting:sdsoc_platform_folder.png?500 |}} |
* Open Vivado and in the tcl console //cd// to the target project sdsoc folder, //eg. \hdl\projects\fmcomms2\zc702// | * Open Vivado and in the tcl console //cd// to the target project sdsoc folder, //eg. \hdl\projects\fmcomms2\zc702// |
* Update the HDL design to Vivado 2015.2 by running the //sdsoc_platform/update_hdl.tcl// script. | * Update the HDL design to Vivado 2015.2 by running the //sdsoc_platform/update_hdl.tcl// script. This step needs to be ran only once after downloading the HDL reference design. |
* Generate the SDSoC platform by running the //sdsoc_platform/sdsoc_platform.tcl// script. At the end of the process the new platform will be placed in the SDSoC platforms folder and will be named //<board>_<carrier>//, where //<board>// is the name of the FMCOMMSx board and //<carrier>// is the name of the Xilinx carrier, //eg. fmcomms2_zc702// | * Regenerate the IP libraries following the steps described here: http://wiki.analog.com/resources/fpga/docs/hdl. This step needs to be ran only once after downloading the HDL reference design, or every time the IP libraries are modified. |
| * Generate the SDSoC platform by running the //sdsoc_platform/sdsoc_platform.tcl// script. Before running the script you need to edit it and change line 26 **//set argv [list D:/Xilinx/SDSoC/2015.2/platforms]//** to point to your SDSoC platforms folder. At the end of the process the new platform will be placed in the SDSoC platforms folder and will be named //<board>_<carrier>//, where //<board>// is the name of the FMCOMMSx board and //<carrier>// is the name of the Xilinx carrier, //eg. fmcomms2_zc702// |
{{ :resources:eval:user-guides:targetting:tcl_update_hdl.png?500 |}} | {{ :resources:eval:user-guides:targetting:tcl_update_hdl.png?500 |}} |
| |
<WRAP round download 80%> | <WRAP round download 80%> |
* [[https://github.com/analogdevicesinc/hdl/tree/hdl_2015_r1 | Analog Devices HDL reference design]] | * [[https://github.com/analogdevicesinc/hdl/tree/hdl_2015_r1 | Analog Devices HDL reference design]] |
* {{:resources:eval:user-guides:targetting:sdsoc_platform.zip|SDSoC platform generation files}} | * {{:resources:eval:user-guides:targetting:fmcomms2_zc702_sdsoc_platform.zip|FMCOMMS2 + ZC702 SDSoC platform generation files}} |
| * {{:resources:eval:user-guides:targetting:fmcomms2_zc706_sdsoc_platform.zip|FMCOMMS2 + ZC706 SDSoC platform generation files}} |
| * {{:resources:eval:user-guides:targetting:fmcomms3_zc702_sdsoc_platform.zip|FMCOMMS3 + ZC702 SDSoC platform generation files}} |
| * {{:resources:eval:user-guides:targetting:fmcomms3_zc706_sdsoc_platform.zip|FMCOMMS3 + ZC706 SDSoC platform generation files}} |
</WRAP> | </WRAP> |
===== FMCOMMS2 SDSoC Example ===== | ===== FMCOMMS2 SDSoC Example ===== |
* On the newly created SD card copy the //boot.bin// generated by SDSoC in the //sd_card// folder | * On the newly created SD card copy the //boot.bin// generated by SDSoC in the //sd_card// folder |
* Insert the SD card in the Xilinx ZC702 carrier board, connect antennas to the RF ports of the FMCOMMS2 or loopback cables between Rx and Tx, connect the FMCOMMS2 to the ZC702, connect the ZC702 to a HDMI monitor, connect a mouse and keyboard to the ZC702, connect an Ethernet cable to the ZC702, start the system | * Insert the SD card in the Xilinx ZC702 carrier board, connect antennas to the RF ports of the FMCOMMS2 or loopback cables between Rx and Tx, connect the FMCOMMS2 to the ZC702, connect the ZC702 to a HDMI monitor, connect a mouse and keyboard to the ZC702, connect an Ethernet cable to the ZC702, start the system |
- After Linux boots the IIO Oscilloscope starts automatically. In the IIO Oscilloscope configure the Rx and Tx LO frequencies to be the same, eg. 2.4GHz | * After Linux boots the IIO Oscilloscope starts automatically. In the IIO Oscilloscope configure the Rx and Tx LO frequencies to be the same, eg. 2.4GHz |
- In the IIO Oscilloscope configure the Transmit/DDS as shown below. Please make sure to select a file unde ‘DAC Buffer settings’, any file will do, and press the ‘Load’ button. All the DAC Channels must be selected before pressing ‘Load’. | * In the IIO Oscilloscope configure the Transmit/DDS as shown below. Please make sure to select a file unde ‘DAC Buffer settings’, any file will do, and press the //Load// button. All the DAC Channels must be selected before pressing //Load//. |
- Using a program like WinSCP copy from the project folder the //dds_script.sh// to the device’s ///usr/local/bin folder//. The credentials for the SCP connection between the PC and the device are: user – analog, password – analog. In order to configure the SCP connection you need the IP of the device, to get that just type //ifconfig// in a terminal on the device. | * Using a program like WinSCP copy from the project folder the //dds_script.sh// to the device’s ///usr/local/bin folder//. The credentials for the SCP connection between the PC and the device are: user – analog, password – analog. In order to configure the SCP connection you need the IP of the device, to get that just type //ifconfig// in a terminal on the device. |
- Run the //dds_script.sh// as shown below. This will initialize and activate the DDS IP. | * Run the //dds_script.sh// as shown below. This will initialize and activate the DDS IP. |
- On the IIO Oscilloscope select the //voltage0// and //voltage1// channels and press the //Play// button. You should see the DDS waveforms displayed by the IIO Oscilloscope . | * On the IIO Oscilloscope select the //voltage0// and //voltage1// channels and press the //Play// button. You should see the DDS waveforms displayed by the IIO Oscilloscope . |
{{ :resources:eval:user-guides:targetting:dds_out.png?400 |}} | {{ :resources:eval:user-guides:targetting:dds_out.png?400 |}} |
| |