Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:stingray:userguide [27 Apr 2022 17:41] – Sam Ringwood | resources:eval:user-guides:stingray:userguide [18 Dec 2023 23:46] (current) – [Documents] updated sch Sam Ringwood |
---|
====== ADAR1000-EVAL1Z (STINGRAY) ANALOG BEAMFORMING FRONT-END ====== | ====== ADAR1000EVAL1Z (STINGRAY) ANALOG BEAMFORMING FRONT-END ====== |
====== (UNDER CONSTRUCTION) ====== | |
====== GENERAL DESCRIPTION ====== | ====== GENERAL DESCRIPTION ====== |
The ADAR1000-EVAL1Z evaluation board is an analog beamforming front-end designed for testing the performance of the [[adi>adar1000|ADAR1000]] and [[adi>adtr1107|ADTR1107]]. The [[adi>adar1000|ADAR1000]] is an 8 GHz to 16 GHz, 4-Channel, X Band and Ku Band Beamformer IC. The [[adi>adtr1107|ADTR1107]] is a 6 GHz to 18 GHz, Front-End Transmit/Receive module. | The ADAR1000-EVAL1Z evaluation board is an analog beamforming front-end designed for testing the performance of the [[adi>adar1000|ADAR1000]] and [[adi>adtr1107|ADTR1107]]. The [[adi>adar1000|ADAR1000]] is an 8 GHz to 16 GHz, 4-Channel, X Band and Ku Band Beamformer IC. The [[adi>adtr1107|ADTR1107]] is a 6 GHz to 18 GHz, Front-End Transmit/Receive module. |
The ADAR1000-EVAL1Z board consists of 8 RF cells. Each cell contains a core [[adi>adar1000|ADAR1000]] surrounded by four [[adi>adtr1107|ADTR1107s]]. All RF input/outputs on the evaluation board are brought out to SMPM coaxial connectors. There is a 12V power input and all required voltage rails for the board are generated on-board. Digital control of the board as well as the beamformers is enabled using either an [[adi>SDP-S|System Demonstration Platform (SDP-S)]] connector or a dual PMOD interface. Control signals for the board are expected to be 3.3V logic with on-board level translators converting this to the on-chip logic level of 1.8V. | The ADAR1000-EVAL1Z board consists of 8 RF cells. Each cell contains a core [[adi>adar1000|ADAR1000]] surrounded by four [[adi>adtr1107|ADTR1107s]]. All RF input/outputs on the evaluation board are brought out to SMPM coaxial connectors. There is a 12V power input and all required voltage rails for the board are generated on-board. Digital control of the board as well as the beamformers is enabled using either an [[adi>SDP-S|System Demonstration Platform (SDP-S)]] connector or a dual PMOD interface. Control signals for the board are expected to be 3.3V logic with on-board level translators converting this to the on-chip logic level of 1.8V. |
| |
{{ :resources:eval:user-guides:stingray:front.png?direct | ADAR1000-EVAL1Z Board}} | |
<WRAP centeralign>**//Figure 1: ADAR1000-EVAL1Z Board//**</WRAP> | {{ :resources:eval:user-guides:stingray:adar1000eval1z_bottom-web.gif?200 |}} |
| <WRAP centeralign>**//Figure 1A: ADAR1000EVAL1Z Front//**</WRAP> |
| |
| {{ :resources:eval:user-guides:stingray:adar1000eval1z_top-web.gif?200 |}} |
| <WRAP centeralign>**//Figure 1B: ADAR1000EVAL1Z Back//**</WRAP> |
| |
| {{ :resources:eval:user-guides:stingray:adar1000eval1z_top_kit.jpg?200 |}} |
| <WRAP centeralign>**//Figure 1C: ADAR1000EVAL1Z with Heatsink//**</WRAP> |
| |
| {{ :resources:eval:user-guides:stingray:adar1000eval1z_bottom_kit-web.jpg?200 |}} |
| <WRAP centeralign>**//Figure 1D: ADAR1000EVAL1Z with Antenna Tiles//**</WRAP> |
| |
| |
| |
| |
---- | ---- |
===== Main RFICs ===== | ===== Main RFICs ===== |
* {{ :resources:eval:user-guides:stingray:059522a_bom.zip |BOM}} | * {{ :resources:eval:user-guides:stingray:059522a_bom.zip |BOM}} |
* Rev. B/C design: | * Rev. B/C design: |
* {{ :resources:eval:user-guides:stingray:059522b.pdf |Schematic}} | * {{ :resources:eval:user-guides:stingray:02_059522b_top.pdf |Schematic}} |
* {{ :resources:eval:user-guides:stingray:059522b_bom.zip |BOM}} | * {{ :resources:eval:user-guides:stingray:059522b_bom.zip |BOM}} |
===== Hardware ===== | ===== Hardware ===== |
* RF Power Meter (optional) | * RF Power Meter (optional) |
===== Software/Digital Control ===== | ===== Software/Digital Control ===== |
=== SDP Control === | |
* [[http://swdownloads.analog.com/ACE/SDP/SDPDrivers.exe|SDP Drivers]] | |
* {{ :resources:eval:user-guides:stingray:stingray_test.zip |Basic SDP Test Program}} (Windows 10 might try to block this, you'll have to explicitly allow it in your security settings) | |
* [[adi>sdp-s|SDP-S controller board]] | |
| |
=== PMOD Control === | === PMOD Control === |
* Two 12-pin PMOD cables ([[https://www.mouser.com/ProductDetail/Samtec/IDSD-06-D-1800-R?qs=0lQeLiL1qybunuONxYyYYQ%3D%3D|Example]]) | * Two 12-pin PMOD cables ([[https://www.mouser.com/ProductDetail/Samtec/IDSD-06-D-1800-R?qs=0lQeLiL1qybunuONxYyYYQ%3D%3D|Example]]) |
* [[https://www.arduino.cc/|Arduino]] | * [[https://www.arduino.cc/|Arduino]] |
* [[https://www.ftdichip.com/|FTDI]] | * [[https://www.ftdichip.com/|FTDI]] |
| |
| === SDP Control === |
| * [[http://swdownloads.analog.com/ACE/SDP/SDPDrivers.exe|SDP Drivers]] |
| * {{ :resources:eval:user-guides:stingray:stingray_test.zip |Basic SDP Test Program}} (Windows 10 might try to block this, you'll have to explicitly allow it in your security settings) |
| * [[adi>sdp-s|SDP-S controller board]] |
| |
| <note>SDP Control is fine for initial characterization. Recommended to use the linux drivers for end system control for easier software control and software scalability.</note> |
| |
=== Software === | === Software === |
GPIO PINS ARE HI-Z! SEE [[#configuring_the_ltc2992|CONFIGURING THE LTC2992]]** | GPIO PINS ARE HI-Z! SEE [[#configuring_the_ltc2992|CONFIGURING THE LTC2992]]** |
</note> | </note> |
**4.** Initialize the ADAR1000s to put the ADAR1000-EVAL1Z into a known safe state with the ADTR1107 PAs pinched off. See the [[#Recommended ADAR1000 Initialization Sequence]] section for a recommended set of SPI writes. | **4.** Initialize the ADAR1000s to put the ADAR1000-EVAL1Z into a known safe state with the ADTR1107 PAs pinched off. See the [[:resources:eval:user-guides:stingray:userguide#recommended_adar1000_initialization_sequences|Recommended ADAR1000 Initialization Sequences]] section for a recommended set of SPI writes. |
| |
**5.** Now that the ADTR1107 PAs are pinched off, +5V can safely be applied. This is accomplished by pulsing the **+5V_CTRL** signal. Once the +5V rail is up, a green LED (D4) is lit showing that the board is fully powered up. | **5.** Now that the ADTR1107 PAs are pinched off, +5V can safely be applied. This is accomplished by pulsing the **+5V_CTRL** signal. Once the +5V rail is up, a green LED (D4) is lit showing that the board is fully powered up. |
# HOUSEKEEPING | # HOUSEKEEPING |
(0x000, 0x81, 'Reset'), | (0x000, 0x81, 'Reset'), |
| (0x401, 0x02, 'Allow LDO adjustments from user settings'), |
| (0x400, 0x55, 'Adjust LDO Settings'), |
(0x038, 0x60, 'Bypass the beam and bias RAM (enable SPI)'), | (0x038, 0x60, 'Bypass the beam and bias RAM (enable SPI)'), |
(0x02E, 0x7F, 'Enable all Rx channels, LNA, VGA, Vector Mod'), | (0x02E, 0x7F, 'Enable all Rx channels, LNA, VGA, Vector Mod'), |
{{ :resources:eval:user-guides:stingray:channel_mapping_reverse.png?direct | ADAR1000-EVAL1Z Channel Mapping (Back of Board)}} | {{ :resources:eval:user-guides:stingray:channel_mapping_reverse.png?direct | ADAR1000-EVAL1Z Channel Mapping (Back of Board)}} |
<WRAP centeralign>**//Figure 8: ADAR1000-EVAL1Z Channel Mapping (Back of Board)//**</WRAP> | <WRAP centeralign>**//Figure 8: ADAR1000-EVAL1Z Channel Mapping (Back of Board)//**</WRAP> |
| |
| ===== Support ===== |
| For additional questions or support, please visit the Engineering Zone forum at [[ez>ADEF]]. |
| |
| [[resources/eval/user-guides/stingray|ADAR1000EVAL1Z Homepage]] |
| |
| [[:resources:eval:user-guides:x-band-platform|X Band Development Platform]] |