This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:rpd-6lowpan [28 Aug 2018 11:19] – added section evaluation kit Pranit Jadhav | resources:eval:user-guides:rpd-6lowpan [28 Aug 2018 15:00] – [Evaluation Kit] Pranit Jadhav | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== |
Analog Devices offers Rapid 6LoWPAN Protocol—a long range sub-GHz wireless networking solution that leverages the market proven ADF7023 radio transceiver and lowest power ULP processors (ADuCM3029 or ADuCM4050). | Analog Devices offers Rapid 6LoWPAN Protocol—a long range sub-GHz wireless networking solution that leverages the market proven ADF7023 radio transceiver and lowest power ULP processors (ADuCM3029 or ADuCM4050). | ||
- | Rapid 6LoWPAN Protocol uses star-repeater network topology, targeting commercial and industrial applications such as electronic shelf label (ESL), | + | Rapid 6LoWPAN Protocol uses star-repeater network topology, targeting commercial and industrial applications such as Electronic Shelf Label (ESL), |
+ | {{ : | ||
===== Features and Specification ===== | ===== Features and Specification ===== | ||
* Efficient low power network | * Efficient low power network | ||
Line 29: | Line 30: | ||
===== Evaluation Kit ===== | ===== Evaluation Kit ===== | ||
+ | |||
+ | Below are the different kits available for evaluating Rapid-6LoWPAN. | ||
+ | - EV-6LOWPAN-900Z - Rapid-6LoWPAN Evaluation Kit for all the regions except Japan. | ||
+ | - EV-6LOWPAN-900JZ - Rapid-6LoWPAN Evaluation kit with TELEC Certification specific for Japan. | ||
+ | - EV-ENG-ESLNODE1Z - Electronic Shelf Labelling node which should be ordered only if more nodes are required during the evaluation of EV-6LOWPAN-900Z. | ||
+ | |||
+ | Below are the kit contents. | ||
+ | - EV-6LOWPAN-900Z/ | ||
+ | * [[adi> | ||
+ | * EV-DNG-RFMOD-9001Z - USB Dongle which acts as Border Router for Rapid-6LoWPAN Network **(902-958MHz)** | ||
+ | * EV-COG-ADF7023-9Z - [[adi> | ||
+ | * EV-GEAR-EINK1Z - Cog Ecosystem Gear with E-Paper Display from E-INK. | ||
+ | - EV-ENG-ESLNODE1Z | ||
+ | * EV-COG-AD3029LZ - development platform for Analog Devices Ultra Low Power Microcontroller [[adi> | ||
+ | * EV-COG-ADF7023-9Z - [[adi> | ||
+ | * EV-GEAR-EINK1Z - Cog Ecosystem Gear with E-Paper Display from E-INK. | ||
+ | |||
+ | |||