This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:rf-trx-vcxo-and-profiles [03 Jan 2021 21:46] – fix links Robin Getz | resources:eval:user-guides:rf-trx-vcxo-and-profiles [04 Mar 2022 13:17] – [ERROR: 321: Tx Profile IQrate and filter settings are not possible with current CLKPLL frequency] Michael Hennerich | ||
---|---|---|---|
Line 8: | Line 8: | ||
There are limitations with the default hardware configuration in the scenario where a user desired device frequencies are not related to the on-board 122.88MHz VCXO by a rational fraction. Examples of such device clock frequency are: 125MHz, 133.33MHz, 250MHz and 266.66MHz. The document below outlines these limitations as well as explains how they can be overcome with an AD9371 evaluation board hardware modification. Pretty much the same things also apply for all the other devices listed above. | There are limitations with the default hardware configuration in the scenario where a user desired device frequencies are not related to the on-board 122.88MHz VCXO by a rational fraction. Examples of such device clock frequency are: 125MHz, 133.33MHz, 250MHz and 266.66MHz. The document below outlines these limitations as well as explains how they can be overcome with an AD9371 evaluation board hardware modification. Pretty much the same things also apply for all the other devices listed above. | ||
- | * [[https://ez.analog.com/ | + | * [[ez>wide-band-rf-transceivers/ |
This page is supposed to be a system level addition to the aforementioned document with some extra tips and tricks. | This page is supposed to be a system level addition to the aforementioned document with some extra tips and tricks. | ||
Line 62: | Line 62: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[/ |
< | < | ||
Line 343: | Line 343: | ||
// | // | ||
+ | |||
+ | ==== ERROR: 64: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case () ==== | ||
+ | |||
+ | Can be caused by an invalid filter wizard profile. | ||
+ | Please see answer here: [[ez> | ||