This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:rapidnet-ip [19 Nov 2018 07:36] – [Binary Installer] Pranit Jadhav | resources:eval:user-guides:rapidnet-ip [03 Jan 2021 22:04] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== RapidNet IP Wireless Networking Protocol Solution====== | ====== RapidNet IP Wireless Networking Protocol Solution====== | ||
- | RapidNet IP protocol is a long range sub-GHz wireless networking solution that addresses industrial and commercial applications where reliability, | + | [[adi>RapidNet-IP]] protocol is a long range sub-GHz wireless networking solution that addresses industrial and commercial applications where reliability, |
RapidNet IP is a complete point-to-multipoint wireless networking solution operating in sub-GHz worldwide regional bands. RapidNet IP protocol uses star-repeater network topology, enables longer range communication with faster message transmit times. | RapidNet IP is a complete point-to-multipoint wireless networking solution operating in sub-GHz worldwide regional bands. RapidNet IP protocol uses star-repeater network topology, enables longer range communication with faster message transmit times. | ||
Line 35: | Line 35: | ||
===== Software Package ===== | ===== Software Package ===== | ||
+ | |||
+ | Below are the pre-requisites for RapidNet IP for Developing application or running in-build demo. Please follow procedure on how to install IAR and DFP packs on [[resources: | ||
+ | - IAR 8.22.2 | ||
+ | - ADuCM3029 DFP 3.2.0 | ||
+ | - EV-COG-AD3029LZ BSP 3.1.0 | ||
+ | - RapidNet IP Binary installer 1.1.0 - for running the in-built demo | ||
+ | - RapidNet IP Source installer 1.1.0 - for developing applications | ||
+ | |||
RapidNet IP offers below Software Package. | RapidNet IP offers below Software Package. | ||
==== Binary Installer ==== | ==== Binary Installer ==== | ||
- This software pack contains only binary files, tools and document required to run the RapidNet IP application. | - This software pack contains only binary files, tools and document required to run the RapidNet IP application. | ||
- | | + | |
==== Source Installer==== | ==== Source Installer==== | ||
Line 45: | Line 53: | ||
- Follow these steps to download " | - Follow these steps to download " | ||
- Click www.analog.com/ | - Click www.analog.com/ | ||
- | - Fill your details. | + | - Fill required |
- Under ' | - Under ' | ||
- Under ' | - Under ' | ||
Line 83: | Line 91: | ||
* [[resources: | * [[resources: | ||
+ | ===== Additional Resources ===== | ||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | * [[resources: | ||