This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:pzsdr:testing [16 Jun 2022 14:15] – [Power Sequencer] Monica Constandachi | resources:eval:user-guides:pzsdr:testing [20 Feb 2023 13:57] (current) – updated fmc carrier sd card image Monica Constandachi | ||
---|---|---|---|
Line 20: | Line 20: | ||
* The instructions regarding the setup and how to program the sequencer can be found by clicking on the link below. | * The instructions regarding the setup and how to program the sequencer can be found by clicking on the link below. | ||
* After opening the link, follow the steps that use the **USB-SDP-CABLEZ serial I/O Interface**. | * After opening the link, follow the steps that use the **USB-SDP-CABLEZ serial I/O Interface**. | ||
- | * Make sure the sequencer is programmed before starting the production testing | + | |
Line 31: | Line 31: | ||
<WRAP lo round download 80%> | <WRAP lo round download 80%> | ||
- | | + | * **22 June 2022 release ** |
+ | * [[https:// | ||
+ | * **22 January 2016 release ** | ||
* [[http:// | * [[http:// | ||
* Checksum picozed-sdr2-brk-test-2016_01_05.img.xz '' | * Checksum picozed-sdr2-brk-test-2016_01_05.img.xz '' | ||
Line 44: | Line 46: | ||
<WRAP lo round download 80%> | <WRAP lo round download 80%> | ||
+ | * **27 July 2022 release ** | ||
+ | * [[https:// | ||
* **14 August 2020 release ** | * **14 August 2020 release ** | ||
* [[https:// | * [[https:// | ||
</ | </ | ||
+ | <WRAP lo round download 80%> | ||
+ | * **27 July 2022 release ** | ||
+ | * [[https:// | ||
+ | * **22 June 2022 release ** | ||
+ | * [[https:// | ||
+ | </ | ||
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
It is also possible to manually create one using [[/ | It is also possible to manually create one using [[/ | ||
Line 59: | Line 69: | ||
==== Required hardware ==== | ==== Required hardware ==== | ||
- | * Frequency counter with a USB-GPIB port (tested with an [[https:// | + | * Frequency counter with a USB-GPIB port (tested with an [[https:// |
* Raspberry Pi 4 with provided Linux image, keyboard, mouse, micro-HDMI cable, and a monitor with HDMI input; | * Raspberry Pi 4 with provided Linux image, keyboard, mouse, micro-HDMI cable, and a monitor with HDMI input; | ||
* 1 adrv936x_rfsom breakout board and loopback test fixture; | * 1 adrv936x_rfsom breakout board and loopback test fixture; | ||
Line 83: | Line 93: | ||
* Insert the flash drive into the OTG port on the breakout board. Make sure the USB jumper is set to OTG mode on the breakout board, see the image below for confirmation of correct positioning. | * Insert the flash drive into the OTG port on the breakout board. Make sure the USB jumper is set to OTG mode on the breakout board, see the image below for confirmation of correct positioning. | ||
* Insert the frequency counter USB into the Raspberry Pi. | * Insert the frequency counter USB into the Raspberry Pi. | ||
- | * The probes | + | * The "INPUT A" |
Line 100: | Line 110: | ||
{{ : | {{ : | ||
- | Make sure all the required setup explained above is completed and the frequency counter is turned on in addition to the Raspberry Pi running the test script. Once the test setup is ready, SOM testing should be done using the following steps: | + | * Make sure the sequencer is programmed before starting the production testing. |
+ | * Make sure all the required setup explained above is completed and the frequency counter is turned on in addition to the Raspberry Pi running the test script. Once the test setup is ready, SOM testing should be done using the following steps: | ||
<note important> | <note important> | ||
Line 134: | Line 145: | ||
* USB host mode: a Micro USB (male) an adapter to type A (female) is used to connect a usb flash, lsusb linux command is run on carrier to see if host mode is enabled and flash is detected, check speed with hdparm, check that partition is mounted | * USB host mode: a Micro USB (male) an adapter to type A (female) is used to connect a usb flash, lsusb linux command is run on carrier to see if host mode is enabled and flash is detected, check speed with hdparm, check that partition is mounted | ||
* Ethernet: A cable is connected between the board' | * Ethernet: A cable is connected between the board' | ||
- | * Audio: Audio loopback cables plugged into horizontal sets of output/ | + | * Audio: Audio loopback cables plugged into horizontal sets of output/ |
* HDMI: Monitor connectivity is checked through physical displaying output on the attached monitor | * HDMI: Monitor connectivity is checked through physical displaying output on the attached monitor | ||
* Clocks: he clock monitor IP (axi_clock_monitor) is used to test several clock signal paths. The IP features a mechanism which measures the input clock frequency relative to the system clock and stores the result in an internal register. By checking if the measured clock signal is within an expected range the path is validated. 4 clock signals are measured, 3 of them generated by the FMC loopback at the same frequency of 156MHz and one is generated by the AD9517 PLL | * Clocks: he clock monitor IP (axi_clock_monitor) is used to test several clock signal paths. The IP features a mechanism which measures the input clock frequency relative to the system clock and stores the result in an internal register. By checking if the measured clock signal is within an expected range the path is validated. 4 clock signals are measured, 3 of them generated by the FMC loopback at the same frequency of 156MHz and one is generated by the AD9517 PLL | ||
Line 147: | Line 158: | ||
<WRAP hi round download 80%> | <WRAP hi round download 80%> | ||
* **20 Dec 2021 release ** | * **20 Dec 2021 release ** | ||
- | * [[https:// | + | * [[https:// |
- | * Checksum '' | + | * Checksum '' |
</ | </ | ||
Line 179: | Line 190: | ||
* 1 adrv9361_rfsom module | * 1 adrv9361_rfsom module | ||
* 1 adrv9361_rfsom FMC carrier board (ADRV1CRR) | * 1 adrv9361_rfsom FMC carrier board (ADRV1CRR) | ||
- | * 1 microSD card and SD adapter with the latest test image ([[resources/tools-software/linux-software/ | + | * 1 microSD card and SD adapter with the latest test image ([[:resources:tools-software:linux-software: |
* 1 External monitor with HDMI input | * 1 External monitor with HDMI input | ||
* 1 Scanner | * 1 Scanner | ||
Line 285: | Line 296: | ||
=== Test image === | === Test image === | ||
- | The production test software running on the target device is the [[/resources/tools-software/linux-software/ | + | The production test software running on the target device is the [[:resources:tools-software:linux-software: |
=== Required hardware === | === Required hardware === | ||
Line 296: | Line 307: | ||
* 1 adrv9361_rfsom module | * 1 adrv9361_rfsom module | ||
* 1 adrv936x_rfsom breakout board and power adapter | * 1 adrv936x_rfsom breakout board and power adapter | ||
- | * 1 microSD card using the latest [[/resources/tools-software/linux-software/ | + | * 1 microSD card using the latest [[:resources:tools-software:linux-software: |
* 1 External computer set up to monitor the serial connection | * 1 External computer set up to monitor the serial connection | ||