This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:pzsdr:power-and-sequencing [26 Aug 2016 23:41] – [Is there a default file I can load?] Neil Wilson | resources:eval:user-guides:pzsdr:power-and-sequencing [26 Aug 2016 23:42] – [Software Settings - Input Voltage Range Determination and Setting] Neil Wilson | ||
---|---|---|---|
Line 185: | Line 185: | ||
{{: | {{: | ||
- | =====Software | + | =====Software - Input Voltage Range Determination and Setting===== |
The following provides a detailed overview on how the ADM1166 input voltage ranges are calculated and programmed to account for input and output ZYNQ voltage settings, ADM116 power sequencer input voltage ranges etc. | The following provides a detailed overview on how the ADM1166 input voltage ranges are calculated and programmed to account for input and output ZYNQ voltage settings, ADM116 power sequencer input voltage ranges etc. | ||