Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision |
resources:eval:user-guides:pzsdr:carriers:packrf [22 May 2019 16:50] – Neil Wilson | resources:eval:user-guides:pzsdr:carriers:packrf [14 Jan 2021 05:24] – use / interwiki links Robin Getz |
---|
====== PackRF ====== | ====== ADRV-PackRF ====== |
PackRF is a pair of software defined radios designed using the [[https://wiki.analog.com/resources/eval/user-guides/adrv936x_rfsom|ADRV9361-Z7035]]system on module (SOM). The SOM is based on the[[http://www.analog.com/en/products/rf-microwave/integrated-transceivers-transmitters-receivers/wideband-transceivers-ic/ad9361.html|AD9361]] RF Transceiver and the Xilinx Zynq®-7000 All Programmable (AP)SoC. | PackRF is a pair of software defined radios designed using the [[/resources/eval/user-guides/adrv936x_rfsom|ADRV9361-Z7035]]system on module (SOM). The SOM is based on the[[adi>en/products/rf-microwave/integrated-transceivers-transmitters-receivers/wideband-transceivers-ic/ad9361.html|AD9361]] RF Transceiver and the Xilinx Zynq®-7000 All Programmable (AP) SoC. |
| |
| See the [[adi>en/design-center/reference-designs/circuits-from-the-lab/cn0412.html#rd-overview|Analog Devices Product Home Page]] for information on price and options to purchase the system. |
| |
The purpose of the radio is to provide an RF platform to software developers, system architects, and product developers who want a single platform which operates over a wide tuning range (70 MHz – 6 GHz). PackRF accelerates development from initial evaluation to field deployment. | The purpose of the radio is to provide an RF platform to software developers, system architects, and product developers who want a single platform which operates over a wide tuning range (70 MHz – 6 GHz). PackRF accelerates development from initial evaluation to field deployment. |
The radio is contained inside a blue aluminum enclosure with access to connections for power, ethernet, USB, OLED, audio and micro SD card. Antenna’s connect to SMA’s on the second face plate (not shown here) for TX, RX, monitoring and GPS I/O’s. Silkscreen on the radio contains various part numbers and links to additional material. | The radio is contained inside a blue aluminum enclosure with access to connections for power, ethernet, USB, OLED, audio and micro SD card. Antenna’s connect to SMA’s on the second face plate (not shown here) for TX, RX, monitoring and GPS I/O’s. Silkscreen on the radio contains various part numbers and links to additional material. |
| |
{{ :resources:eval:user-guides:pzsdr:carriers:packrf:production_build.png?600 |1 Portable Radio Unit}} | {{ :resources:eval:user-guides:pzsdr:carriers:adrv1cc-box:pelican_case.jpg?600 | PackRF}} |
| |
===== Portable Radio Reference Design ===== | ===== Portable Radio Reference Design ===== |
The radios are referred to as 'Portable Radio Reference Design'. Each one is a combination of [[https://wiki.analog.com/resources/eval/user-guides/adrv936x_rfsom|ADRV9361-Z7035]] PCB, carrier card, metal enclosure and additional, smaller items (adapter PCBs, cables, connectors etc). The image below is one radios with plastic windows installed. The SOM, RF Shield, FPGA, and other connections are visible. Note: this unit is for demonstration purposes only. | The radios are referred to as 'Portable Radio Reference Design'. Each one is a combination of [[/resources/eval/user-guides/adrv936x_rfsom|ADRV9361-Z7035]] PCB, carrier card, metal enclosure and additional, smaller items (adapter PCBs, cables, connectors etc). The system is fully contained inside of a 159.99mm x 78.00mm x 43.00mm (6.3" x 3.071" x 1.69") aluminum metal enclosure. Card guides on the inside of the case provide a secure shelf for the PCB's. Production units will be a blue metal etched with silkscreen providing part numbers, links to documentation and more. |
| |
The system is fully contained inside of a 159.99mm x 78.00mm x 43.00mm (6.3" x 3.071" x 1.69") aluminum metal enclosure. Card guides on the inside of the case provide a secure shelf for the PCB's. Production units will be a blue metal etched with silkscreen providing part numbers, links to documentation and more. | {{ :resources:eval:user-guides:pzsdr:carriers:packrf:production_build.png?600 | 1 Portable Radio Unit}} |
| |
{{ :resources:eval:user-guides:pzsdr:carriers:portable_radio_concept:bottom.jpg?600 | Portable Radio Reference Design}} | Included with the radio module is a complete single carrier modem reference design. The modem is designed as a constantly transmitting frequency division duplexing (FDD) system with a single transmit channel (uplink) and single receive channel (downlink), enabling a single bidirectional point-to-point link between two nodes. A complete wireless video link can be demonstrated with the webcams provided in this kit between disjoint nodes. |
| |
==== Radio Hardware ==== | ==== Radio Hardware ==== |
A list of Design files is located [[https://wiki.analog.com/resources/eval/user-guides/portable-radio-reference-design/hardware|Hardware]]. These include pdf's of the schematics, gerber files, board file in native format, bill of materials and more. | A list of Design files is located in the [[/resources/eval/user-guides/pzsdr/carriers/packrf/hardware|Hardware]] section. These include pdf's of the schematics, gerber files, board file in native format, bill of materials and more. |
| |
==== Radio Features ==== | ==== Radio Design Features ==== |
The Portable Radio Reference Design is a complex system with a variety of design features. Click here for [[https://wiki.analog.com/resources/eval/user-guides/pzsdr/carriers/portable-radio-reference-design/features|information]] regarding the power supply design, mechanical considerations, battery maintenance and system logic. Each one of these plays a critical role in guaranteeing a robust design, as well as a friendly user experience. | * Hot-swappable Input Power |
| * Battery Backup |
| * Charge Maintenance |
| * OLED and Navigation Scroll Wheel |
| * Custom Designed Menu |
| |
==== Assembly ==== | |
[[https://wiki.analog.com/resources/eval/user-guides/pzsdr/carriers/portable-radio-reference-design/assembly-instructions|Assembly]] of the Portable Radio Reference Design is almost as complicated as some of the hardware and software. At the very least, it occupies a significant amount of time and will cause headaches, finger aches and if you do not pay attention or follow directions, it will test your patience. | |
| |
A detailed list of instructions is provided in the event you decided to open your Portable Radio Reference Design. Perhaps you are just assembling a unit. In either case, before you try to fix something or start building, have a look at the instructions provided below. There are a few pitfalls which can damage part of the radio and send you three steps back before you continue forward. | Follow this link for more detailed information on [[/resources/eval/user-guides/pzsdr/carriers/portable-radio-reference-design/features|design features]] regarding the power supply design, mechanical considerations, battery maintenance system logic and more. |
| ==== Portable Radio Software and HDL ==== |
| The software for the ADRV-PACKRF is provided by Analog Devices as an open source reference design that can be used in various applications. The system source code consists of several components, which are used together to control onboard devices and provide connectivity to external tools for development. Follow this link for more information on the [[/resources/eval/user-guides/pzsdr/carriers/packrf/system-software-architecture| System Software Architecture]] |
| |
The worst thing you can do is finish assembling a unit and realize you forgot to attach the heatsink, or the cable brace, or you hear something rattling around on the inside. Please be patient, read first, build second. | ==== Radio GUI ==== |
| |
| ==== Portable Radio Application Use Cases ==== |
| This [[/resources/eval/user-guides/pzsdr/carriers/packrf/example-use-case| example use case ]] allows the user to perform a simple experiment with the datalink and USB webcams. |
| * Default |
| * Modem |
| |
| |
==== The Gallery ==== | ==== Radio Assembly ==== |
There is also a [[https://wiki.analog.com/resources/eval/user-guides/pzsdr/carriers/portable-radio-reference-design/gallery|picture gallery]] to document the travels and adventures of the radio. | |
| |
| Save yourself a headache and do not disassemble the radio. |
| |
===== PackRF - Contents ===== | Assembly of the Portable Radio Reference Design is almost as complicated as some of the hardware and software. It occupies a significant amount of time and will cause headaches, finger aches and potential damage to the device. A detailed list of instructions is provided in case you are assembling or opening a radio. Have a look at the [[/resources/eval/user-guides/pzsdr/carriers/portable-radio-reference-design/assembly-instructions|assembly instructions]] before beginning. |
* This is a list of every item contained inside one PackRF. When you purchase your PackRF, it includes a variety of accessories allowing the user to exercise all aspects of the radio. | |
* Portable Radio Reference Design x2 | |
* [[http://www.xppower.com/Product/VER36-Series|AC-DC Wall-wart Power Supply (12V, 4A)]] x2 | ==== The Gallery ==== |
* [[https://www.trendnet.com/products/poe-splitters-injectors-extenders/tpe-115gi|Power over Ethernet Injector]] x2 | There is also a [[/resources/eval/user-guides/pzsdr/carriers/portable-radio-reference-design/gallery|picture gallery]] to document the travels and adventures of the radio. |
* Ethernet Cables x 2 | |
* [[https://www.logitech.com/en-us/product/hd-webcam-c270?crid=34|USB Webcam]] x2 | |
* [[http://www.tripplite.com/micro-usb-usb-otg-host-adapter-cable-5-pin-usb-micro-b-usb-a-male-female-white-6-in~U05206NWH/|USB OTG Cable]] x2 | |
* [[https://productfinder.pulseeng.com/product/W1910|Pulse W1910]] 3G Pentaband 824-2170MHz, SMA Antenna x20 | |
* [[http://www.inventeksys.com/products-page/gps-antennas/antdom-05-01-wpm-gps-antenna/|GPS Antenna]] x2 | |
* [[http://www.memoryprotectiondevices.com/documents/catalogs/MPD-12V-Parts.pdf|Power Plug to DC Cigarette Lighter]] x2 | |
* Micro SD Card x2 | |
| |
| |