This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:pmd-ard-intz [04 Sep 2020 08:50] – [I²C Port] Jesse Daniel Santos | resources:eval:user-guides:pmd-ard-intz [30 Jul 2021 07:01] – Victor Calinao, Jr | ||
---|---|---|---|
Line 94: | Line 94: | ||
==== UART Port ==== | ==== UART Port ==== | ||
- | Pmod port (P13) can be reconfigured between an expanded SPI and expanded UART. To configure P13 as expanded UART, set the shunt connectors P8, P9, and P10 similiar to the encircled in Figure U. | + | Pmod port (P13) can be reconfigured between an expanded SPI and expanded UART. To configure P13 as expanded UART, set the shunt connectors P8, P9, and P10. |
^Pin No.^P13: UART^ | ^Pin No.^P13: UART^ | ||
Line 123: | Line 123: | ||
</ | </ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | // End of document // |