Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:picozed_sdr [10 Feb 2017 19:55] – Fix spelling of GNU Radio Robin Getz | resources:eval:user-guides:picozed_sdr [20 Apr 2017 21:47] – some edits David Babicz |
---|
====== PicoZed SDR ====== | ====== RFSOM SDR ====== |
{{ http://picozed.org/sites/default/files/styles/product_slider/public/product/hand.png}} | |
| |
The [[http://picozed.org/sdr|PicoZed SDR]] is built on a portfolio of highly integrated System-On-Module (SOMs) based on the Xilinx Zynq®-7000 All Programmable (AP)SoC, built by [[http://www.avnet.com|Avnet]]. Avnet is expanding into application-specific solutions to meet the unprecedented demand for wideband wireless communications. Built on the AD9361, it is schematically & HDL similar to the [[AD-FMCOMMS3-EBZ]]. | The RFSOM SDR is built on a portfolio of highly integrated System-On-Module (SOMs) based on the Xilinx Zynq®-7000 All Programmable (AP)SoC. These SOMs are application-specific solutions designed to meet the unprecedented demand for wideband wireless communications. Built on the AD9361, it is schematically & HDL similar to the [[AD-FMCOMMS3-EBZ]]. |
| |
The purpose of the PicoZed SDR is to provide an RF platform to software developers, system architects, product developers, etc, who want a single platform which operates over a wide tuning range (70 MHz – 6 GHz). | The purpose of the RFSOM SDR is to provide an RF platform to software developers, system architects, product developers, etc, who want a single platform which operates over a wide tuning range (70 MHz – 6 GHz). |
| |
===== Table of Contents ===== | ===== Table of Contents ===== |