This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:mykonos:software:filters [28 Aug 2017 08:40] – sripad Jadhav | resources:eval:user-guides:mykonos:software:filters [14 Jan 2021 05:24] – use mw> interwiki links Robin Getz | ||
---|---|---|---|
Line 15: | Line 15: | ||
* **Executable**: | * **Executable**: | ||
- | >> | + | The MATLAB runtime engine can be downloaded from the following link: |
- | [[https:// | + | [[mw>products/ |
* **MATLAB App**: the app runs as an application within MATLAB. Use of the app requires MATLAB to be running with valid licenses for the Control System Toolbox as well as MATLAB itself. The GUI and flexibility are identical to the executable, but running as an app in MATLAB allows the user to write additional code to post-process the data files created by the wizard. | * **MATLAB App**: the app runs as an application within MATLAB. Use of the app requires MATLAB to be running with valid licenses for the Control System Toolbox as well as MATLAB itself. The GUI and flexibility are identical to the executable, but running as an app in MATLAB allows the user to write additional code to post-process the data files created by the wizard. | ||
Line 97: | Line 97: | ||
- < | - < | ||
- | - < | + | - < |
- < | - < | ||
- < | - < | ||
Line 104: | Line 104: | ||
* Tx Rules | * Tx Rules | ||
* 30 MSPS < = Tx Input Sample Rate < = 320 MSPS | * 30 MSPS < = Tx Input Sample Rate < = 320 MSPS | ||
- | * 5 MHz < = Tx Primary Signal BW < = 100 MHz | + | * 10 MHz < = Tx Primary Signal BW < = 100 MHz |
* 20 MHz < = Tx RF (Synthesis) BW < = 240 MHz | * 20 MHz < = Tx RF (Synthesis) BW < = 240 MHz | ||
* Tx Primary Signal BW < = Tx RF (Synthesis) BW | * Tx Primary Signal BW < = Tx RF (Synthesis) BW | ||
Line 115: | Line 115: | ||
* Rx Rules | * Rx Rules | ||
* 20 MSPS < = Rx Output Sample Rate < = 200 MSPS | * 20 MSPS < = Rx Output Sample Rate < = 200 MSPS | ||
- | * 5 MHz < = Rx Signal BW < = 100 MHz | + | * 8 MHz < = Rx Signal BW < = 100 MHz |
* Rx Signal BW > = 0.4 * Rx Output Sample Rate | * Rx Signal BW > = 0.4 * Rx Output Sample Rate | ||
* Rx Signal BW < = 0.82 * Rx Output Sample Rate | * Rx Signal BW < = 0.82 * Rx Output Sample Rate | ||
Line 124: | Line 124: | ||
* Rx FIR decimation options: 1, 2, 4 | * Rx FIR decimation options: 1, 2, 4 | ||
* ORx Rules | * ORx Rules | ||
- | * 5 MHz < = ORx Signal BW < = 240 MHz | + | * 8 MHz < = ORx Signal BW < = 240 MHz |
* 20 MSPS < = ORx Output Sample Rate < = 320 MSPS | * 20 MSPS < = ORx Output Sample Rate < = 320 MSPS | ||
* ORx Signal BW > = 0.4 * ORx Output Sample Rate | * ORx Signal BW > = 0.4 * ORx Output Sample Rate |