This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:mykonos:software:filters [02 Aug 2017 22:58] – Tom Karpus | resources:eval:user-guides:mykonos:software:filters [24 Jul 2018 06:47] – [AD9371 Filter Wizard Rules] sripad Jadhav | ||
---|---|---|---|
Line 14: | Line 14: | ||
There are three ways you can use the AD9371 Filter Wizard: | There are three ways you can use the AD9371 Filter Wizard: | ||
- | * **Executable**: | + | * **Executable**: |
+ | The MATLAB runtime engine can be downloaded from the following link: | ||
[[https:// | [[https:// | ||
Line 92: | Line 93: | ||
{{: | {{: | ||
+ | |||
+ | When you click on the " | ||
+ | |||
+ | - < | ||
+ | - < | ||
+ | - < | ||
+ | - < | ||
====== AD9371 Filter Wizard Rules ====== | ====== AD9371 Filter Wizard Rules ====== | ||
* Tx Rules | * Tx Rules | ||
* 30 MSPS < = Tx Input Sample Rate < = 320 MSPS | * 30 MSPS < = Tx Input Sample Rate < = 320 MSPS | ||
- | * 5 MHz < = Tx Primary Signal BW < = 100 MHz | + | * 10 MHz < = Tx Primary Signal BW < = 100 MHz |
* 20 MHz < = Tx RF (Synthesis) BW < = 240 MHz | * 20 MHz < = Tx RF (Synthesis) BW < = 240 MHz | ||
* Tx Primary Signal BW < = Tx RF (Synthesis) BW | * Tx Primary Signal BW < = Tx RF (Synthesis) BW | ||
Line 107: | Line 115: | ||
* Rx Rules | * Rx Rules | ||
* 20 MSPS < = Rx Output Sample Rate < = 200 MSPS | * 20 MSPS < = Rx Output Sample Rate < = 200 MSPS | ||
- | * 5 MHz < = Rx Signal BW < = 100 MHz | + | * 8 MHz < = Rx Signal BW < = 100 MHz |
* Rx Signal BW > = 0.4 * Rx Output Sample Rate | * Rx Signal BW > = 0.4 * Rx Output Sample Rate | ||
* Rx Signal BW < = 0.82 * Rx Output Sample Rate | * Rx Signal BW < = 0.82 * Rx Output Sample Rate | ||
Line 116: | Line 124: | ||
* Rx FIR decimation options: 1, 2, 4 | * Rx FIR decimation options: 1, 2, 4 | ||
* ORx Rules | * ORx Rules | ||
- | * 5 MHz < = ORx Signal BW < = 240 MHz | + | * 8 MHz < = ORx Signal BW < = 240 MHz |
* 20 MSPS < = ORx Output Sample Rate < = 320 MSPS | * 20 MSPS < = ORx Output Sample Rate < = 320 MSPS | ||
* ORx Signal BW > = 0.4 * ORx Output Sample Rate | * ORx Signal BW > = 0.4 * ORx Output Sample Rate |