This is an old revision of the document!
The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the ADRV9371-N/PCBZ, ADRV9371-W/PCBZ boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.
The ADRV9371/PCBZ is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:
The supported OS are:
In most carriers, the ADRV9371/PCBZ board connects to the HPC connector (unless otherwise noted). The carrier setup requires power, UART (115200), ethernet (Linux), HDMI (if available) and/or JTAG (no-OS) connections. A few typical setups are shown below.