This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:mykonos:no-os-setup [04 Jun 2018 15:58] – Add KCU105 and ZCU102 platforms Dragos Bogdan | resources:eval:user-guides:mykonos:no-os-setup [11 Sep 2018 13:15] – 2016_R2 -> master Dragos Bogdan | ||
---|---|---|---|
Line 127: | Line 127: | ||
* The next step is to copy all the relevant source code into the **software** directory. | * The next step is to copy all the relevant source code into the **software** directory. | ||
* **AD9371/ | * **AD9371/ | ||
- | * Download from https:// | + | * Download from https:// |
* Next copy the files intro the src folder of your newly created project. You can do this with Ctrl+C Ctrl+V or simple drag and drop | * Next copy the files intro the src folder of your newly created project. You can do this with Ctrl+C Ctrl+V or simple drag and drop | ||
Line 205: | Line 205: | ||
* Once DDS or DMA mode is selected and the project configuration can be ran. | * Once DDS or DMA mode is selected and the project configuration can be ran. | ||
* Open an UART terminal, set the baud rate to 115200bps and make sure the initialization was completed, as in the screenshot bellow: {{ : | * Open an UART terminal, set the baud rate to 115200bps and make sure the initialization was completed, as in the screenshot bellow: {{ : | ||
- | * Next, download the capture scripts from the [[https:// | + | * Next, download the capture scripts from the [[https:// |
* By running **capture.bat**, | * By running **capture.bat**, | ||
* Start [[http:// | * Start [[http:// |