Jupiter SDR - known issues
Since this evaluation platform is not yet released we have a list of known issues and features which are not supported on the early evaluation samples.
Known issues
TX RF matching is not optimal - it will be improved on the released product
IIO buffer size limited to 131072 samples when used with
USB interface
Features not supported
-
QSPI boot - no boot image flashed on the memory
Multi chip synchronization (MCS) - Synchronizing multiple Jupiter SDR devices is not supported.
Fan control - we don't have implemented the automatic fan control
Current libiio implementation allows data streaming throughput of about 45
MB/s on both
USB and Ethernet. The throughput will be improved once
future libiio improvements will be implemented.
HDL does not support ADRV9002 CMOS interface