Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision |
resources:eval:user-guides:inertial-mems:imu:vibrationevaluationprogram [08 Jan 2021 09:36] – Fixed bad link for ADIS16228 Ioana Chelaru | resources:eval:user-guides:inertial-mems:imu:vibrationevaluationprogram [17 Feb 2021 05:20] – test Juan Chong |
---|
====VIBRATION EVALUATION PROGRAM WIKI GUIDE===== | ====== EVAL-ADIS2 Vibration Evaluation Software User Guide ====== |
| |
=====PRODUCT SUPPORT===== | <note warning>The [[adi>EVAL-ADIS2|EVAL-ADIS2]] has been superseded by the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] and is **no longer supported**.</note> |
| |
The [[http://www.analog.com/en/evaluation/EVAL-ADIS/eb.html#SOFTWARE_AND_TOOLS|Vibration Evaluation Program]] supports PC-based evaluation of the following products with the [[adi>EVAL-ADIS|EVAL-ADIS]] Evaluation System. | <note warning>This guide assumes that you've connected your vibration sensor to the [[adi>EVAL-ADIS2|EVAL-ADIS2]], drivers were successfully installed on your PC, and you've downloaded the correct software for your sensor. We recommend reviewing the [[:resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis2-hardware-guide|Hardware User Guide]] before continuing.</note> |
| |
^IMU Evaluation/EVAL-ADIS Product Support List ^ | ===== Software Downloads ===== |
|[[adi>ADIS16000|ADIS16000AMLZ]]/[[adi>ADIS16229|ADIS16229AMLZ]] | | |
|[[adi>ADIS16227|ADIS16227/PCBZ]] | | |
|[[adi>ADIS16228|ADIS16228/PCBZ]] | | |
| | | |
| |
NOTE: The [[adi>ADIS16000|ADIS16000AMLZ]] manages wireless communication with the [[adi>ADIS16229|ADIS16229AMLZ]]. | Click [[adi>media/en/evaluation-boards-kits/evaluation-software/Vibration_Evaluation.zip|here]] to download the latest version of the Vibration Evaluation software. |
| |
NOTE: The [[adi>ADIS16000|ADIS16000AMLZ]] requires an interface board to connect to the [[adi>eval-adis|EVAL-ADIS]] evaluation system. This board will be released shortly as the ADIS16COM1/PCBZ. | Click [[adi>media/en/evaluation-boards-kits/evaluation-software/SDPDrivers.zip|here]] to download the latest drivers for the [[adi>EVAL-ADIS2|EVAL-ADIS2]]. |
| |
=====PC SYSTEM REQUIREMENTS===== | <note important>This application requires Microsoft .NET 3.5 to be installed and enabled on the host PCs running Windows 10. Additional information on enabling .NET 3.5 can be found [[https://answers.microsoft.com/en-us/windows/forum/windows_10-windows_install-winpc/installingenabling-net-35-on-windows-10/fe7b4699-c096-4369-b06f-e1063da42e18|here]].</note> |
Windows XP, Vista, 7 | |
| |
.NET Framework 3.5 | ===== EVAL-ADIS2 Vibration Evaluation Software Overview ===== |
| |
NOTE: Newer versions of the .NET framework do not currently support the [[/resources/eval/user-guides/inertial-mems/imu/vibrationevaluationprogram|Vibration Evaluation Program]]. | The Vibration Evaluation Software is a Microsoft Windows (.NET) application that works in conjunction with the EVAL-ADIS2, in order to provide users with a PC-Based interface to a subset of iSensor products designed specifically for machine health and vibration monitoring applications. The platform enables observation of basic sensor functions, read/write access to all user-accessible registers, and full-rate data acquisition. |
| |
=====VIBRATION EVALUATION PROGRAM DOWNLOAD===== | Due to the specialized nature of the machine health monitoring portfolio, only a subset of sensors is supported by this software. These devices are shown below. |
| |
[[http://www.analog.com/en/evaluation/EVAL-ADIS/eb.html#SOFTWARE_AND_TOOLS|Vibration Evaluation Software]] installation only requires two simple step: | ^SENSOR DEVICE NUMBER ^ |
| |[[adi>ADIS16000|ADIS16000AMLZ]] | |
| |[[adi>ADIS16229|ADIS16229AMLZ]] | |
| |[[adi>ADIS16227|ADIS16227/PCBZ]] | |
| |[[adi>ADIS16228|ADIS16228/PCBZ]] | |
| |
1. Download, unzip and install the EVAL-ADIS USB Driver [[http://www.analog.com/en/evaluation/EVAL-ADIS/eb.html#SOFTWARE_AND_TOOLS|(click here to see the download link)]] | <note important>The [[adi>ADIS16000|ADIS16000AMLZ]] manages wireless communication between several [[adi>ADIS16229|ADIS16229AMLZ]] devices. </note>. |
| |
2. Download, unzip and copy the Vibration*.exe file to the desired location on the test PC [[http://www.analog.com/en/evaluation/EVAL-ADIS/eb.html#SOFTWARE_AND_TOOLS|(click here to see the download link)]] | <note important>This guide builds upon the [[:resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis2-hardware-guide|EVAL-ADIS2 Hardware User Guide]] and assumes that you've installed the necessary drivers and software.</note> |
=====USB DRIVER INSTALLATION===== | |
After downloading the EVAL-ADIS USB Driver file, extract the SDPDrivers.exe file from the zip file, into a convenient location and then double click on it to start the process. | |
| |
{{:resources:eval:user-guides:inertial-mems:imu:USBDriver-Install-000.png?500|}} | ===== Using the EVAL-ADIS2 Vibration Evaluation Software ===== |
| Once the Vibration Evaluation software loads, you should be presented with a window similar to the image shown below. |
When the setup wizard opens, click on **Next** to start the installation process | |
| |
{{:resources:eval:user-guides:inertial-mems:imu:USBDriver-Install-001.png?500|}} | |
| |
Click on **Next** to accept the default driver location. | |
| |
{{:resources:eval:user-guides:inertial-mems:imu:USBDriver-Install-002.png?500|}} | |
| |
The process will involve at least two progress bars that look like the following: | |
| |
{{:resources:eval:user-guides:inertial-mems:imu:USBDriver-Install-003.png?500|}} | |
| |
If you encounter this type of message during the process, click on **Install** to continue with the installation. | |
| |
{{:resources:eval:user-guides:inertial-mems:imu:USBDriver-Install-003a.png?500|}} | |
| |
Once the installation has completed, click on **Finish** to complete the process. | |
| |
{{:resources:eval:user-guides:inertial-mems:imu:USBDriver-Install-004.png?500|}} | |
| |
=====DOWNLOAD SOFTWARE===== | |
Download to the **Vibration Evaluation Program** package from the [[adi>EVAL-ADIS|EVAL-ADIS]] home page, under SOFTWARE AND TOOLS ([[adi>en/evaluation/EVAL-ADIS/eb.html#SOFTWARE_AND_TOOLS|Click here to access]]). Extract the *.exe file from the zip file and copy it to any directory on the PC. | |
| |
=====LAUNCH SOFTWARE===== | |
Plug the EVAL-ADIS (with ADIS16xxx/PCBZ device installed) and wait for both LED1 and LED2 to illuminate on the EVAL-ADIS. After LED1 and LED2 illuminate, double click on the *.exe file to launch the **Vibration Evaluation Program** and access the **Main Menu**. | |
| |
You might see the appearance of a Window that indicates a search for an SDP device (USB), but this will disappear quickly. If this error message appears, click **OK** to proceed to the **Main Screen**. | |
| |
{{:resources:eval:user-guides:inertial-mems:imu:227-select-device.png?400|}} | {{:resources:eval:user-guides:inertial-mems:imu:227-select-device.png?400|}} |
=====PROGRAM FEATURES===== | =====PROGRAM FEATURES===== |
====Device Selection==== | ====Device Selection==== |
Click on **Device**, located on the left hand side of the Menu bar, at the top of the **Main Screen**, to select the appropriate DUT (Device Under Test). In this example, the [[adi>adis16228|ADIS16228]] is in use. Note that some of the Menu bar options appear in a lighter gray color, to indicate that they are not associated with a particular device. For example, all of the **Network** options presently only apply to the [[adi>adis16299|ADIS16229]] at this time, so they will appear in the lighter gray color when either [[adi>ADIS16227|ADIS16227]] or [[adi>ADIS16228|ADIS16228]] options are in use. | Click on **Device**, located on the left hand side of the Menu bar, at the top of the **Main Screen**, to select the appropriate DUT (Device Under Test). In this example, the [[adi>adis16228|ADIS16228]] is in use. Note that some of the Menu bar options appear in a lighter gray color, to indicate that they are not associated with a particular device. For example, all of the **Network** options presently only apply to the [[adi>ADIS16229|ADIS16229]] at this time, so they will appear in the lighter gray color when either [[adi>ADIS16227|ADIS16227]] or [[adi>ADIS16228|ADIS16228]] options are in use. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:227-main-device.png?600|}} | {{:resources:eval:user-guides:inertial-mems:imu:227-main-device.png?600|}} |
====Demo==== | ====Demo==== |
| |
Visit the [[resources/eval/user-guides/inertial-mems/imu/vibrationdemo|ADIS16229 Vibration Demo Wiki Guide]] for more details on this function. | Visit the [[resources:eval:user-guides:inertial-mems:imu:vibrationdemo|ADIS16229 Vibration Demo Wiki Guide]] for more details on this function. |
====About==== | ====About==== |
This option offers the revision and some codes that might be useful when seeking technical support. | This option offers the revision and some codes that might be useful when seeking technical support. |
| |
====Data Collection Mode==== | ====Data Collection Mode==== |
The [[adi>ADIS16227|ADIS16227]], [[adi>ADIS16228|ADIS16228]] and [[adi>adsi16229|ADIS16229]] all have four basic modes of data collection: Manual FFT, Automatic FFT, Manual Time (Time Domain) and Real-Time. Inside of these products, these modes are typically related to the settings in the REC_CTRL1 register. The **Main Screen** offers a drop-down selection menu for these modes, along with a **Start** button to begin operation. | The [[adi>ADIS16227|ADIS16227]], [[adi>ADIS16228|ADIS16228]] and [[adi>ADIS16229|ADIS16229]] all have four basic modes of data collection: Manual FFT, Automatic FFT, Manual Time (Time Domain) and Real-Time. Inside of these products, these modes are typically related to the settings in the REC_CTRL1 register. The **Main Screen** offers a drop-down selection menu for these modes, along with a **Start** button to begin operation. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:vep_wiki_mainscreen_modeselection_01b.png?600|}} | {{:resources:eval:user-guides:inertial-mems:imu:vep_wiki_mainscreen_modeselection_01b.png?600|}} |